element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 3D Printer support
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 31 subscribers
  • Views 1568 views
  • Users 0 members are here
  • printer
  • 3d
  • stepper-motor
  • ramps
  • arduino
  • extruder
Related

3D Printer support

anej
anej over 11 years ago

Hello.

So i am planning on making a 3D printer. I know that i can buy a kit and all that but i really want to build my own.

Here are some of the parts i would use:

- Extruder head: http://www.ebay.com/itm/Geeetech-MK8-extruder-J-head-Print-ABS-PLA-for-3D-Printer-Reprap-Mendel-/390993481130?pt=LH_DefaultDomain_15&var=&hash=item5b09070daa

- 4X Stepper motor (one for X, one for Y and two for Z): http://www.ebay.com/itm/1pcs-Nema17-Stepper-Motors-2-Phase-Motor-for-3D-Printer-Prusa-Mendel-Makerbot-/191081254280?pt=LH_DefaultDomain_0&hash=item2c7d548d88

- Heated bed: http://www.ebay.com/itm/1-RepRap-3D-Printer-PCB-Heatbed-MK2a-Heat-Bed-for-Prusa-Mendel-/171275126930?pt=LH_DefaultDomain_0&hash=item27e0cb0892

- Controller: http://www.ebay.com/itm/Mega2560-R3-RAMPS-1-4-REPRAP-3D-Printer-CONTROLLER-A4988-Stepper-Motor-Driver-/131057008442?pt=LH_DefaultDomain_0&hash=item1e839b3f3a

Ok. So now I don't know if that arduino + ramps is everything i need. Does arduino connect to the computer and the data is transfered through arduino or ?

Are there any additional parts that i would need ?

Here is the design of how i am planing making it (not quite finnished yet but you get the idea...): http://prntscr.com/68ep96

EDIT: Shoud i use a display too ?

  • Sign in to reply
  • Cancel

Top Replies

  • kingrahl
    kingrahl over 11 years ago +1
    You've got some of the major necessities down. Judging from your picture, you'll need the pulleys, belts, linear rods, threaded rods, and nuts for threaded rods. Not to mention all the hardware, nuts,…
  • kingrahl
    kingrahl over 11 years ago in reply to anej +1
    I use 1.75mm. It seems to be becoming a standard amongst printers. Some people have strong opinions for either. Just like size of filament, the type (ABS, PLA, other) each have there advantages and disadvantages…
  • kingrahl
    kingrahl over 11 years ago in reply to anej +1
    Yes. It's friction is higher than ABS or PLA so sliding through a PTFE tube will be harder. Also since it is "softer" it can smash and bend inside the tube creating a bind.
Parents
  • sgtsabot
    sgtsabot over 11 years ago

    One though. Using screws for the Y and Z axis will have a much higher resolution than the X axis which is belt driven. While the screw also increases the lifting ability of the Z axis, you dont gain much in the Y axis over using another belt or you could use a screw to match the resolution of the X to the Y.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anej
    anej over 11 years ago in reply to sgtsabot

    So should I use threaded rods on X,Y and Z ? Doesent that slow down the whole print or will it be OK ?

    EDIT: Could I use gears to increase the resolution?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • kingrahl
    kingrahl over 11 years ago in reply to anej

    I don't know what Mark Huey was talking about. There is no reason why changing a belt to a threaded rod in one axis (Y) and not the other (X) would make any sense. I took it as some sort of miscommunication and was just going to not reply.

     

    Threaded rods will definitely slow the printer. This would be the equivalent to using a CNC machine as a 3d printer.

     

    Yes, you can use gears. This will also slow the motors. There are so many steps per revolution depending on the motor you use. The more steps per inch the higher the resolution. But your motors can only spin so fast. In other words, slower movements. You will also need to make everything tight fitting. Any "slop" between gears and that takes away the added resolution you are going for.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anej
    anej over 11 years ago in reply to kingrahl

    Ok. So i will stay with the belt on X and Y and on Z i will use rod - the Z doesen't need to move fast right?

    So those stepper motors i will buy it says "Step Angle: 1.8 degree+-5%" - is that the "resolution" of the motor and is that ok?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • anej
    anej over 11 years ago in reply to kingrahl

    Ok. So i will stay with the belt on X and Y and on Z i will use rod - the Z doesen't need to move fast right?

    So those stepper motors i will buy it says "Step Angle: 1.8 degree+-5%" - is that the "resolution" of the motor and is that ok?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kingrahl
    kingrahl over 11 years ago in reply to anej

    You probably won't get a full turn of the screw on the z-axis for each layer. It doesn't need to move fast.

     

    1.8 degrees is pretty much the standard to use. The resolution is a factor of the gearing system. Resolution measurements is accomplished by calculating how many steps (or 1.8 degrees out of 360) your motor takes causing the circumference of your pulley to move your belt a linear length of 100mm. This is all a part of calibrating your printer when you program your controller board.