element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 3D Printer support
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 31 subscribers
  • Views 1579 views
  • Users 0 members are here
  • printer
  • 3d
  • stepper-motor
  • ramps
  • arduino
  • extruder
Related

3D Printer support

anej
anej over 11 years ago

Hello.

So i am planning on making a 3D printer. I know that i can buy a kit and all that but i really want to build my own.

Here are some of the parts i would use:

- Extruder head: http://www.ebay.com/itm/Geeetech-MK8-extruder-J-head-Print-ABS-PLA-for-3D-Printer-Reprap-Mendel-/390993481130?pt=LH_DefaultDomain_15&var=&hash=item5b09070daa

- 4X Stepper motor (one for X, one for Y and two for Z): http://www.ebay.com/itm/1pcs-Nema17-Stepper-Motors-2-Phase-Motor-for-3D-Printer-Prusa-Mendel-Makerbot-/191081254280?pt=LH_DefaultDomain_0&hash=item2c7d548d88

- Heated bed: http://www.ebay.com/itm/1-RepRap-3D-Printer-PCB-Heatbed-MK2a-Heat-Bed-for-Prusa-Mendel-/171275126930?pt=LH_DefaultDomain_0&hash=item27e0cb0892

- Controller: http://www.ebay.com/itm/Mega2560-R3-RAMPS-1-4-REPRAP-3D-Printer-CONTROLLER-A4988-Stepper-Motor-Driver-/131057008442?pt=LH_DefaultDomain_0&hash=item1e839b3f3a

Ok. So now I don't know if that arduino + ramps is everything i need. Does arduino connect to the computer and the data is transfered through arduino or ?

Are there any additional parts that i would need ?

Here is the design of how i am planing making it (not quite finnished yet but you get the idea...): http://prntscr.com/68ep96

EDIT: Shoud i use a display too ?

  • Sign in to reply
  • Cancel

Top Replies

  • kingrahl
    kingrahl over 11 years ago +1
    You've got some of the major necessities down. Judging from your picture, you'll need the pulleys, belts, linear rods, threaded rods, and nuts for threaded rods. Not to mention all the hardware, nuts,…
  • kingrahl
    kingrahl over 11 years ago in reply to anej +1
    I use 1.75mm. It seems to be becoming a standard amongst printers. Some people have strong opinions for either. Just like size of filament, the type (ABS, PLA, other) each have there advantages and disadvantages…
  • kingrahl
    kingrahl over 11 years ago in reply to anej +1
    Yes. It's friction is higher than ABS or PLA so sliding through a PTFE tube will be harder. Also since it is "softer" it can smash and bend inside the tube creating a bind.
Parents
  • anej
    anej over 11 years ago

    One more thing image
    Do I need a gearbox on the extruder if I decide to use 3mm filament ?

    And is printing with 1,75mm little slower or no ?

    EDIT: What threated rod should I use ? The one ont the picture 1 or picture 2 (finer)

    Picture1: http://image.made-in-china.com/2f0j00mjrQcHfKbDbP/Acme-Carbon-Steel-Threaded-Rod.jpg

    Picture2: http://www.onlinemetalsupply.com/Images/Threaded_Rod.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • anej
    anej over 11 years ago

    One more thing image
    Do I need a gearbox on the extruder if I decide to use 3mm filament ?

    And is printing with 1,75mm little slower or no ?

    EDIT: What threated rod should I use ? The one ont the picture 1 or picture 2 (finer)

    Picture1: http://image.made-in-china.com/2f0j00mjrQcHfKbDbP/Acme-Carbon-Steel-Threaded-Rod.jpg

    Picture2: http://www.onlinemetalsupply.com/Images/Threaded_Rod.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • kingrahl
    kingrahl over 11 years ago in reply to anej

    Gearbox? No. There are many people using direct drive in there extruders.

    Slower? No. It all depends on how fast the heater can melt the volume of plastic. While the travel distance of 1.75mm will be longer to match the volume of a shorter piece of 3mm filament, the thicker diameter of 3mm may take longer to melt the center. Pretty much equaling each other out.

     

    The threaded rod will depend on what you thread onto it. While the fine threads allow for more accurate layer height. If there is any slop or wobble moving the build platform, layer height won't matter if they aren't aligned. Fine threads also means more steps for the motor. More steps per distance equals higher detail control. More steps also means slower movement.