element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Help: Raspberry Pi with a Portable TV as a screen?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 32 subscribers
  • Views 1494 views
  • Users 0 members are here
  • composite
  • tv
  • mod
  • raspberry
  • help
  • hack
  • portable
  • pi
  • project
  • video
  • show
  • challenge
  • heck
  • ben
Related

Help: Raspberry Pi with a Portable TV as a screen?

RovertScott
RovertScott over 11 years ago

Hey Ben,

 

I'm trying to find a way to add composite video to an old OPTIMUS portable LCD TV for a Raspberry Pi project, but information is scarce.

Then I found out you used to use them on old portable game console hacks.

Here are some pictures of what I'm working with, do you think it's possible?

 

Rov

 

image

image

image

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 11 years ago +4 suggested
    Hi Rovert, Check out the data sheet (PDF) for the Mitsubishi M51348FP IC on that board, you can see there is a ceramic resonator (probably the one above the two cans in your second photo) and you could…
  • shabaz
    shabaz over 11 years ago in reply to RovertScott +1
    Hi Rovert, I was originally thinking lift the resonator on short wires, remove the wire that is connected to pin 18, and connect your video feed (via a 10nF capacitor) to the pin on the resonator that…
Parents
  • clem57
    0 clem57 over 11 years ago

    Looking at http://support.radioshack.com/support_video/doc48/48495.htm it appears it can take a/v in. Why not splice a cable together to adapt RCA to this A/V.

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RovertScott
    0 RovertScott over 11 years ago in reply to clem57

    I don't think that applies to this model. From what I can tell, that A/V jack is just for an external antenna.

    I've tried using various connections, but to no avail...

    It works with old game consoles such as the NES and SNES but they use an RF signal tuned to channel 3.

    Based on the traces, it appears it's wired to the same as the standard antenna.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • RovertScott
    0 RovertScott over 11 years ago in reply to clem57

    I don't think that applies to this model. From what I can tell, that A/V jack is just for an external antenna.

    I've tried using various connections, but to no avail...

    It works with old game consoles such as the NES and SNES but they use an RF signal tuned to channel 3.

    Based on the traces, it appears it's wired to the same as the standard antenna.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • screamingtiger
    0 screamingtiger over 11 years ago in reply to RovertScott

    All you cant do is convert the composite signal to RF.

    UP front cost will be more expensive than just buying a TFT lcd screen designed for the Pi.

    http://www.mcmelectronics.com/product/83-16871?t=2&utm_expid=8634549-27.0czCl7fSQamjILoiAH9mgA.1&utm_referrer=http%3A%2F%2Felectronics.mcmelectronics.com%2Fsearch%3Fcataf%3D%26view%3Dlist%26w%3Dpi%2Bscreen%26x%3D0%26y%3D0

     

    $34 USD?  I mean unless you just want the work for some reason I would go this route.