element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Need help identifying an early 90s PCB thru-hole transformer and a few other questions
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 7 answers
  • Subscribers 34 subscribers
  • Views 4275 views
  • Users 0 members are here
Related

Need help identifying an early 90s PCB thru-hole transformer and a few other questions

chrisbc
chrisbc over 8 years ago

Hi. I need help identifying an early 90s PCB transformer. It's on an auto-idle control board from an early 90s gas-powered generator from a company that has since gone out of business. I'm not familiar with components but think I can identify all of the other components to remake another board in case of a catastrophic failure. The problem I'm having is identifying the size and type of what I think is a transformer. I've included a few pictures. It's located at the bottom of the board and has a yellow and red wire wrapped around it. The red wire comes from the generator head and goes out to a breaker to power the receptacles, and the yellow wire comes from a terminal lug next to another terminal lug which accepts the other (yellow) wire coming from the generator head.imageimageimage

And can anyone tell how big the small capacitor is that's located to the right above the transformer? I can't find any marks on it other than the temperature rating.

 

I also have to replace a 5W 82ohm resistor that blew due to a bad Schottky diode that I've found and will replace. Would it be safer to replace the blown resistor with a 12W 82ohm resistor? And can I use an aluminum encased surface mount resistor on a thru-hole PCB?

 

Any help would be appreciated!

Attachments:
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +4 suggested
    Hi Chris, The small capacitor is probably marked on the side that is glued down. You may have to pry it loose carefully. You can up the wattage of a resistor without any consequence except that of a larger…
  • jw0752
    jw0752 over 8 years ago in reply to chrisbc +4 suggested
    Hi Chris, If you mount a power resistor on the board make sure it is in a raised position so air is free to flow around it. This will keep it from damaging the board. You may not get the full wattage dissipation…
  • three-phase
    three-phase over 8 years ago +3 suggested
    I would agree with jw0752 that the small transformer is a current transformer measuring the load on the sockets to allow the engine speed to be controlled based upon the load the generator is supplying…
Parents
  • mcb1
    0 mcb1 over 8 years ago

    There is one available to purchase.

    100105-01 | Desa International* | Circuit Board REPAIR

     

    Not sure if this one is valid or not

    http://www.uhtastore.top/space-heaters-c-42_1633_3697_3699/desa-auto-idle-circuit-board-10010501-nos-p-7315.xhtml

     

    Sounds like these are not as reliable as they should be, and maybe you can start a repair business...

     

    The manual shows how they interconnect.

    Desa GENERATOR User's Manual

    so the transformer seems to be detecting the load and throttling back whenever the load drops off.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • chrisbc
    0 chrisbc over 8 years ago in reply to mcb1

    Thanks for the help Mark. I've seen the first one about Galco's repair for almost $200 which I'm trying to avoid by repairing it myself if possible; I've called them for a little information on parts but they couldn't help. That second website looks suspect, they've only been registered since last August. I've now, with John's help, been able to identify all of the parts except for the small ceramic disc capacitor's voltage. It says 103Z on it which I've found is a .01uF capacitor but I don't know what voltage is needed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to chrisbc

    chrisbc

    That second website looks suspect

    I thought that as well, but sometimes you never know.

     

    jw0752 is quite right

    No one seems to be too concerned with the voltage on ceramic disks and it is extremely rare for them to degrade or fail.

    500v versions will work if there is no other choice, however I doubt it is faulty, and you should be able to test it.

     

    The black electrolytic seems to be part of the power supply to control the SCR which then controls the solenoid, and I'm pretty sure this will be degraded.

     

    If you were to take a good photo of the underside, I'm pretty sure John will have the schematic done in no time. image

    (To be fair the details of the SCR would also be nice to inclde here as well.)

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • chrisbc
    0 chrisbc over 8 years ago in reply to mcb1

    I may re-use the old ones but will these work? CERA-MITE .01uF 250v 103Z 12mm disk Radial Ceramic Capacitor? They're 12mm instead of the 6mm on my board... Would it be okay to squeeze them in? And how do I test ceramic disc capacitors? I only have an average digital multimeter but can check capacitance and diodes too. The two SCRs are MCR100-8 thyristors, I've ordered some of those along with a replacement electrolytic cap which was a 47uF 16v.

     

    Here's a picture of the back of the board and a picture of the pull solenoid that's hooked to the engine's governor arm that the auto-idle board controls. I've pulled a few of the components so is still some flux I've yet to clean off the board. The darkened area on the board is where the 5W 82ohm resistor blew and made a mess (I've cleaned out the carbon with a Dremel). I think I'll replace it with a larger 12w 82ohm resistor.

     

     

    imageimageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to chrisbc

    Hi Chris,

     

    The ceramics look good, they don't really need changing. Physically bigger ones would be fine if you really want to, but it is not going to fix anything, because the originals won't be faulty.

    Can I ask, where are you getting your replacement parts from?

    The reason I'm asking is because if I google "CERA-MITE .01uF 250v 103Z 12mm disk Radial Ceramic Capacitor" then I get hits on Amazon and ebay.

    That's not really a good source for parts. You might get lucky with them, but if you're obtaining your semiconductors, i.e. the SCRs from there too, that rings some warning bells. From personal experience, there is a significant risk of getting fake or pre-used parts disguised to look like new.

    Fake/pre-used and real semiconductors are difficult enough for any engineer to distinguish visually (and sometimes even with test tools), so it really isn't worth the risk unless perhaps it is for some low power hobby experimentation (which isn't the case for your repair).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • chrisbc
    0 chrisbc over 8 years ago in reply to shabaz

    Hi shabaz. Yes, that is where I ordered the MCR100-8 SCRs from... coming from China. I couldn't find them anywhere else in stock. I'm not very familiar with electrical components or where to get them. Where would you suggest I get them where decent quality can be reasonably assured for a moderate cost? Yes, I have bought electric motor bearings off Ebay and found they were counterfeit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to chrisbc

    Hi Chris,

     

    It could be an obsolete part, I can't find it on the original component manufacturer site (On Semi).

    It is likely that an alternative replacement will have different pin ordering, and might be a different size, so you may need to be adventurous with how you physically mount it (e.g. bending wires into a different order).

    The Farnell website is currently offline, so I'll check later on for a close substitute to hopefully meet your needs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 8 years ago in reply to chrisbc

    Hi Chris,

     

    It could be an obsolete part, I can't find it on the original component manufacturer site (On Semi).

    It is likely that an alternative replacement will have different pin ordering, and might be a different size, so you may need to be adventurous with how you physically mount it (e.g. bending wires into a different order).

    The Farnell website is currently offline, so I'll check later on for a close substitute to hopefully meet your needs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • chrisbc
    0 chrisbc over 8 years ago in reply to shabaz

    It was originally made by Motorola. I found an MCR100-8 equivalent on wholesale electronics and ordered a couple. Why would they change the pin order? Is it standard practice to bend and switch pins around? Wouldn't there be a standard pin order that manufacturers follow? Thanks for the info. and the help though... I should be able to fix it from here.