element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Prototyping Male Connector
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 33 subscribers
  • Views 1608 views
  • Users 0 members are here
  • prototyping
Related

Prototyping Male Connector

nbuuck
nbuuck over 12 years ago

NOTE: As a correct answer has been received and marked, I will not be following up on further responses. Once I've measured and modeled the connector I'll happily share the drawing file here.

 

Hi all,

 

I have a personal project that needs to interface with a port that uses a physical configuration that is believed to be proprietary. To provide a stable interface with the port, I would like to prototype a male connector but I don't think I'll be able to directly measure some of the dimensions of the existing female connector because of the scale and unique configuration. Does anyone have experience with using a temporarily malleable material to create a form of a female connector so that measurements can be taken of the negative mold of the connector? Any suggestions on what materials or products might be helpful for this purpose?

 

image

 

Thanks, community!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1 verified
    Hi Nathan Contact your dentist as they have materials that will make an excellent detaled impression. They use an impression material called alginate to make impressions of prepared teeth so that they…
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Nathan Contact your dentist as they have materials that will make an excellent detaled impression. They use an impression material called alginate to make impressions of prepared teeth so that they can have a crown cast. Once you have the impression you will have a way to get your measurements.

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • nbuuck
    0 nbuuck over 12 years ago in reply to jw0752

    Interesting suggestion! Do you have any thoughts about the potential for residue to be left in the port? There's a sliding cover that recesses into the port when the male connector is inserted that seems like it has a lot of potential to collect and retain the molding material (alginate or otherwise).

     

    I'm starting to think that maybe taking a block of material the approximate size of the outer dimensions of the female connector, conservatively subtracting material based on initial measurements, and using fine subtraction from the prototype material until it adequately fits the female connector. This would allow me to minimize introducing foreign material into the female connector by thoroughly cleaning the prototype before testing for fit.

     

    Thanks for the suggestion!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • nbuuck
    0 nbuuck over 12 years ago in reply to jw0752

    Interesting suggestion! Do you have any thoughts about the potential for residue to be left in the port? There's a sliding cover that recesses into the port when the male connector is inserted that seems like it has a lot of potential to collect and retain the molding material (alginate or otherwise).

     

    I'm starting to think that maybe taking a block of material the approximate size of the outer dimensions of the female connector, conservatively subtracting material based on initial measurements, and using fine subtraction from the prototype material until it adequately fits the female connector. This would allow me to minimize introducing foreign material into the female connector by thoroughly cleaning the prototype before testing for fit.

     

    Thanks for the suggestion!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to nbuuck

    I was thinking more of some sort of program that hooks up to a camera, and you could have a data base with certain faces in it and you could add and subtract people. It could recognize certain points in your face. For example it would notice where the tip of your nose is and where the top is and measure it

     

    Sent from my iPad