element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Prototyping Male Connector
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 33 subscribers
  • Views 1595 views
  • Users 0 members are here
  • prototyping
Related

Prototyping Male Connector

nbuuck
nbuuck over 12 years ago

NOTE: As a correct answer has been received and marked, I will not be following up on further responses. Once I've measured and modeled the connector I'll happily share the drawing file here.

 

Hi all,

 

I have a personal project that needs to interface with a port that uses a physical configuration that is believed to be proprietary. To provide a stable interface with the port, I would like to prototype a male connector but I don't think I'll be able to directly measure some of the dimensions of the existing female connector because of the scale and unique configuration. Does anyone have experience with using a temporarily malleable material to create a form of a female connector so that measurements can be taken of the negative mold of the connector? Any suggestions on what materials or products might be helpful for this purpose?

 

image

 

Thanks, community!

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 12 years ago +1 verified
    Hi Nathan Contact your dentist as they have materials that will make an excellent detaled impression. They use an impression material called alginate to make impressions of prepared teeth so that they…
Parents
  • jw0752
    0 jw0752 over 12 years ago

    This material is mixed and can be injected into a cavity like your plug recepticle. Within a minute or two it turns into a rubbery solid, much like cured silicon. It usually stays together very well and if part were to be left behind you could easily remove it with a pick. I would try to enlist the dentist to help you as there is an art to injecting it and extracting it. If you have a good guy dentist he should be willing to help you. You probably do not want to buy your own material but you can ask. Thanks John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago

    This material is mixed and can be injected into a cavity like your plug recepticle. Within a minute or two it turns into a rubbery solid, much like cured silicon. It usually stays together very well and if part were to be left behind you could easily remove it with a pick. I would try to enlist the dentist to help you as there is an art to injecting it and extracting it. If you have a good guy dentist he should be willing to help you. You probably do not want to buy your own material but you can ask. Thanks John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 12 years ago in reply to jw0752

    I recall now model shops sell this stuff too, so that could be another source. I think I have some for a model I was making, but it's probably expired a couple of years ago : )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    I think you are getting the wrong idea from me. I am only a teenager new in to the electrical engineering world. I mean the most impressive thing I have done is make a light sensor with an Arduino.

    Sorry.

     

    Sent from my iPad