element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 6v motor not working as expected
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 31 subscribers
  • Views 1703 views
  • Users 0 members are here
Related

6v motor not working as expected

e14 Contributor
e14 Contributor over 11 years ago

Hi

 

This problem is hard to explain so I uploaded a short video as a visual aid:

(Sorry for the bad quality, I seem to have misplaced my HD camcorder)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I'm powering it from a 5v DC wall wart and I have an identical motor that seems to be working fine.

Does anyone know what is wrong with it?

 

Any help would be greatly appreciated!

 

Will

  • Sign in to reply
  • Cancel

Top Replies

  • saurocksall
    saurocksall over 11 years ago +1
    Hi Will, I have been playing with motors like this since childhood, it seems that the Brushes of the motor have Worn Out or are not in contact with the Commutator, or one of the three Windings are not…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to saurocksall +1
    Thanks for your reply Saurabh, I'll have a look inside later and I'll get back to you. Will
  • saurocksall
    saurocksall over 11 years ago in reply to e14 Contributor +1
    These motors are not that hard to open as they are not glued or screwed together, the plastic half slides inside the metal cover and 2 metal clips at the side, just bend those out and the plastic part…
Parents
  • jw0752
    0 jw0752 over 11 years ago

    Hi Will, Do you have a 6 volt battery you can try it on. It looks to me like the current draw of the motor is causing the wall wart to do a current overload shut down. If you can get it to spin continuously on a battery this is likely the cause. There may still be something wrong with the brushes or a partially shorted rotor winding, as suggested by Saurabh, which is causing the current overload. Usually if it they have a bad communtaor or winding they will have a dead spot where they do not start and then will spin if started manually.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 11 years ago

    Hi Will, Do you have a 6 volt battery you can try it on. It looks to me like the current draw of the motor is causing the wall wart to do a current overload shut down. If you can get it to spin continuously on a battery this is likely the cause. There may still be something wrong with the brushes or a partially shorted rotor winding, as suggested by Saurabh, which is causing the current overload. Usually if it they have a bad communtaor or winding they will have a dead spot where they do not start and then will spin if started manually.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to jw0752

    It seems you're right John, I tried it with various different batteries and the motor span continuously.

    It still doesn't explain why the wall wart was doing overload shutdowns because it was rated at 1 A which I would assume is far more than the motor requires.

     

    Thanks, Will