element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Hi Ben, long time watcher of the TBHS. Love it & you. Need Help with Raspberry pi 2 & LCD please!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 5 answers
  • Subscribers 30 subscribers
  • Views 2678 views
  • Users 0 members are here
  • raspberry
  • waveshare
  • lcd
  • spotpear
  • pi
  • 2
  • tft
  • 3.5"
Related

Hi Ben, long time watcher of the TBHS. Love it & you. Need Help with Raspberry pi 2 & LCD please!

e14 Contributor
e14 Contributor over 11 years ago

Super new to the raspberry pi scene been watching you do various projects with them and figured it would be something new and cool to check out. got my noobs installed perfect now running raspbian.

been moving along following different tutorials trying out new things.

 

I finaly got stuff working on my Raspbian good and I'm starting to get a little more comfortable doing stuff on my Pi like, 1.) Installed apache and MySQL got wordpress working. (been tinkering around with it a little) also got a working copy of minecraft server vrs.1.8.4 working on my Pi.

 

Recently wanted to make it a bit more portable.

So I bought the 3.5" TFT LCD from Waveshare spotpear.

thought it was a no brainer plug N play with the Gpio

I pretty sure it is. but I cant seem to get or find proper soft ware, & or documentation to easily install it. there was no software when I got my lcd. it told me to go to few sites which were for the older pi.

I've read through few pages of peoples post seems a lot of new and regulars on the  Pi scene are having similar problems with lcd installations.

Currently My pi is running on hdmi to tv.

 

Best Related web page related info I could find so far Is http://www.wvshare.com/product/3.5inch-RPi-LCD-A.htm

 

image

image

 

Please say you can help figure this out.

 

Also, if anyone else who reads this if you also have a raspi2 w/ the 3.5" tft lcd Waveshare Spotpear addon card let us know if you got it working right and if so let  us know what you did or didn't do, please also provide software as I have been unable to find it.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1 suggested
    I have that same screen, ordered from china off e-mail for around $20. Ill start by saying that you get what you pay for. It is not as easy to install but it works great! These instructions should get…
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    falon wrote:

     

    sudo: ts_calibrate: command not found
    is what i do when i do your command.

    Did you install the command? You can do an aptitude or apt-get to search the repos and install it. I think it is part of libts-bin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Mathew Harvey wrote:

     

    will this guide work for the 4 inch waveshare spotpear lcd I ccan get it to work on the supplied image but I want to use my propper pi image

    and I would if attall possible use hdmi and screen and if not is it possible to stop kodi or xbmc going through hdmi and use the touch screen or both

    I have never tried it on a 4in screen and I have seen it reported that xbmc will work with the 3.5". Beyond that I dont know.

     

    I use this setup (3.5" screen on a r-pi) as stand alone touch controls. For example, the one I am currently doing will be attached to an eggbot as the control panel allowing my wife to simple select the pattern she wants and go. No need for an extra computer.

     

    They are also used on 3dprinters as the control panel to run pronterface.

     

    With kdialog or gtkdialog you are write scripts that provide standard buttons on the screen and create the control panels you need for any project.

     

    As such, once these screens are installed I have no need to switch back and forth between them and the HDMI port. Though digging through google there appears to be ways to do it but you would need to mod the config some.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    falon wrote:

     

    also failing at getting my bluetooth stuff installed. I think this is probly the number 1 reason most windows users still havent moved to linux is because its not so simple to install stuff on.

     

    But after all said and done I was so happy to see my screen work at all and even happier when I finaly got it to be in the rotation I wanted. So thank you guys for your help on this.

    Falon,

     

    Congrats on getting it working!

     

    Im going to take a moment here to comment on your statement that this is probably the number 1 reason most windows users have not switched to Linux. The truth is you have jumped off into the deep end of linux. lol

     

    To put this into prospective, getting the LCD running is a PITA. I have been working with Linux for close to 25 years. Going back to the days of custom compiling everything and building the linux system by hand (Pre-Slackware 0.99), I am also a professional Linux engineer. With that in mind, it took me 5 days to figure out how to make the 3.5" screen work on the Raspberry Pi. IMHO that makes getting one of these low cost LCD's from china to work with no documentation a solid 8 on a 1 to 10 scale.

     

    Raspbery Pi's are great little units but the Linux distributions for them are not the easiest to work with.  Desktop Linux distributions like Fedora or Ubuntu are far easier to work with and far more user friendly.

     

    With that in mind, I think you are right to some extent. A lot of windows users will get something like a Raspberry pi to try Linux. Never realizing that they have jumped off into the deep end. They will then get frustrated because they dont understand it and think that all Linux is like that. To use a car analogy they try to build a kit car from the ground up and then get frustrated that it is not as easy as going to the car lot and buying a Ford or Chevy.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    ok so i installed the

     

      sudo apt-get install evtest tslib libts-bin

     

     

     

    then did update

    then rebooted

    and then did the

     

      sudo TSLIB_FBDEVICE=/dev/fb1 TSLIB_TSDEVICE=/dev/input/touchscreen ts_calibrate

     

    then got the famous

    sudo: ts_calibrate: command not found
    is what i do when i do your command.

     

    So i then googled how to install ts_calibrate,

    everything I have found so far points to the install of the libts-bin

     

    So I went to where it said /dev/input/touchscreen only to find I don't have a touchscreen directory.

    This is what i have in my /dev/input/ directory

     

    pi@rpi2-54 /dev/input $ ls
    by-id    event0  event2  event4  mice    mouse1
    by-path  event1  event3  event5  mouse0  mouse2

     

    At this point I'm stuck. so maybe you know what I should do next? or so I'm hoping.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    cyberlink,

     

    I cannot thank you enough! I was just about to give up hope before finding this thread and your instructions. After doing as you said my display is fully functional touchscreen and all! FYI for others, I have a SainSmart 3.5" TFT touchscreen and the instructions in this thread worked as is.

     

    falon - if you're somehow still searching for an answer to your calibration issue, try running ts_calibrate a few different times and each time try setting TSDEVICE as a different one of the "event" items in /dev/input. I had the same issue but once I tried event3 it worked like a charm.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<