DC to Daylight
  • Challenges & Projects
  • element14 presents
  • DC to Daylight
  • More
  • Cancel
DC to Daylight
Documents How to Control a DC Motor using Optocouplers with an H-Bridge -- DC to Daylight 18
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DC to Daylight to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 14 Oct 2022 12:04 PM Date Created
  • Last Updated Last Updated: 19 Oct 2022 7:24 AM
  • Views 222452 views
  • Likes 7 likes
  • Comments 11 comments
Related
Recommended

How to Control a DC Motor using Optocouplers with an H-Bridge -- DC to Daylight 18

In this application/project based episode, we're going to put together an H-bridge which will allow us to control the speed and direction of a DC brushed motor. An Arduino will provide the PWM pulses and direction control. We'll also use optocouplers as the interface between the H-bridge and Arduino, which will mitigate noise and potentially dangerous voltages from damaging our IO pins.

Watch the Video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Supplemental Content

  • Schematics

element14 presents

element14 presents  | About Derek  |  DC to Daylight

  • h bridge
  • how to control a dc motor
  • h-bridge
  • pwm
  • dc to daylight
  • optocouplers
  • optoisolator
  • pulse with modulation
  • motor speed controller
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • DAB
    DAB over 4 years ago

    Nice episode.

    I like the use of the optocouplers, safety first.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to bit_wrangler

    Any function or method should have proper validation / abstraction / encapsulation - good programming practice... proper input validation for each and every function or method is also key. The demo code in the video is not the best example of 'good programming practice' - the goal was really to just show how the h-bridge works. Though a good takeaway from this discussion thread: Maybe it's better in making simple demos, not with the intent of making them appear more concise on screen, but more inline with how it'd be done in the real world.

    I can't speak for other industries, but at least in semiconductor, hardware has the final say - for Semi (S2?) standards, there must be an exclusion zone and any access points must be interlocked - hardware loop with redundant lines that kills servo if the loop is broken. Both signals must transition within x number of milliseconds or servo is also powered down immediately. One of the unwritten rules is, never enter the 'zone' - because you never know what the software could do - like in the Therac-25 thing, race condition causing unexpected behavior. Good read by the way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bit_wrangler
    bit_wrangler over 4 years ago in reply to e14 Contributor

    I personally try do both - where possible. The software shouldn't tell the hardware to do something that is logically unsafe, and the hardware shouldn't assume that the software won't signal it to do something unsafe. The motion function in the sample I provided is actually a simple example of that. motion() was changed to only accept bytes, so it can rely on pwm never being out of range, and direction is handled in a switch that's completely ignoring invalid directions (the only side effect of such should be causing harmless extra 'stops'). It also doesn't rely on an external variable to keep track of current direction, so from the function's perspective, it can rely on no external actor accidentally modifying that variable.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to e14 Contributor

    Perhaps just think of Therac-25 where reliance on software over hardware interlocks was allowed in the design and the horrific consequences that followed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to beacon_dave

    Never control with software! I love it. This is a good tip for designing actual hardware that has the potential to lose the smoke.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to e14 Contributor

    I can't seem to find the lecture that I was thinking of. I thought it was part of this one by Bruce Land at Cornell Uni: 

    https://youtu.be/WlU-uIC2LNk?list=PLD7F7ED1F3505D8D5&t=1218

    but it is missing the part I was thinking of that discussed various protection methods.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to beacon_dave

    Yep. I've seen some clever approaches using additional hardware logic to prevent no-no situations... even reducing control lines. However, I didn't want to add another layer of complexity for presentation (though in this case, the software came back to bite me anyway). Maybe those additional transistors would have been a good feature after all. 

    -Derek

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 4 years ago in reply to bit_wrangler

    Ha. I cringed a little when I used int's as well, but it's a fine line - keeping a simple presentation vs. the most efficient way to write code.

    Anyway, I like your solution!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to e14 Contributor

    Do it in hardware. Don't most H bridges have an additional transistor on each side to prevent those 'magic smoke' situations from occurring?  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bit_wrangler
    bit_wrangler over 4 years ago in reply to e14 Contributor

    const byte FWD = 0;
    const byte REV = 1;
    
    const byte H1 = 3; // PWM pin 3
    const byte H2 = 5; // PWM pin 5
    const byte L1 = 6; // PWM pin 6
    const byte L2 = 9; // PWM pin 9
    
    const unsigned long DWELLTIME = 2000; // time mS to hold at max speed
    const unsigned long PWMSTPTIME = 10; // mS delay between PWM changes
    const unsigned long STOPTIME = 25; // mS delay between direction changes
    const byte PWMMAXVAL = 255; // 8-bit PWM so 0 - 255
    
    
    byte direction = FWD;
    
    
    void stop() {
      analogWrite(H1, 0);
      analogWrite(H2, 0);
      analogWrite(L1, 0);
      analogWrite(L2, 0);
      delay(STOPTIME);
    }
    
    void motion(const byte dir, const byte duty) {
      static byte current_dir = 2; // keep track of current h-bridge direction, initialized to invalid state
    
      // Check for direction change (or first execution)
      if(dir != current_dir){
        stop();
        current_dir = dir;
      }
      
      switch(dir){
        case FWD:
          analogWrite(H1, duty);
          analogWrite(L2, duty);
         break;
        case REV:
          analogWrite(H2, duty);
          analogWrite(L1, duty);
          break;
      }
    }
    
    void ramp_pwm(const byte start, const byte end){
      if(start == end) return;
      const short step = end > start ? 1 : -1;
      
      // ramp profile
      for(short pwmvalue=start; pwmvalue != end; pwmvalue += step){
        motion(direction, pwmvalue);
        delay(PWMSTPTIME);
      }
    }
    
    void setup() {
      Serial.begin(9600);
    }
    
    void loop() {
    
      // ramp up profile
      ramp_pwm(0, PWMMAXVAL);
    
      // dwell in plateau
      delay(DWELLTIME);
    
      // ramp down profile
      ramp_pwm(PWMMAXVAL, 0);
    
      // swap direction
      direction ^= 1;
    }

    Something like this, maybe.
    I tried to keep it relatively simple, but my sensibilities scream about using int when it's not necessary (or non-stdint types for that matter, but I compromised).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>