element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Suggestions For Creating Video Content
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 8 answers
  • Subscribers 145 subscribers
  • Views 3269 views
  • Users 0 members are here
  • element14 community
  • element14 presents
Related

Suggestions For Creating Video Content

ninjatrent
ninjatrent over 6 years ago

Hello Element 14 Community!

 

My name is Trent and I would like to know what your suggestions are for creating video content in the E14 Community.

 

What kind of video capture equipment do you use?

Which editing software and methods would you recommend?

 

Most of the video content that I've previously shared has been captured with a smartphone camera.

 

While the smartphone method works for some instances, it's not very good with hands-free  video capture.

 

 

I recently purchased a Logitech C930e USB Webcam and tripod. This webcam has performed exceptionally well in my tests with Windows10 PC and the Win10 Camera Software. This software  limhas it's limitations and I would really like to find methods that offer more control in capture format and encoding (preferably open source and/or free).

 

I'm also interested in learning methods of capturing video screenshots from Win10, adding voice audio from separate microphone sources, and any other tip that you can recommend for producing the next E14

 

 

Thank you for your time.

 

Trent

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +7 verified
    Hi Trent, There's a thread here that's got some suggestions: Tips for recording screen and camera A smartphone works fine, but any camera and desk clamp or tripod will be good too. And then transfer across…
  • dougw
    dougw over 6 years ago +6 suggested
    I am firmly in the cheap, easy camp when it comes to video production. I do have a decent camera though (Panasonic FZ1000) which can do time lapse photography and 4K video. I use CamStudio for capturing…
  • shabaz
    shabaz over 6 years ago in reply to BigG +5 suggested
    I found the audio most difficult too : ( I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great reviews,…
  • Sean_Miller
    Sean_Miller over 6 years ago +4 suggested
    Nowadays, smartphones can be very competitive in quality to video cameras and they are definitely easier to use. In fact, the major movie release Unsane was filmed entirely on a iPhone 7 plus. It's gotten…
  • BigG
    BigG over 6 years ago +4 suggested
    I would second shabaz 's suggestion that you should read through the " Tips for recording screen and camera ". Within that thread https://obsproject.com/ is mentioned. I took up that suggestion and I must…
  • robogary
    robogary over 6 years ago in reply to Sean_Miller +4 suggested
    Hi Trent, E14 does not present media arts academy awards, quick understandable content is most valuable to viewers. My perspective for E14 videos: decide on your target audience capability and include…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +4 suggested
    shabaz wrote: I found the audio most difficult too : ( I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great…
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps +4 suggested
    I used to have one of those for web-conferences. I didn't think of trying that, that's a good idea. For now I'm happy with the Zoom method, it meets my needs. Hehe yeah the speaking louder is a real solution…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dougw +3 suggested
    I'm using a subset of dougw . I take care that audio is good. Video not so much. For capturing screen action, I also use CamStudio. I try to speak real-time, using a headset with good microphone. If I…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Trent,

     

    There's a thread here that's got some suggestions: Tips for recording screen and camera

    A smartphone works fine, but any camera and desk clamp or tripod will be good too. And then transfer across the photos/videos using SD card etc.. Maybe webcam is not needed, since a camera doesn't cost that much extra (e.g. IXUS seems low-cost). Also, the small cameras often have good macro capability, so you get a multi-purpose tool with that.

     

    To me, there seems to be at least two categories of video creation/editing methods.

    Method 1: Requires you to set up sources, and then record.

    Method 2: Requires you to (a) independently record your material, and then (b) later rearrange it all in a timeline view.

     

    The method I use is Method 2. For part (a), I'll use a camera for photos/video, and Snagit for desktop screenshots and video captures. For part (b) rearranging it in a timeline view, I use Camtasia.

    For me the main benefit is that Camtasia is easy to use (it is like a dumbed-down video editing system). Once you have your previously recorded material (from anywhere - can include photos, video, audio etc) you have a timeline, and you can drag any content to it, and cut and rearrange and overlay and resize as necessary, and do fade ins/outs/mixes etc to any previously recorded audio too. Camtasia cannot do high-end audio/video effects, only basic stuff. The main disadvantage is the cost (more expensive than I wish it was, but at least it's cheaper and easier to use than Adobe etc). There's a list of other timeline-based tools here: https://en.wikipedia.org/wiki/List_of_video_editing_software

     

    Sometimes for part (a) I'll use Audacity to mess with audio, but I find its interface to be confusing. There is a better 'Cool Edit' which I have an ancient (maybe Windows 95 era? but it still runs on Windows 10) license for, so I'll use that more often. It is not available any more though (Adobe took it and made a more complicated and expensive subscription version)... you can see my pattern : ) Cool Edit was a dumbed-down audio editing piece of software too : )

     

    Example below.. The lower half contains the timeline, and the top-left portion has the source media files, which were dragged to the timeline. You can see the audio is on track 4 (some basic stuff can be done to it, like amplify or fade-in our out, using the Audio Effects menu on the left-side palette). The video is on track 1 mostly it seems, as well as some screen capture on track 1 with the name code1. There is a Transitions menu item on the left that can be used for video, and any chosen effect is dragged onto the timeline in the desired location. The other tracks for this project just contain random bits of overlaid text or arrows or boxes, etc. I don't have any set pattern that I use.

     

    image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi Trent,

     

    There's a thread here that's got some suggestions: Tips for recording screen and camera

    A smartphone works fine, but any camera and desk clamp or tripod will be good too. And then transfer across the photos/videos using SD card etc.. Maybe webcam is not needed, since a camera doesn't cost that much extra (e.g. IXUS seems low-cost). Also, the small cameras often have good macro capability, so you get a multi-purpose tool with that.

     

    To me, there seems to be at least two categories of video creation/editing methods.

    Method 1: Requires you to set up sources, and then record.

    Method 2: Requires you to (a) independently record your material, and then (b) later rearrange it all in a timeline view.

     

    The method I use is Method 2. For part (a), I'll use a camera for photos/video, and Snagit for desktop screenshots and video captures. For part (b) rearranging it in a timeline view, I use Camtasia.

    For me the main benefit is that Camtasia is easy to use (it is like a dumbed-down video editing system). Once you have your previously recorded material (from anywhere - can include photos, video, audio etc) you have a timeline, and you can drag any content to it, and cut and rearrange and overlay and resize as necessary, and do fade ins/outs/mixes etc to any previously recorded audio too. Camtasia cannot do high-end audio/video effects, only basic stuff. The main disadvantage is the cost (more expensive than I wish it was, but at least it's cheaper and easier to use than Adobe etc). There's a list of other timeline-based tools here: https://en.wikipedia.org/wiki/List_of_video_editing_software

     

    Sometimes for part (a) I'll use Audacity to mess with audio, but I find its interface to be confusing. There is a better 'Cool Edit' which I have an ancient (maybe Windows 95 era? but it still runs on Windows 10) license for, so I'll use that more often. It is not available any more though (Adobe took it and made a more complicated and expensive subscription version)... you can see my pattern : ) Cool Edit was a dumbed-down audio editing piece of software too : )

     

    Example below.. The lower half contains the timeline, and the top-left portion has the source media files, which were dragged to the timeline. You can see the audio is on track 4 (some basic stuff can be done to it, like amplify or fade-in our out, using the Audio Effects menu on the left-side palette). The video is on track 1 mostly it seems, as well as some screen capture on track 1 with the name code1. There is a Transitions menu item on the left that can be used for video, and any chosen effect is dragged onto the timeline in the desired location. The other tracks for this project just contain random bits of overlaid text or arrows or boxes, etc. I don't have any set pattern that I use.

     

    image

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer