element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Suggestions For Creating Video Content
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 8 answers
  • Subscribers 145 subscribers
  • Views 3269 views
  • Users 0 members are here
  • element14 community
  • element14 presents
Related

Suggestions For Creating Video Content

ninjatrent
ninjatrent over 6 years ago

Hello Element 14 Community!

 

My name is Trent and I would like to know what your suggestions are for creating video content in the E14 Community.

 

What kind of video capture equipment do you use?

Which editing software and methods would you recommend?

 

Most of the video content that I've previously shared has been captured with a smartphone camera.

 

While the smartphone method works for some instances, it's not very good with hands-free  video capture.

 

 

I recently purchased a Logitech C930e USB Webcam and tripod. This webcam has performed exceptionally well in my tests with Windows10 PC and the Win10 Camera Software. This software  limhas it's limitations and I would really like to find methods that offer more control in capture format and encoding (preferably open source and/or free).

 

I'm also interested in learning methods of capturing video screenshots from Win10, adding voice audio from separate microphone sources, and any other tip that you can recommend for producing the next E14

 

 

Thank you for your time.

 

Trent

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +7 verified
    Hi Trent, There's a thread here that's got some suggestions: Tips for recording screen and camera A smartphone works fine, but any camera and desk clamp or tripod will be good too. And then transfer across…
  • dougw
    dougw over 6 years ago +6 suggested
    I am firmly in the cheap, easy camp when it comes to video production. I do have a decent camera though (Panasonic FZ1000) which can do time lapse photography and 4K video. I use CamStudio for capturing…
  • shabaz
    shabaz over 6 years ago in reply to BigG +5 suggested
    I found the audio most difficult too : ( I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great reviews,…
  • Sean_Miller
    Sean_Miller over 6 years ago +4 suggested
    Nowadays, smartphones can be very competitive in quality to video cameras and they are definitely easier to use. In fact, the major movie release Unsane was filmed entirely on a iPhone 7 plus. It's gotten…
  • BigG
    BigG over 6 years ago +4 suggested
    I would second shabaz 's suggestion that you should read through the " Tips for recording screen and camera ". Within that thread https://obsproject.com/ is mentioned. I took up that suggestion and I must…
  • robogary
    robogary over 6 years ago in reply to Sean_Miller +4 suggested
    Hi Trent, E14 does not present media arts academy awards, quick understandable content is most valuable to viewers. My perspective for E14 videos: decide on your target audience capability and include…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +4 suggested
    shabaz wrote: I found the audio most difficult too : ( I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great…
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps +4 suggested
    I used to have one of those for web-conferences. I didn't think of trying that, that's a good idea. For now I'm happy with the Zoom method, it meets my needs. Hehe yeah the speaking louder is a real solution…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dougw +3 suggested
    I'm using a subset of dougw . I take care that audio is good. Video not so much. For capturing screen action, I also use CamStudio. I try to speak real-time, using a headset with good microphone. If I…
Parents
  • dougw
    0 dougw over 6 years ago

    I am firmly in the cheap, easy camp when it comes to video production.

    I do have a decent camera though (Panasonic FZ1000) which can do time lapse photography and 4K video.

    I use CamStudio for capturing screen activity.

    I use Adacity for editing audio tracks.

    I use Microsoft MovieMaker to edit VLOGs - add video, transitions, still images, captions, audio, etc.

    The most important things are:

    • use a tripod for the camera
    • use lots of high temperature lighting
    • get a decent microphone and position it properly (I use cheap mics, but at least I can position them close to my face )
      • I use a low-cost headset with my camera (because it is mono) that puts the mic consistently close to my mouth
      • I use a Soonhua SH-666 mic when adding voice-over with Moviemaker (<$10)
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to dougw

    I'm using a subset of dougw. I take care that audio is good. Video not so much.

     

    • For capturing screen action, I also use CamStudio. I try to speak real-time, using a headset with good microphone. If I want to show action at the same time, I put an IP Camera Viewer window on the captured desktop showing a webcam pointing at the device under test.
    • To capture live action, I use either an iPad or a smartphone, filming out of my hand (no tripod or other fixture), I plug that same headset into the iPad or phone.
    • I try to do as much as I can in a single shot, to avoid editing effort later.
    • Then I use the standard Microsoft Movie Maker to edit the result. I try to use as little cutting as possible. I use a fast animation (Bars, duration 0.25 to 0.75) to smoothen the cuts and avoid jumping video boundaries.
    • Where needed, I make Captions to point out details, and Narration for overdubs.
    • Then I generate the output for high definition, 1920 x 1080, 24000 bitrate, 29.97 fps.audio 192 kbps, 48 Hz, stereo (lord knows why I use stereo when recording with a single mono mike)
    • I upload to youtube and use the e14 embed function if I want to have the video here. I never load the video to e14 because the player handles youtube videos better than uploaded ones
    • I have an automatic sync with LBRY.tv just to annoy youtube.

    Example showing shaky video out of hand, + desktop and webcam together:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

     

    Edit: heres the editing for the video above (click to enlarge).

    image

    I did overdub the talk over the CamStudio capture. Most likely because my initial talk did not catch op with the LabVIEW automation at real time ...

    The cuts are at 0:30, 0:36, 0:39 (video only to reduce video length, the audio is continuous) and 0:53

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to dougw

    I'm using a subset of dougw. I take care that audio is good. Video not so much.

     

    • For capturing screen action, I also use CamStudio. I try to speak real-time, using a headset with good microphone. If I want to show action at the same time, I put an IP Camera Viewer window on the captured desktop showing a webcam pointing at the device under test.
    • To capture live action, I use either an iPad or a smartphone, filming out of my hand (no tripod or other fixture), I plug that same headset into the iPad or phone.
    • I try to do as much as I can in a single shot, to avoid editing effort later.
    • Then I use the standard Microsoft Movie Maker to edit the result. I try to use as little cutting as possible. I use a fast animation (Bars, duration 0.25 to 0.75) to smoothen the cuts and avoid jumping video boundaries.
    • Where needed, I make Captions to point out details, and Narration for overdubs.
    • Then I generate the output for high definition, 1920 x 1080, 24000 bitrate, 29.97 fps.audio 192 kbps, 48 Hz, stereo (lord knows why I use stereo when recording with a single mono mike)
    • I upload to youtube and use the e14 embed function if I want to have the video here. I never load the video to e14 because the player handles youtube videos better than uploaded ones
    • I have an automatic sync with LBRY.tv just to annoy youtube.

    Example showing shaky video out of hand, + desktop and webcam together:

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

     

    Edit: heres the editing for the video above (click to enlarge).

    image

    I did overdub the talk over the CamStudio capture. Most likely because my initial talk did not catch op with the LabVIEW automation at real time ...

    The cuts are at 0:30, 0:36, 0:39 (video only to reduce video length, the audio is continuous) and 0:53

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer