element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Suggestions For Creating Video Content
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 8 answers
  • Subscribers 145 subscribers
  • Views 3269 views
  • Users 0 members are here
  • element14 community
  • element14 presents
Related

Suggestions For Creating Video Content

ninjatrent
ninjatrent over 6 years ago

Hello Element 14 Community!

 

My name is Trent and I would like to know what your suggestions are for creating video content in the E14 Community.

 

What kind of video capture equipment do you use?

Which editing software and methods would you recommend?

 

Most of the video content that I've previously shared has been captured with a smartphone camera.

 

While the smartphone method works for some instances, it's not very good with hands-free  video capture.

 

 

I recently purchased a Logitech C930e USB Webcam and tripod. This webcam has performed exceptionally well in my tests with Windows10 PC and the Win10 Camera Software. This software  limhas it's limitations and I would really like to find methods that offer more control in capture format and encoding (preferably open source and/or free).

 

I'm also interested in learning methods of capturing video screenshots from Win10, adding voice audio from separate microphone sources, and any other tip that you can recommend for producing the next E14

 

 

Thank you for your time.

 

Trent

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +7 verified
    Hi Trent, There's a thread here that's got some suggestions: Tips for recording screen and camera A smartphone works fine, but any camera and desk clamp or tripod will be good too. And then transfer across…
  • dougw
    dougw over 6 years ago +6 suggested
    I am firmly in the cheap, easy camp when it comes to video production. I do have a decent camera though (Panasonic FZ1000) which can do time lapse photography and 4K video. I use CamStudio for capturing…
  • shabaz
    shabaz over 6 years ago in reply to BigG +5 suggested
    I found the audio most difficult too : ( I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great reviews,…
  • Sean_Miller
    Sean_Miller over 6 years ago +4 suggested
    Nowadays, smartphones can be very competitive in quality to video cameras and they are definitely easier to use. In fact, the major movie release Unsane was filmed entirely on a iPhone 7 plus. It's gotten…
  • BigG
    BigG over 6 years ago +4 suggested
    I would second shabaz 's suggestion that you should read through the " Tips for recording screen and camera ". Within that thread https://obsproject.com/ is mentioned. I took up that suggestion and I must…
  • robogary
    robogary over 6 years ago in reply to Sean_Miller +4 suggested
    Hi Trent, E14 does not present media arts academy awards, quick understandable content is most valuable to viewers. My perspective for E14 videos: decide on your target audience capability and include…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +4 suggested
    shabaz wrote: I found the audio most difficult too : ( I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great…
  • shabaz
    shabaz over 6 years ago in reply to Jan Cumps +4 suggested
    I used to have one of those for web-conferences. I didn't think of trying that, that's a good idea. For now I'm happy with the Zoom method, it meets my needs. Hehe yeah the speaking louder is a real solution…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to dougw +3 suggested
    I'm using a subset of dougw . I take care that audio is good. Video not so much. For capturing screen action, I also use CamStudio. I try to speak real-time, using a headset with good microphone. If I…
Parents
  • BigG
    0 BigG over 6 years ago

    I would second shabaz's suggestion that you should read through the "Tips for recording screen and camera".

     

    Within that thread https://obsproject.com/  is mentioned.

     

    I took up that suggestion and I must say it works very well for my needs. In particular, it provides a means for capturing video screenshots from Win10, adding voice audio from separate microphone sources and it also can grab visuals from windows applications rather than just the video monitor.

     

    I still find that the microphone (or getting nice audio) is the biggest headache. So I rather like Sean's suggestion.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • BigG
    0 BigG over 6 years ago

    I would second shabaz's suggestion that you should read through the "Tips for recording screen and camera".

     

    Within that thread https://obsproject.com/  is mentioned.

     

    I took up that suggestion and I must say it works very well for my needs. In particular, it provides a means for capturing video screenshots from Win10, adding voice audio from separate microphone sources and it also can grab visuals from windows applications rather than just the video monitor.

     

    I still find that the microphone (or getting nice audio) is the biggest headache. So I rather like Sean's suggestion.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 6 years ago in reply to BigG

    I found the audio most difficult too : (

    I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great reviews, and they were both pretty bad (for me) - I speak quietly, so the signal-noise was terrible. Either that, or I was too picky..

    There was so much hiss, and Audacity clean-up is quite rotten.

     

    Next on the journey I tried two handheld mics (Sennheiser) and two brands of lapel mics (Sennheiser and one I can't recall), but the recommendations from a couple of audio experts was in the $$$$ mic range! : ) so I tried some friendlier-priced dynamic mics (Sennheiser again) - only to realize that most consumer music audio interfaces (like Focusrite) that are in the $100 or so bracket, only have good SNR with low gain - they don't provide specs at the higher gain settings for the cheaper interfaces : ) and no good for dynamic mics.( I don't do much audio of myself facing the camera, so the lapel mic wasn't as essential for me.

     

    Anyway, this was all turning out to be a terrible time-waste and money sink. I almost gave up. Surprisingly, the best value-for-money thing for me turned out to be the sub-$100 all-in-one Zoom H1N, i.e. has an in-built mic. I still have to speak deliberately louder slightly, but finally I was reasonably happy with it. It is quite small - fits in a small pencil-case incidentally - not that that matters.

     

    I used it a lot. My little nephew liked it, so after a year or so I gave it away to him (so he can act as a football match reporter and interview his younger brother each time he misses a goal in the garden), and bought a more expensive Zoom product, but it wasn't perceptibly better. In comparison I feel the lower-cost H1N was the better product for easy audio recording, so if I had to do it all again, I'd just get that. The H1N is handheld, but has a thread for a stand (or can use a mobile phone angle stand, which is nice).

     

    Also, maybe Youtube audio processing has improved too - compared to a couple of years ago, today if stuff is recorded with slightly poorer quality sound, it seems to sound better after a few hours on Youtube (this is subjective, I've not really investigated). So maybe it is becoming less important to faff so much on the audio side : ).

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 6 years ago in reply to shabaz

    shabaz  wrote:

     

    I found the audio most difficult too : (

    I tried several USB mics (some Audio Technica one, and a blue Yeti? was silver colored..) that were advertised as Youtube-creation friendly with great reviews, and they were both pretty bad (for me) - I speak quietly, so the signal-noise was terrible. Either that, or I was too picky..

    There was so much hiss, and Audacity clean-up is quite rotten.

    ...

    If your computer supports audio in, an old-school headset-with-micro (the ones that hava an extra contact on the connector for audio) can do a better job than a usb microphone.

    This is the very cheap one I use: a Trust from a discounter shop.

     

    image

     

    I've forced myself to speak louder while recording - without shouting. It helps reduce hiss and get better pronunciation (you don't mumble when you force yourself a level higher). The downside is that it can sound a little forced.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to Jan Cumps

    I used to have one of those for web-conferences. I didn't think of trying that, that's a good idea. For now I'm happy with the Zoom method, it meets my needs. Hehe yeah the speaking louder is a real solution : )

    I forgot to add one more product I attempted along the journey to the list.. a Panasonic USB handheld mic for dictation.. no good, but probably fantastic for its intended purpose though! : )

    This video is unavailable.
    You don't have permission to edit metadata of this video.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer