element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Episode 607 Reboot request
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 63 replies
  • Subscribers 140 subscribers
  • Views 9036 views
  • Users 0 members are here
Related

Episode 607 Reboot request

Mikeatencio
Mikeatencio over 1 year ago

/challenges-projects/element14-presents/project-videos/w/documents/28198/from-strava-to-motion-creating-an-arduino-powered-arcade-game-with-running-data----episode-607

I included the episode for context. Can someone please recreate this project for horse racing like the carnival arcades instead of the STAVA Lorraine created? I would truly enjoy making this now that I am retired. Thanks

Mike 

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +3
    I recall colporteur created a project 14 entry based on PWM locomotive motor control about 3 years ago as part of the world in motion competition and won a prize. I think it will have some similarities…
  • beacon_dave
    beacon_dave over 1 year ago +2
    You may need to start by sharing some pictures of the version of the game that you are after creating, as they vary quite a bit. Over here in my youth it was known as the 'Donkey Derby' but that I believe…
  • beacon_dave
    beacon_dave over 1 year ago +2
    If you still want to use a pinball mechanism, then perhaps look at the Ben Heck Show episode archive, as he built a number of pinball machines from scratch.
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +2
    Well that was a quick and easy decision... You can get GPIO expanders if you run out or you can just add another microcontroller, like has been done here where 200 buttons are being used: https://www…
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave +1
    I recall that some were based on linear tracks like Lorrainbow's Strava version whereas some were based on oval tracks. Size varied a lot as well from the large arcade versions like this Blackpool Pier…
  • michaelkellett
    michaelkellett over 1 year ago in reply to Mikeatencio +1
    I would have had a look but you can't see much at all without signing in an creating an account - but they want you to pay before you can access the 14 day free account. I won't pay money to a supplier…
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave +1
    I recall SparkFun did a corn hole board game with a LED light strip in the hole the corn bag drops through Sketch Up SparkFun Corn Hole Lorrainbow also did a BasketBall hoop using a colour sensor …
  • michaelkellett
    michaelkellett over 1 year ago in reply to Mikeatencio +1
    No need to apologise - it's not you being a muppet ! MK
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +1
    Mikeatencio said: 6 foot long. For 12 players then a 6' long track might be a bit on the short side. If you have 6 players either side then that only leaves 1' per player. Might be worth considering…
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio +1
    I think you are going to be around 2' shoulder width, then you need extra for the elbow movement when picking and rolling the balls. One way to maximize space may be to make it dodecagonal as that way…
Parents
  • beacon_dave
    beacon_dave over 1 year ago

    You may need to start by sharing some pictures of the version of the game that you are after creating, as they vary quite a bit.

    Over here in my youth it was known as the 'Donkey Derby' but that I believe that was a copy of George Valentine Tonner's 'Kentucky Derby' game. Some had animatronic horses on a Scalextric type track whereas some were pulled along by ropes wrapped around pulleys more like Lorrainbow's design. Some were controlled by rolling balls into pockets, and others by tapping switches alternately. Horses have been replaced by camels and rabbits as well.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Mikeatencio
    Mikeatencio over 1 year ago in reply to beacon_dave

    Yes, my youth was filled with the same thing. Oh those were great times. Now we have n inept moron running our country. I presume you are in the UK?

    What I really want is based on George Valentine Tonner's Kentucky Derby. I played that at the fairgrounds every year with my mom.

    With Arduinos and programmable RGB's, it would be easy to have the lights advance instead of mechanical horses. I could use a laser cutter to cut out the horses in a row and cover them with colored plastic.

    The lights would be behind the cutout illuminating the horses as they advance. They would advance when the ball hits one of three switches to gain points. 

    The patent was quite brilliant on your part. As my friend would say "I'm chuffed!" I think that's the correct saying. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 1 year ago in reply to Mikeatencio

    We managed to leave politics off this forum. Let's keep it focused on engineering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    Yes, UK. 

    LEDs would be a lot easier than a mechanical solution, but perhaps not so good in daylight. It would also limit the resolution of the track to the number of horse cut-outs. A 3" long horse on a 6' track would give you 24 positions from start to finish whereas a mechanical version would give you near infinite positions. Depends if you want to scale the game play on the number of points collected or on the distance travelled per point.

    With an Arduino controlling this you could have penalty/bonus options appear on certain pockets that speed up or slow down the movement of the player's horse. Perhaps borrow some of the game play features from pinball games to spice it up a bit. If you light the legs separately from the rest of the horse you could perhaps flash them red to indicate an injury penalty is active.

    Were you thinking of a single row of horses being lit with different colours to indicate player position or multiple rows with a row for each player ? 

    If you use clear plastic for the horses you could try edge lighting the horses from below. Can work well with engraving.

    You could use RGB LED rings around the pockets to provide animation and game play feedback.

    I've seen some of the horse cars up for sale from the original carnival games, which would just require a Scalextric type track to run them on. They may be a bit on the large side.   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    Yes, UK. 

    LEDs would be a lot easier than a mechanical solution, but perhaps not so good in daylight. It would also limit the resolution of the track to the number of horse cut-outs. A 3" long horse on a 6' track would give you 24 positions from start to finish whereas a mechanical version would give you near infinite positions. Depends if you want to scale the game play on the number of points collected or on the distance travelled per point.

    With an Arduino controlling this you could have penalty/bonus options appear on certain pockets that speed up or slow down the movement of the player's horse. Perhaps borrow some of the game play features from pinball games to spice it up a bit. If you light the legs separately from the rest of the horse you could perhaps flash them red to indicate an injury penalty is active.

    Were you thinking of a single row of horses being lit with different colours to indicate player position or multiple rows with a row for each player ? 

    If you use clear plastic for the horses you could try edge lighting the horses from below. Can work well with engraving.

    You could use RGB LED rings around the pockets to provide animation and game play feedback.

    I've seen some of the horse cars up for sale from the original carnival games, which would just require a Scalextric type track to run them on. They may be a bit on the large side.   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Mikeatencio
    Mikeatencio over 1 year ago in reply to beacon_dave

    Oh yeah. I like lighting the holes. There are 12 rows of horse for 12 players. I can make horses smaller to add more. That's easy enough. Penalty holes would make it interesting but it would take longer to play.

    The Scalextric idea sounds fun for a home or carnival game but how would I get the horse to move a specific segment and start or end with a winner?  How would that work?

    I can build a slot car track from scratch. I have a track here. If you're interested,  I would like to explore this idea using the HO scale track and I'll create the horse miniatures for it. Thanks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio

    If you look at the original rabbit design patent it had a segmented power rail which was energised by a rotary switch turned by the balls. The motor would run until the end of the energised segment whereby it would lose power until the next segment was energised.

    You could use a timer in the microcontroller to energise the track for a certain period of time. However motors tend not to run the same so you may need to calibrate them a bit. This could be automated by timing the length of time it takes for each horse to run the length of the track and then adjust the timing to make them all match the slowest horse. A bit of randomness in this type of game is perhaps not a bad thing as real world horses run at different speeds.

    You could make the horses more intelligent so that the wheels have feedback sensors so they only turn a certain number of times for each segment when the track is energised. Although this wouldn't account for traction slippage. You get motors with built-in encoders.

    You could put feedback sensors into the track so the microcontroller will know when a segment has been completed and remove the power.

    You could use a sensor to measure the distance from the start line / end line to the horse and energise the track until a set distance has been reached. Time of flight might work if you can find one of a suitable range for your track (50mm to 1200mm Could use both start and finish sensors to double the range).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio
    Mikeatencio said:
    I can build a slot car track from scratch. I have a track here. If you're interested,  I would like to explore this idea using the HO scale track and I'll create the horse miniatures for it.

    This might be a fairly quick way to get going as I expect you can buy the ready-made slot car chassis and then 3D print the horse to go on top at an appropriate scale.

    Looks like you can get some electronics for them as well, which may be a quick way to make for more advanced control.

    Perhaps start off by looking out for projects involving interfacing slot cars with Arduino. Here is one using hall effect sensors around the track to detect the position of the car to trigger a change in speed: Playing Slot Cars Against an Arduino   

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio
    Mikeatencio said:
    Oh yeah. I like lighting the holes.

    You can get these light rings off-the-shelf NeoPixel Ring - 24 x 5050 RGB LED with Integrated Drivers just need to match the inner hole diameter to the ball diameter.

    A RGB pixel string might be better though as you can just drill holes around the pocket and insert the LEDs from behind.

    Alternatively, make your own custom PCB to the required diameter and use discrete RGB pixel LEDs.

    Balls are going to be rolling over these LEDs into the pockets so some degree of protection well likely be required.

    Alternatively use RGB pixel strip in silicon sleeve and line the hole cut-out with it NeoPixel RGB Neon-like LED Flex Strip with Silicone Tube - 1 meter These silicon sleeves will tend to diffuse the light so you get more of a diffuse neon glow than individual dot light effect.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to beacon_dave

    I recall SparkFun did a corn hole board game with a LED light strip in the hole the corn bag drops through

     Sketch Up SparkFun Corn Hole

    Lorrainbow also did a BasketBall hoop using a colour sensor  
    /challenges-projects/element14-presents/project-videos/w/documents/27881/how-to-make-a-basketball-auto-score-keeper-using-colour-sensing----episode-579

    so if you were to use coloured balls then you could perhaps do bonus points for matching ball and light ring colour with the light rings changing colour based on game play.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 1 year ago in reply to Mikeatencio
    Mikeatencio said:
    I can build a slot car track from scratch. I have a track here.

    I think I recall seeing that standard 2-lane HO track is around 3" wide, so for 12 lanes then probably looking at around 18" total ?

    How are the power taps normally done for those larger tracks ? Just wires soldered directly to the underside of the track ?