element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum DIY Discrete Logic LED Countdown Timer
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 142 subscribers
  • Views 4227 views
  • Users 0 members are here
  • automation
Related

DIY Discrete Logic LED Countdown Timer

evo
evo over 1 year ago

Hey everyone, I'm trying to create a countdown system, but I'm having trouble understanding how everything works together. I'm not really sure how to chain the parts properly. Could someone please show me a clear schematic or example of how to connect everything step by step?

  • Sign in to reply
  • Cancel

Top Replies

  • beacon_dave
    beacon_dave over 1 year ago +3 suggested
    I'm assuming that you are referring to the element 14 Presents timer project ? /challenges-projects/element14-presents/project-videos/w/documents/5402/diy-discrete-logic-led-countdown-timer----episode…
  • beacon_dave
    beacon_dave over 1 year ago +2
    Start with the clock circuit: and connect the 1Hz output (top right) to the Clk input (middle left) of the 1's counter: Then connect the CarryOut (lower right) to the Clk input (upper middle left…
  • evo
    evo over 1 year ago in reply to beacon_dave +1
    do you know what the full one is with everyting
  • beacon_dave
    beacon_dave over 1 year ago in reply to evo +1
    Yes, but I think you need to remove the reset logic on the 1's counter for the minutes and the 1's counter for the hours as they will need to show 0-9 and not 0-5.
  • beacon_dave
    beacon_dave over 1 year ago in reply to evo +1
    It looks like you are almost there. It is perhaps time to start building a prototype on some breadboard to help understand the circuit. If you start with one decade counter connected to one display driver…
Parents
  • beacon_dave
    0 beacon_dave over 1 year ago

    Start with the clock circuit:
    image

    and connect the 1Hz output (top right) to the Clk input (middle left) of the 1's counter:

    image

    Then connect the CarryOut (lower right) to the Clk input (upper middle left) on the 10's counter:

    image

    The cascade connection between the two counters is shown here:

    image

    To add the preset option you need to insert the switches between the clock 1Hz output and the 1's counter, and the carry out of the 1's counter and the clock input of the 10's counter as shown here:

    image

    which disconnects it from automatic clock operation and allows you to clock it manually with the push buttons.

    Note that the display digits are in the reverse order here. The 1's counter display is shown on the left on the schematic whereas in the physical world it will be positioned on the right.   

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evo
    0 evo over 1 year ago in reply to beacon_dave

    imagelike this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 1 year ago in reply to evo

    Yes, but I think you need to remove the reset logic on the 1's counter for the minutes and the 1's counter for the hours as they will need to show 0-9 and not 0-5.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evo
    0 evo over 1 year ago in reply to beacon_dave

    is that binairy?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 1 year ago in reply to evo

    BCD (binary coded decimal).

    The  JAM1-JAM4 pins set the value you want to reset the decade counter to, so in this case it has been set to the value of 0101 (5 decimal).

    The reset is triggered by the combinational logic attached to the counter outputs Q1-Q4.

    When ( Q2 AND Q3 are high ) OR when Q4 is HIGH the counter is reset.

    The logic added will therefore reset the counter to 5 whenever the counter outputs a value of 6,7,8, or 9.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evo
    0 evo over 1 year ago in reply to beacon_dave

    image

    is this good?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • evo
    0 evo over 1 year ago in reply to beacon_dave

    image

    is this good?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • beacon_dave
    0 beacon_dave over 1 year ago in reply to evo

    You probably want the switches on all 6 counters so that you can set each individually.

    You have too much reset logic. Only the 2nd, 4th (and potentially 5th and 6th) counter needs it.

    image
    The 1st counter (seconds units) drives the last digit so it needs to be able to count from 9 down to 0
    The 2nd counter (seconds tens) drives the second last digit so needs to count from 5 down to 0 so needs the reset logic.

    image

    Same with the minutes counters.   

    image

    What is the maximum number of hours are you wanting to count down from as that will affect the reset logic. No logic and it will count down from max of 99hours.  

    The same logic for the minutes and seconds and it will count down from max of 59hours.

    image

    but you could change the reset logic to make it from max of whatever you want.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evo
    0 evo over 1 year ago in reply to beacon_dave

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 1 year ago in reply to evo

    Where you have removed the logic you probably want to pull the preset enable pin low rather than leave it floating

    image

    as per the original schematic

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • evo
    0 evo over 1 year ago in reply to beacon_dave

    heb je easyeda, ik ben nog vrij nieuw bij al dit dus zou je mischien kunnen helpen met het maken van alles, je kan ook altijd de webversie gebruiken

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave over 1 year ago in reply to evo

    It looks like you are almost there. It is perhaps time to start building a prototype on some breadboard to help understand the circuit.

    If you start with one decade counter connected to one display driver you can clock it manually using the switch and watch the results on the display.

    Build a second decade counter circuit and add the preset logic to see it counting down from 5 instead of 9. 

    Then join the two together to see the cascade working.

    Build the clock circuit and test it counting down from 59 seconds. 

    Add in another two decade counters for the minutes display, and then another two decade counters for the hours display.

    There is more information on how decade counters work over on episode 73 of The Learning Circuit:

    /challenges-projects/element14-presents/thelearningcircuit/w/documents/4898/how-decade-counters-work----the-learning-circuit-73