Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Let's Build an Electronic Fidget Cube! -- Episode 528
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 7 Dec 2021 6:56 PM Date Created
  • Last Updated Last Updated: 10 Dec 2021 8:24 AM
  • Views 9670 views
  • Likes 12 likes
  • Comments 18 comments

Let's Build an Electronic Fidget Cube! -- Episode 528

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Fidget toys are fun but lack electronics. Let see if we can make an electronics-based fidget cube. What would you like to see on one of the sides?

Join the discussion where Katie discusses her original concepts.

Supplemental Content:

  • Episode 528: Bonus Content: Fidget Cube
  • Link to the Github:  https://github.com/hifromkatie/Fidget-Cube

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
AVR64DA32-I/PT MICROCHIP AVR Microcontroller, AVR DA Family AVR64DA Series Microcontrollers, AVR, 8bit, 24 MHz, 64 KB MICROCHIP 2 Buy Now
PG164100 MICROCHIP Debugger/Programmer, MPLAB Snap, In-Circuit, For PIC, dsPIC, AVR Flash MCUs MICROCHIP 1 Buy Now
53398-0271 MOLEX Pin Header, Wire-to-Board, 1.25 mm, 1 Rows, 2 Contacts, Surface Mount Straight MOLEX 7 Buy Now
53398-0371 MOLEX Pin Header, Vertical, Signal, 1.25 mm, 1 Rows, 3 Contacts, Surface Mount Straight MOLEX 1 Buy Now
15134-0200 MOLEX Cable Assembly, PicoBlade Receptacle to PicoBlade Receptacle, 2 Ways, 1.25 mm, 1 Row, 50 mm, 2 " MOLEX 2 Buy Now
MAX16054AZT+T MAXIM INTEGRATED PRODUCTS Push Button On/Off Controller with Debouncer, Latched Output, 2.7V to 5.5V, TSOT-23-6 MAXIM 2 Buy Now
MCOT128064P1V-WM MIDAS Graphic OLED, 128 x 64 Pixels, White on Black, 3V, I2C, Parallel, SPI, 34.5mm x 23mm, -40 °C MIDAS 1 Buy Now
MCMT5-F-V MULTICOMP PRO Navigation Switch, 1.57 N, 12 V, 50 mA, Solder, 4 MULTICOMP PRO 1 Buy Now
SKSTAAE010 ALPS ALPINE Tactile Switch, SKST Series, Top Actuated, Surface Mount, Round Button, 400 gf, 50mA at 16VDC ALPS ALPINE 1 Buy Now
MSLPT5252BG4MTR ALCOSWITCH - TE CONNECTIVITY Tactile Switch, MSLPT Series, Top Actuated, Surface Mount, Round Button, 260 gf, 50mA at 12VDC ALCOSWITCH - TE CONNECTIVITY 6 Buy Now
JSX08001SAQNL C&K COMPONENTS Slide Switch, SPDT, Momentary Spring Return, Surface Mount, 10 mA C&K COMPONENTS 1 Buy Now
434121025816 WURTH ELEKTRONIK Tactile Switch, WS-TASV Series, Top Actuated, Surface Mount, Round Button, 160 gf, 50mA at 12VDC WURTH ELEKTRONIK 2 Buy Now
PMN48XPA2X NEXPERIA Power MOSFET, P Channel, 20 V, 4.4 A, 0.037 ohm, TSOP, Surface Mount NEXPERIA 2 Buy Now
MAX1675EUA+T MAXIM INTEGRATED PRODUCTS DC-DC Switching Sync-Boost (Step Up)Regulator, Adj, 700mV-5.5Vin, 3.3V-5V/300mA out, 500 kHz, µMAX-8 MAXIM INTEGRATED PRODUCTS 1 Buy Now
MC33275ST-3.0T3G ONSEMI LDO Voltage Regulator, AEC-Q100, Fixed, up to 13 V in, 260 mV drop, 3 V/300 mA out, SOT-223-4 ONSEMI 1 Buy Now
LQH43NH220J03L MURATA Wirewound Inductor, 22 µH, 0.564 ohm, 15 MHz, 300 mA, 1812 [4532 Metric], LQH43NH_03 Series MURATA 1 Buy Now
599-0230-007F DIALIGHT LED, Orange, SMD, 1206 [3216 Metric], 20 mA, 2.1 V, 605 nm DIALIGHT 2 Buy Now
599-0210-007F DIALIGHT LED, Red, SMD, 1206 [3216 Metric], 20 mA, 2.1 V, 633 nm DIALIGHT 2 Buy Now
599-0291-007F DIALIGHT LED, Blue, SMD, 1206 [3216 Metric], 20 mA, 3.2 V, 470 nm DIALIGHT 2 Buy Now
599-0281-007F DIALIGHT LED, Green, SMD, 1206 [3216 Metric], 20 mA, 3.2 V, 525 nm DIALIGHT 2 Buy Now
MC011368 MULTICOMP PRO LED, Orange Red, SMD, 0805 [2012 Metric], 20 mA, 2.1 V, 620 nm MULTICOMP PRO 7 Buy Now
MP000443 MULTICOMP PRO LED, Green, SMD, 0805 [2012 Metric], 20 mA, 3.1 V, 525 nm MULTICOMP PRO 7 Buy Now
KPHCM-2012SYCK KINGBRIGHT LED, Low Power, Yellow, SMD, 0805 [2012 Metric], 20 mA, 2 V, 590 nm KINGBRIGHT 2 Buy Now
MULTICOMP PRO 3D Printer Filament, 2.85mm Dia, Black, PLA, 1 kg MULTICOMP PRO 1 Buy Now

 

Additional Parts:

PCBs (3)
Rechargable Lithium Polymer Battery with Molex PicoBlade 3 pin connector, 300mAh

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • Fidget
  • molex
  • buttons
  • e14p_KD
  • microchip
  • fidget cube
  • Small Circuits
  • e14presents_katiedumont
  • element14 presents
  • leds
  • katie
  • maxim
  • friday_release
  • Electronics Cube
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 4 years ago +1
    Awesome project. I like that little etch-a-sketch.
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    It looks like you could add some fillets to your posts to beef them up a bit. Also you could perhaps pin where the posts from the two halves meet in the middle.

      3D image of cube half with fillet positions shown

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 4 years ago in reply to beacon_dave

    That's a great idea, I'll give that an go and see how it compares to the original design. 

    I was planning a pin/post on one half and a hole for it to locate on the other, but forgot to add it, and then decided that it didn't seem to need it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hifromkatie
    hifromkatie over 4 years ago in reply to beacon_dave

    That's a great idea, I'll give that an go and see how it compares to the original design. 

    I was planning a pin/post on one half and a hole for it to locate on the other, but forgot to add it, and then decided that it didn't seem to need it.