Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Electronic Controlled Motorized Wheelchair -- Episode 550
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 3 May 2022 12:28 PM Date Created
  • Last Updated Last Updated: 13 May 2022 7:24 AM
  • Views 148445 views
  • Likes 7 likes
  • Comments 22 comments

DIY Electronic Controlled Motorized Wheelchair -- Episode 550

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Taking a manual wheelchair and making an adaptable system that would work on most chairs out there is something I thought about for sometime. Making it cost effective and something anyone with a 3D printer and a few tools can put together in no time. Featuring Low cost parts and hardware.

 

Mobility is a huge issue when getting older and doing the same tasks you once did you might not be able to accomplish anymore without the aid of an assistive device like a power chair or scooter. Since I do work in the medical field where I see many people struggle with simple tasks and some with even more of a simple task not being able to accomplish this. So,  Why not try to build something that can be used in multiple situations but for starters lets start with something as simple as being able to inch forward to the kitchen table or move out of the sun or turn to watch tv at a better angle. I thought creating a powered wheelchair out of a manual wheelchair would be the best thing to try to do motorizing something at a low cost that anyone can build and be able to adjust based on their needs. Now like most projects this is a proof of concept and may not hold up over the long term but making a manual chair with off the shelf parts like Arduino’s, Stepper motor controllers, and Nema17 motors.  As well as many really accessible parts from a hardware store or electronics parts shop like Newark, we can start the process of prototyping things at a reasonable price and hopefully help someone in the long run come up with an idea that can be used to help others. I had an idea and so many ideas for that one I had to start building it to see where it would lead me on my learning path of what's going to work, what's not going to work and finally a product that moves and does what it should. Making a motorized wheelchair can be upgraded to fit so many people's needs whether it's a simple task or just being able to rip around the mall for a bit.

Supplemental Content

  • Resources

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Stepper Motor, Single Shaft, Hybrid, 42 mm, Bipolar, 1.8 °, 49 N-cm, 1 A TRINAMIC 1 Buy Now
12V Battery Float Charger PERFORMANCE TOOLS 1 Buy Now
Fuseholder, Automotive, In-Line, ATO, 30A MULTICOMP PRO 1 Buy Now
Rechargeable Battery, 12 V, Lead Acid, 7 Ah, Quick Connect ENERSYS 1 Buy Now
XLR Connector, 3 Contacts, Jack, Cable Mount, Silver Plated Contacts, Metal Body, XX Series NEUTRIK 1 Buy Now
Slide Switch, SPST, Off-On, Panel Mount, R13, 16 A, 125 V MULTICOMP PRO 1 Buy Now
Rotary Potentiometer, Rotary Switch, 10 kohm, 1 Turns, Linear, 200 mW, ± 20%, P162 Series TT ELECTRONICS / BI TECHNOLOGIES 1 Buy Now
XLR Connector, 3 Contacts, Plug, Cable Mount, Gold Plated Contacts, Metal Body, DL Series NEUTRIK 1 Buy Now
Arduino Uno ARDUINO 1 Buy Now
Joystick, 2, 5 A, 250 V, 4 Position APEM 1 Buy Now
 

Additional Parts

2 x Generic L298n motor controllers

element14 presents

element14 presents  |  About Wesley | Project Videos

  • diy
  • wheelchair
  • e14p_WG
  • Motorize
  • wesley
  • Accessibility
  • arduino
  • friday_release
  • 3d print
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 4 years ago +1
    This is a great project. Might want to consider adding an enable/disable and kill switch close to the joystick. Sometimes you would want to temporarily disable the joystick to prevent accidental movement…
  • DAB
    DAB over 4 years ago +1
    Very good build. FYI, there is not a project made that does not end up with a list of changes they would do if they made it again.
  • baldengineer
    baldengineer over 4 years ago +1
    Green tape?! You Monster! Dislike. Unfollow. Unsubscribe. Hahah. Great build and video.
Parents
  • mex
    mex over 2 years ago

    can I have full documents on the project , I can't find any

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mex
    mex over 2 years ago

    can I have full documents on the project , I can't find any

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 2 years ago in reply to mex

    In general there aren't 'full documents' for these projects, however if you follow the Resources link posted above, then the download will provide more information than in the video alone.

    Project Resources:
    /cfs-file/__key/commentfiles/6b577b8c04704e209d29b6772bf67243-035beb27-0cd7-45e3-bc9a-3214aab42dea/Resources-_2800_2_2900_.zip