Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents DIY Open Source Bluetooth Headphones -- Episode 586
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 17 Jan 2023 3:59 PM Date Created
  • Last Updated Last Updated: 20 Jan 2023 8:24 AM
  • Views 37435 views
  • Likes 6 likes
  • Comments 41 comments

DIY Open Source Bluetooth Headphones -- Episode 586

Dodgy apps, subscription fees, and exclusive phone apps for a pair of headphones? Clem says: no thanks! He's fed up with the shenanigans some manufacturers pull for simple products that should just work. And why change to a different model of headphones when you've found the perfect wired pair? Can't you have that same fit and style, but wireless? So, for this project, Clem sets out to add Bluetooth to some of his favorite wired AKG headphones, using a DFRobot FireBeetle and an I2S audio module. But, to be a true open-source alternative, Clem has to whip up a custom PCB, which doesn't go according to plan. Learn the pitfalls of overly similar part numbers by following his process of figuring out the problem! What Device should have an open source variant in your opinion and would you build it yourself?

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Download All CAD and Code for Free!

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
DF robot firebeetle Esp32 DFROBOT 1 Buy Now
 

Additional Parts:

PCM5100 i2s module
Your favourite wired headphones

element14 presents

element14 presents  |  About Clem  |  Project Videos

  • DFrobot Firebeetle
  • Bluetooth Headphones
  • diy
  • e14_CMM
  • open source
  • I2S audio module
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 3 years ago +1
    This was another interesting element14 presents project. Up until now I've been using the likes of Denon or Radial Engineering Bluetooth receivers: https://www.denonpro.com/products/view/dn-200br …
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    This was another interesting element14 presents project.

    Up until now I've been using the likes of Denon or Radial Engineering Bluetooth receivers:  

    https://www.denonpro.com/products/view/dn-200br

    https://www.radialeng.com/product/bt-pro

    to accommodate those pesky mobile device users... Starts to get expensive when you need to pair with multiple devices.

    However, this open-source project looks like this could open up some alternatives and experimentation.

    USB Audio 'Class Compliant' interfaces would be another interesting area to explore further. It would be great to have some 'problem-solving' adapters that can plug into a computer USB port without needing additional drivers and provide basic channel mixing / splitting type functionality along with basic level control and metering, ideally all within the limited USB power budget to avoid the need for yet another wall wart power supply.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    that sounds indeed like a neat problem solving product! would be cool to elaborate on that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    I was thinking along the lines of taking the basic functionality of a USB audio interface something along the lines of this:

    https://cpc.farnell.com/behringer/uca202/usb-audio-interface-2-in-2-out/dp/CS20448

    and enhancing it somewhat to make it more useful as a problem-solving tool.

    One scenario I'm faced with is that a lot more people are relying on Zoom / MS Teams for online meetings these days however, such systems often expect a 2ch stereo USB based audio input/output whereas audio equipment is often still analogue based. Issues often encountered are:

    • no USB audio connectivity or USB audio connectivity but needs audio device drivers require installing but no admin rights to do so.
    • different analogue standards in use +4dBu on XLR vs -10dBV on RCA/phono so different levels and balanced / unbalanced signalling.
    • limited gain adjustment range at one or both ends.
    • mic level versus line level signals.
    • stereo vs mono.signals.
    • no visible level metering (is a signal actually present and if so, how hot is it?)

    So, you either tend to require an audio mixer with USB interface or end up with a number of problem-solving boxes and cables. 

    A single problem-solving tool that can be simply plugged into the USB port and give you immediate indication if there is a signal present or not and at what sort of level and be able to configure it for mono/stereo operation and to be able to adjust the gains into the right ball-park and to deliver it on XLR or RCA/phono, all without needing to install drivers or a configuration app, would be a valuable tool.

    I've not seen anything available off-the-shelf that ticks all the boxes, without going over-the-top.

    Also, sometimes you want a problem-solving tool to use yourself and sometimes you want a problem-solving tool that you can mostly pre-configure and then hand to someone else and be able to support remotely over the phone.   

    In an ideal world it might end up being an audio interface that has a bidirectional USB to I2S stage followed by a I2S DSP stage and then an analogue IO stage for maximum flexibility. However, to start off with I was thinking of something a bit simpler, basically an open-source USB audio interface with some basic signal mixing, level monitoring and gain control ability, all that can be powered off the USB port it is connected to.

    If it was a modular design, people could tailor it to their individual requirements e.g. balanced vs unbalanced outputs, different metering scales, different gain ranges etc. and even build their own custom mixer. I expect a number of people will be familiar with creating analogue audio circuits, but adding USB audio may be a bit new.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    oh yes that sounds very interesting, to solve the problems i actually have a fully fledged (small) audio mixer with USB interface.
    so its quite overkill and big to solve just me wanting to use normal audio gear instead of a dedicated USB microphone which I usually use.
    It basically was the reason apart from recommendations that I got a dedicated podcasting mic with USB.

    So the  key features are just controlling of levels and gain directly on the device, and instant working without drivers to install.
    I wonder if there are MCUS that can directly support WIn/mac/linux audo device types on native usb...

    A good DAC and ADC via I2S and a sturdy compact case would do the trick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    oh yes that sounds very interesting, to solve the problems i actually have a fully fledged (small) audio mixer with USB interface.
    so its quite overkill and big to solve just me wanting to use normal audio gear instead of a dedicated USB microphone which I usually use.
    It basically was the reason apart from recommendations that I got a dedicated podcasting mic with USB.

    So the  key features are just controlling of levels and gain directly on the device, and instant working without drivers to install.
    I wonder if there are MCUS that can directly support WIn/mac/linux audo device types on native usb...

    A good DAC and ADC via I2S and a sturdy compact case would do the trick.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    Other key features are monitoring the signal levels visually, stereo<->mono routing, USB power, and low audio latency.

    To conserve power and save space, the monitoring could be a single LED 'bullet' meter which gets brighter as the input level increases. A bi-colour LED could be used to indicate nearing clipping of the USB input. 

    The basic routing just needs the ability to mix the stereo LR output from the USB down to a mono output signal to send to the external analogue device and to take the mono return from the external analogue device and to send it to both the USB LR inputs. These should be individually selectable as you can often end up with a mono mic but stereo speakers type scenario.

    Not all computer sound drivers provide appropriate or reliable metering or routing functionality.

    Yes, I was wondering what MCUs might be able to do this as it would allow the ability to reconfigure the behaviour of the one hardware device in several ways and make it highly flexible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    with all that I would be a bit worried of either the user interface having to many things to still be simple or with typical "one button designs" be cumbersome to use to get through all options quickly. it is a UX challenge as well.
    I thought about having two rows of adressable RGB leds, act as VU meter and indicator for settings.
    as long as you do nothing --> VU is show vor in/output
    When you move or click a rotary encoder, the leds indicate the setting to adjust. click to enter-> adjust ->click to exit.
    so GAIN in , Volume out, mono/Stereo in , mono/stereo out,
    Am I missing something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    Speaking of USB mics, another problem-solver device waiting to be discovered is how to mix multiple USB mics down to a single USB mic. A number of web conference applications can only handle a single audio input device so if you have a presenter on a USB microphone and want to take a question from the audience or bring in a guest on another microphone, then you may have to reconfigure the audio input device in you web conference application and then reconfigure it back again. Being able to mix the 2 USB audio devices externally would be useful.

    There are a few USB audio type problems out there waiting for solutions.

    (Similar with USB web cams, I'm only aware of a single (expensive) product at the moment that allows you to switch between two USB webcams externally to the computer. If they are UVC class compliant webcams, then it should be possible to have a driverless solution.)  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    oh thats is a whole different can of worms, but also a very interesting one.
    I think with a USB-Host capable MCU one could act as an intermediary to pass on only the data not the USb communications form the PC unlike a switch/hub.
    So the PC hosts an MCU via USB
    the MCU hosts 2 USB devices
    data from USb devices get pased on to the pc.
    the PC only ever sees 1 device, so for it its the same device that just passes on different data.

    the biggest challenge for that might be latency.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    To keep it simple, the mono/stereo could perhaps just be a pair of slide switches.

    I was concerned about the power consumption of the addressable LED VU meters but it makes for an interesting UX feature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    I think some dinky 20mA leds would be bright enough, no need for fancy neopixels IMO
    since the device could fall under the EU- USB-C recommendetion the power limitations of USB 1.1. don't apply really, but having it all doable with 5V @500mA would of course be preferrable for max compability.

    slide switches would be the simplest way for passive routing ,but beeing able to mix them lets say via digital pot would be cool...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    Yes, that was intended as a separate project idea.  Slight smile

    ( The Inogenie devices do the webcam switching:
    https://inogeni.com/product/share2u/  )

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 3 years ago in reply to beacon_dave

    Seems the intended use is dunymic composition of additional sources into an hdmi feed, that is passed on downstream.
    yeah a simpler solution for just the mentioned usecase seems to fit aniche here!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    They do a 4:1 switcher 2xUSB/2xHDMI as well:

    https://inogeni.com/product/cam300/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to mayermakes

    Originally, I was thinking of passive routing with the switches but then I was thinking of GPIO inputs so that their function could be defined in software depending on an individual's use case making it more flexible.

    They could also be push buttons though that act as a simple mode selector that uses the LED VU bar position to show what mode you are in and then the rotary selector does inc/dec push to set.

    5V at 500mA would be ideal as there is a lot of kit out there that isn't USB-C yet. It could use a second USB port though to bring it up to 1000mA, without reaching for a wall-wart PSU.  

    In a lot of cases, the LEDs don't need to be on for the duration. They would mainly be used for configuration purposes, so a small battery could be used to provide the additional power demand for LEDs or even a small OLED display. However that adds to the design.