Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents From Strava to Motion: Creating an Arduino-Powered Arcade Game with Running Data -- Episode 607
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 13 Jun 2023 1:11 PM Date Created
  • Last Updated Last Updated: 16 Jun 2023 7:24 AM
  • Views 25152 views
  • Likes 9 likes
  • Comments 25 comments

From Strava to Motion: Creating an Arduino-Powered Arcade Game with Running Data -- Episode 607

Following on from building an air hockey table, Lorraine is recreating another classic arcade game: the Derby. Instead of horses racing along a track, it will be runners! Find out how to download your running data from strava and move a runner along a track in competition with your family and friends. This project involves a bit of everything: 3d printing, laser cutting, coding in C and using motors with the Arduino Wifi board.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Bonus Content:

  • Registration Required:  Download Code  (Register to become a Member!)
  • Registration Required:  Download CAD Files   (Register to become a Member!)
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
Bill of Materials

Product Name Manufacturer Quantity Buy Kit
DFROBOT Micro DC Motor, TT Geared, Encoder, 6V, 160RPM, 120:1, L Shape, Arduino Board DFRobot 4 Buy Now
Expansion Board, Quad DC Motor Driver Shield, Arduino Development Board DFRobot 1 Buy Now
Microswitch, Miniature, Long Hinge Lever, SPST-NO, Quick Connect, 16 A, 8 V Omron 4 Buy Now
Single Board Computer, Arduino Uno WiFi, ATmega328P, 14 I/O, 48KB Flash, 6144Bytes SRAM, 256Bytes Arduino 1 Buy Now
Rocker Switch, On-Off, SPST, Non Illuminated, Panel Mount, Black, PRA TE Connectivity 1 Buy Now
DC Power Connector, Socket, 2.1 mm, Chassis Mount, Solder Pro Signal 1 Buy Now
AC/DC Power Supply, Level VI, 1 Output, 15 W, 5 VDC, 3 A Multicomp 1 Buy Now
Pin Header, Right Angle, Board-to-Board, 2.54 mm, 1 Rows, 6 Contacts, Through Hole Right Angle AMP - TE CONNECTIVITY 1 Buy Now
Jumper Wire Kit, Male to Female, Multi-Coloured, 200 mm, 0.1" Dupont Connector, 0.2 mm² Multicomp 1 Buy Now
 

Additional Parts:

3mm laser acrylic for box, supports and runners
3d printed pulleys
3d printed supports for motors and runners
Timing belt 6mm, 640mm long x 4

element14 presents

element14 presents  |  About Lorraine |  Project Videos

  • e14p_LU
  • arduino uno
  • 3dprinter
  • strava
  • the derby
  • arcade
  • laser cutter
  • childhood games
  • arcade games
  • 3dprinting
  • strava API
  • DF Robot
  • electronics
  • arduino
  • friday_release
  • laser cutting
  • running
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • RoRo87
    RoRo87 over 2 years ago +1
    Why are the Download Elements not available?
  • beacon_dave
    beacon_dave over 2 years ago in reply to RoRo87 +1
    Code: /challenges-projects/element14-presents/m/files/147743 CAD: /challenges-projects/element14-presents/m/files/147744
  • RoRo87
    RoRo87 over 2 years ago in reply to tmazer +1
    I can't give you a answer because i didn't tried it out.But i wouldn't do it with strava.I prefer to build it with roll-a-ball like the original horse race but a little bit smaller.
Parents
  • beacon_dave
    beacon_dave over 3 years ago

    You could perhaps try using some springs to apply a little bit of tension the belts seeing as you have adjustment slots at one end. 

    Perhaps could use some cable clips/ties to secure the cables to the base plate. You can get clips with sticky fixers which are quick and simple but they tend to dry out and  fail after a while. However as you are laser cutting, then you could cut some holes in nice straight lines at an even spacing to keep it neat and tidy. Could also cut a groove to lay them into with dabs of hot glue to secure. (Health and safety first - don't want your runners tripping over cables) 

    The movement of the runners is looking pretty smooth.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lorrainbow
    lorrainbow over 3 years ago in reply to beacon_dave

    yeah, i was thinking of springs to tension the belts but they just seemed to work! I was very lucky

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to lorrainbow

    They may help over time if the design gets used a lot, as things start to wear and try to work their way loose. A spring tensioned idler wheel against the belt is another way to do it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 3 years ago in reply to lorrainbow

    They may help over time if the design gets used a lot, as things start to wear and try to work their way loose. A spring tensioned idler wheel against the belt is another way to do it.