Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Using PID (Proportional-Integral-Derivative) in Robotics - How Hard Could It Be? -- Episode 614
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 2 Aug 2023 6:07 PM Date Created
  • Last Updated Last Updated: 4 Aug 2023 7:24 AM
  • Views 22959 views
  • Likes 9 likes
  • Comments 10 comments

Using PID (Proportional-Integral-Derivative) in Robotics - How Hard Could It Be? -- Episode 614

Adam has often wondered how PID controls work and how they are implemented. Is PID tuning challenging? Do external factors on the robot affect PID tuning? Watch Adam build a parking robot using PID to accelerate, decelerate, and keep track of the distance from other objects.

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Adam takes on the challenge of using a PID (Proportional Integral Derivative) controller in a robotics project. He is interested in robotics and has experience with Halloween animatronics, but PID control presents a new level of complexity. PID is commonly used in advanced robotics projects. Examples include balancing robots or systems that require precise control to stay centered, such as a platform with a bouncing ping-pong ball. 

image

Adam's project involves creating a basic self-driving car that can accelerate and decelerate within a one-meter distance without overshooting the target. He has designed a robot with two beefy motors (120 RPM, 12 watts each) for the left and right sides. Power management is a concern, so he is considering using a cable instead of a battery. The robot will be driven by an Arduino Uno R4 Minima, which is a compact and capable microcontroller board that interfaces with the motor driver and an ultrasonic sensor to implement the PID control. 

3D CAD

To realize his design, Adam has iterated through various prototypes and 3D-printed parts for the robot. He used M3 screws for all components to avoid the need for hot glue or modifications. The robot features two large tires, and Adam plans to add electrical tape for better traction on hardwood surfaces. Despite the challenges during the design phase, he is excited about the potential success of the final product. 

3D Print

During the PID tuning process, Adam faces some difficulties. He turns to a chatbot for code assistance, but the provided code has some inaccuracies for his specific setup. Regardless, the code from the chatbot gives him valuable insights and prompts him to think about setting PWM limits and stopping when the target distance is reached. This process highlights the complexities involved in fine-tuning PID controllers for individual systems. 

Attempt 2

After adjusting his code and robot setup, Adam sees significant improvements in performance. Although there are still some issues with overcompensation and occasional tipping, the robot is now much closer to achieving its desired behaviour. PID tuning is an art form, it requires patience and understanding of numerous factors beyond just the constant values. 

...Hard

Throughout the project, Adam encounters challenges related to the ultrasonic sensor and weight distribution, but with the Arduino Uno R4 Minima at its core, he can efficiently program and fine-tune the PID controller to achieve the desired performance of the self-driving car. This powerful yet compact microcontroller empowers makers like Adam to explore advanced robotics concepts and experiment with PID control in their projects. Despite the difficulties, he is excited about the progress made and looks forward to further improvements in his robot's behaviour. 

Bonus Content:

  • Download Code and CAD Files!

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
3D Printer Filament, PLA, White MULTICOMP 1 Buy Now
Sensor Board, Ultrasonic Distance Sensor, PING PARALLAX 1 Buy Now
ARDUINO UNO REV4 WIFI ROHS COMPLIANT: YES Arduino 1 Buy Now
 

Additional Parts:

2x 100 RPM 12V Gear Motor High Torque
DC Motor Driver, DROK L298
Various M3 Screws

element14 presents

element14 presents  |  About Adam |  Project Videos

  • robot design
  • advanced robotics
  • ultrasonic sensor
  • Self-Driving Car
  • e14p_AS
  • fine-tuning pid
  • arduino minima r4
  • 3D Printing
  • robitics tuning techniques
  • autonomous vehicles
  • robotics tutorial
  • PID Control
  • balancing robot
  • robotics project
  • motor driver
  • friday_release
  • maker's challenge
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • baldengineer
    baldengineer over 3 years ago

    Great project Adam. I like seeing the multiple attempts and their solutions.

    Most of my experience with PID tuning is for my reflow oven. Which has a very slow cycle time (since I have to wait for it to cool.) Learning about the algorithm with a motor/robot would probably be much easier.

    Since making the video, have you made any other discoveries or learnings to improve the coefficients?

    (Also, side note, that 9V battery triggered me. Don't forget those things are only good for 25-30 milliamps. Anything more, like from motors, and their voltage drops fast!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • baldengineer
    baldengineer over 3 years ago

    Great project Adam. I like seeing the multiple attempts and their solutions.

    Most of my experience with PID tuning is for my reflow oven. Which has a very slow cycle time (since I have to wait for it to cool.) Learning about the algorithm with a motor/robot would probably be much easier.

    Since making the video, have you made any other discoveries or learnings to improve the coefficients?

    (Also, side note, that 9V battery triggered me. Don't forget those things are only good for 25-30 milliamps. Anything more, like from motors, and their voltage drops fast!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • adamsoileau1
    adamsoileau1 over 3 years ago in reply to baldengineer

    Great point! I didn't really wanna worry about power in the project, so I definitely overlooked that detail. I'm not sure how much the motor driver and the ultrasonic sensor draws? I powered the motors from a seperate power supply. They consumed around 24w total, so that was a yikes. I think I'm getting better at tuning for sure! Very glad this project let me be introduced to it, but it's for sure an art form. I remember hearing stories of people spending like a full day trying to tune their PID system, and I can now relate to that lol