Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Mastering Oven Control: Precision Resin Curing with DIY Modifications - How Hard Can it Be? -- Episode 616
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 15 Aug 2023 4:14 PM Date Created
  • Last Updated Last Updated: 18 Aug 2023 7:24 AM
  • Views 22358 views
  • Likes 7 likes
  • Comments 12 comments

Mastering Oven Control: Precision Resin Curing with DIY Modifications - How Hard Can it Be? -- Episode 616

In this element14 presents episode, Katie tackles the challenge of revamping a budget-friendly toaster oven and transforming it into a dependable resin-curing tool with precise temperature control. She begins by explaining her need for clear epoxy resin with specific curing requirements, as well as the dilemma she faces regarding temperature settings. Intrigued by the 'for best results' instructions and a desire to reduce the curing time, Katie turns to an economical toaster oven she found online. Although acknowledging its lower quality, she hopes to modify it for her purpose. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Katie's attention shifts to the toaster oven's temperature control mechanism, which she suspects might not accurately reflect the actual temperature output. The oven's operation involves adjusting the desired temperature and time, but Katie aims for more accuracy. To address this, she opts for a Raspberry Pi Pico and a spare thermistor. However, the thermistor's leads fall short of reaching outside the oven, necessitating soldering. Since the solder's melting point is near the curing temperature, Katie anticipates potential connection challenges. 

 image

The project's crucial stages encompass adapting a kitchen thermometer probe for precise temperature measurement and managing the oven's heating elements. Katie delves into the inner workings of the toaster oven, discovering the series connection between the timer and temperature control. She plans to replace the original control system with her design, integrating an Omron power relay to handle mains voltage switching. She acknowledges the requirement for a separate 24V power supply for the relay coil. 

 image

Constructing a detailed circuit and programming the Raspberry Pi Pico are fundamental steps in Katie's project. She successfully incorporates temperature readouts, buttons for setting and initiating oven functions, and a relay for heating element control. During testing, Katie observes that the temperature remains within a 10-degree range of the set value, marking a significant improvement over the original controller. Impressed with the results, she highlights the potential for wider applications beyond resin curing. 

 image

Subsequently, Katie addresses practical issues, such as preventing the K-Type thermocouple from coming into contact with grounded metal, which could disrupt temperature readings. She develops a protective insulation approach and further optimizes her control setup. Replacing loose connections with Wago block connectors enhances reliability and safety, mitigating grounding concerns. Throughout her journey, Katie demonstrates resourcefulness in troubleshooting and determination to create a refined and user-friendly DIY solution. 

 image

Ultimately, Katie successfully crafts a compact and functional control box for her toaster oven project. While acknowledging potential aesthetic improvements, she celebrates her accomplishment in developing a cost-effective and dependable tool for resin curing. She encourages fellow makers to explore this versatile modification, adaptable to various oven systems. Katie's experience showcases the potential of elevating everyday appliances with technical skills, while also addressing the challenges she overcame in achieving her goal. 

Bonus Content:

  • GitHub (Code): https://github.com/hifromkatie/Toaster-Oven-Controller
  • Download Code

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
RASPBERRY PI PICO RASPBERRY-PI 1 Buy Now
High Temperature Sensor, Gravity, I2C, K-Type, 800℃, for Arduino and Raspberry Pi Board DFROBOT 1 Buy Now
Thermocouple, Nozzle, K, 0 °C, 350 °C, Stainless Steel, 6.6 ft, 2 m LABFACILITY 1 Buy Now
GROMMET, BLACK M20 PK50 PRO POWER 2 Buy Now
Power MOSFET, P Channel, 20 V, 4.2 A, 0.04 ohm, SOT-23, Surface Mount DIODES INC. 1 Buy Now
Plastic Enclosure, Box, With Lid, Multipurpose, ABS, 83.1 mm, 177 mm, 120 mm MULTICOMP PRO 1 Buy Now
IC, V REG +5.0V, 7805, TO-220-3 ONSEMI 1 Buy Now
Power Relay, SPST-NO, 24 VDC, 10 A, G2R Series, Through Hole, Non Latching OMRON ELECTRONIC COMPONENTS 1 Buy Now
 

Additional Parts:

Toaster Oven

element14 presents

element14 presents  |  About Katie Dumont |  Project Videos

  • e14p_KD
  • temperature control
  • raspberry pi pico
  • oven
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • beacon_dave
    beacon_dave over 3 years ago +1
    Can't you 3D print a bezel for the screen aperture ? It will hide the cut edges of your enclosure.
  • michaelkellett
    michaelkellett over 3 years ago +1
    The standard way of getting more precise control (used by millions of temperature controllers) doesn't need any extra parts. To get a fast warm up and low overshoot the controller needs to regulate the…
Parents
  • dougw
    dougw over 3 years ago

    To get a tighter feedback loop, you could try placing the thermocouple closer to the heater element. This reduces the time between a change in heater output to the time when it is detected by the sensor. This will reduce overshoot. There is still thermal inertia in the heater element to contend with. (Turning the heater off does not instantly reduce its temperature) A PID loop works to compensate for thermal inertia but it takes a while to get the hang of tuning the 3 gain constants in PID loops. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 3 years ago in reply to dougw

    Good suggestion, I put it in the middle as there's a element at the top and the bottom, but closer to one of the elements would mean it'd switch off earlier and then may not overshoot quite so much

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • hifromkatie
    hifromkatie over 3 years ago in reply to dougw

    Good suggestion, I put it in the middle as there's a element at the top and the bottom, but closer to one of the elements would mean it'd switch off earlier and then may not overshoot quite so much