Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Spying Under the Christmas Tree with an Arduino-powered Ornament -- Episode-633
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 14 Dec 2023 2:21 PM Date Created
  • Last Updated Last Updated: 22 Dec 2023 11:19 PM
  • Views 6549 views
  • Likes 12 likes
  • Comments 37 comments

Spying Under the Christmas Tree with an Arduino-powered Ornament -- Episode-633

'Tis the season for holiday cheer, and as you adorn your Christmas tree, the excitement of discovering what lies beneath on the morning of celebration is undeniable. Ever tempted to sneak a peek early, risking a spot on the naughty list? What if there was a way to explore the tree's treasures discreetly using robotics? In this video, Milos delves into the concept by creating a Christmas ornament-shaped robot. With the press of a button, this robot will transform into a small mobile robot equipped with a live video feed camera and night driving lights. But how does it navigate among the other ornaments on the tree? Fear not – it can winch down to the ground for a quick look and pull itself back up again, leaving no trace. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Downloads and Links | Bonus Videos | Bill of Material | Discussion

Design & Assembly 

Milos starts by brainstorming a few rough sketches and ideas, which provide a roadmap for the project. The goal is to create a Christmas ornament (a sphere with a diameter of no more than 100mm) that transforms into a drivable robot. 

image

The sphere shape is chosen so that the robot can blend inconspicuously in with the other ornaments on the tree. The robot is 3D printed from shiny red silk PLA filament. Hidden inside, a tiny winch! When it's time to explore, trap doors open, wheels emerge, and the robot descends gracefully from the tree. 

image

Electronics  

Integral to the project's success is the small (but powerful) Arduino Nicla Vision board. The Arduino enables Wi-Fi connectivity and allows Milos to control the robot's motors, while also live streaming footage from the embedded camera to a PC via Wi-Fi (RTSP). 

image 

Powering the robot is a 9V battery regulated to 5.1V using the LM317T linear voltage regulator. For night driving, Milos incorporates six small LEDs controlled by an N-channel MOSFET. To address issues with continuous rotation servos during testing, a level shifter using BJT transistors is added; this successfully corrects any distortions in the motors. 

 image

The comprehensive schematic and Arduino Nicla Vision pinout provide a closer look at the project's electronic configuration.  

image

image

Software 

The software has two components: the Arduino Nicla Vision code and Node-RED software. Milos expands the Arduino Nicla Vision code from the RTSP example in the OpenMV IDE, incorporating PWM and MQTT controls. PWM for the Nicla Vision was implemented using Arduino’s Timers functionality. 

The Node-RED code serves as the interface for controlling the robot. While alternative microcontrollers can be used for MQTT controls, Milos leverages a Raspberry Pi setup with Node-RED and an MQTT broker for efficient control. 

In a nutshell, Milos' MR-04 Robot Christmas Ornament is like holiday magic with a tech twist. It’s an inconspicuous decoration that morphs into a roving robot with a live video feed—pretty cool, right? This perfect blend of festive cheer and cutting-edge fun turns your Christmas into a tech-powered celebration! 

Downloads and Links:

  • Download CAD Files and Code!
  • GitHub: https://github.com/MilosRasic98/RobotChristmasOrnament  

Bonus Videos:
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
Bill of Material:

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Arduino Nicla Vision ABX00051 Samsung 1 Buy Now
PLA Filament Multicomp Pro MP007445 Dialight 1 Buy Now
Position Servo Motor Multicomp Pro MP-708-0001 Dialight 1 Buy Now
Continuous Servo Motor Multicomp Pro MP-708-0002 Microchip 2 Buy Now
Linear Voltage Regulator LM317T Panasonic 1 Buy Now
MOSFET IRL540N Panasonic 1 Buy Now
 

Additional Parts:

Braided fishing line
M3 screws
M2.5 screws
M2 screws
Small piece of PTFE tubing
Basic electronic components
Perfboard and wires
9V battery

element14 presents

element14 presents  |  About Milos Rasic |  Project Videos

  • Electronics for Christmas
  • Christmas tree innovation
  • Arduino Nicla Vision
  • Arduino holiday crafts
  • e14p_Milos
  • Christmas robot ornament
  • DIY tech ornaments
  • Creative festive gadgets
  • Tech-driven holiday crafts
  • Tech-inspired Christmas
  • Robotic holiday joy
  • Festive robotics
  • Holiday tech decor
  • Ornament transformation
  • Smart holiday decorations
  • DIY robot project
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • robogary
    robogary over 2 years ago

    Excellent job keeping the project to the targeting size. I always start small, but by the time the project is done, I end up with something that can snowplow a road in Iceland. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 2 years ago

    Excellent job keeping the project to the targeting size. I always start small, but by the time the project is done, I end up with something that can snowplow a road in Iceland. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • milosrasic98
    milosrasic98 over 2 years ago in reply to robogary

    Thanks, all projects go like that, this one included hahaha! I anticipated that happening, so my original goal was an 80mm sphere, but I was happy with anything under or around 100mm and it ended up being 99.8mm!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to robogary

    Perhaps not such a problem if you mainly work on Icelandic snowplough projects Slight smile