Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Spying Under the Christmas Tree with an Arduino-powered Ornament -- Episode-633
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 14 Dec 2023 2:21 PM Date Created
  • Last Updated Last Updated: 22 Dec 2023 11:19 PM
  • Views 6549 views
  • Likes 12 likes
  • Comments 37 comments

Spying Under the Christmas Tree with an Arduino-powered Ornament -- Episode-633

'Tis the season for holiday cheer, and as you adorn your Christmas tree, the excitement of discovering what lies beneath on the morning of celebration is undeniable. Ever tempted to sneak a peek early, risking a spot on the naughty list? What if there was a way to explore the tree's treasures discreetly using robotics? In this video, Milos delves into the concept by creating a Christmas ornament-shaped robot. With the press of a button, this robot will transform into a small mobile robot equipped with a live video feed camera and night driving lights. But how does it navigate among the other ornaments on the tree? Fear not – it can winch down to the ground for a quick look and pull itself back up again, leaving no trace. 

Watch the Video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Downloads and Links | Bonus Videos | Bill of Material | Discussion

Design & Assembly 

Milos starts by brainstorming a few rough sketches and ideas, which provide a roadmap for the project. The goal is to create a Christmas ornament (a sphere with a diameter of no more than 100mm) that transforms into a drivable robot. 

image

The sphere shape is chosen so that the robot can blend inconspicuously in with the other ornaments on the tree. The robot is 3D printed from shiny red silk PLA filament. Hidden inside, a tiny winch! When it's time to explore, trap doors open, wheels emerge, and the robot descends gracefully from the tree. 

image

Electronics  

Integral to the project's success is the small (but powerful) Arduino Nicla Vision board. The Arduino enables Wi-Fi connectivity and allows Milos to control the robot's motors, while also live streaming footage from the embedded camera to a PC via Wi-Fi (RTSP). 

image 

Powering the robot is a 9V battery regulated to 5.1V using the LM317T linear voltage regulator. For night driving, Milos incorporates six small LEDs controlled by an N-channel MOSFET. To address issues with continuous rotation servos during testing, a level shifter using BJT transistors is added; this successfully corrects any distortions in the motors. 

 image

The comprehensive schematic and Arduino Nicla Vision pinout provide a closer look at the project's electronic configuration.  

image

image

Software 

The software has two components: the Arduino Nicla Vision code and Node-RED software. Milos expands the Arduino Nicla Vision code from the RTSP example in the OpenMV IDE, incorporating PWM and MQTT controls. PWM for the Nicla Vision was implemented using Arduino’s Timers functionality. 

The Node-RED code serves as the interface for controlling the robot. While alternative microcontrollers can be used for MQTT controls, Milos leverages a Raspberry Pi setup with Node-RED and an MQTT broker for efficient control. 

In a nutshell, Milos' MR-04 Robot Christmas Ornament is like holiday magic with a tech twist. It’s an inconspicuous decoration that morphs into a roving robot with a live video feed—pretty cool, right? This perfect blend of festive cheer and cutting-edge fun turns your Christmas into a tech-powered celebration! 

Downloads and Links:

  • Download CAD Files and Code!
  • GitHub: https://github.com/MilosRasic98/RobotChristmasOrnament  

Bonus Videos:
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
Bill of Material:

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Arduino Nicla Vision ABX00051 Samsung 1 Buy Now
PLA Filament Multicomp Pro MP007445 Dialight 1 Buy Now
Position Servo Motor Multicomp Pro MP-708-0001 Dialight 1 Buy Now
Continuous Servo Motor Multicomp Pro MP-708-0002 Microchip 2 Buy Now
Linear Voltage Regulator LM317T Panasonic 1 Buy Now
MOSFET IRL540N Panasonic 1 Buy Now
 

Additional Parts:

Braided fishing line
M3 screws
M2.5 screws
M2 screws
Small piece of PTFE tubing
Basic electronic components
Perfboard and wires
9V battery

element14 presents

element14 presents  |  About Milos Rasic |  Project Videos

  • Electronics for Christmas
  • Christmas tree innovation
  • Arduino Nicla Vision
  • Arduino holiday crafts
  • e14p_Milos
  • Christmas robot ornament
  • DIY tech ornaments
  • Creative festive gadgets
  • Tech-driven holiday crafts
  • Tech-inspired Christmas
  • Robotic holiday joy
  • Festive robotics
  • Holiday tech decor
  • Ornament transformation
  • Smart holiday decorations
  • DIY robot project
  • friday_release
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply
Parents
  • beacon_dave
    beacon_dave over 2 years ago

    Another nice design.

    Just wondering if a small magnet might replace the tape to hold the lower flaps closed until the wheels are ready to be deployed ?

    Also wondering if the wheels returning to their closed position hitting a lever could help pull the flaps closed ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 over 2 years ago in reply to beacon_dave

    Thanks!

    My initial idea was for the rubber bands to do all of the work, so I didn't plan for the magnet in advance. As for the wheels hitting a lever, I thought about having a lever system for the trap doors as I did for the wheels, but due to them needing a much bigger range of motion, I needed a compound system of levers. I tried figuring out the geometry in the constraints of the round shape, but couldn't manage to get a working model even in CAD. This is something I would sure love to upgrade for the next iteration. Another idea I had was to have gear teeth on both the trap door and the wheel segment so that they interact in that way!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to milosrasic98

    If there was a way to replace the opening threads of the trap doors with a Bowden cable then it may be possible to get open/close action in one go.

    If you can use gravity to your advantage then perhaps that could halve the amount of travel required. That's what I was originally thinking of - have the retracting wheels hit a cantilever connected to the trap doors once gravity has played its part. 

    Another thought was a rack and pinion arrangement using a pinion gear on the wheel lowering servo to push out / pull in two racks which are then attached to the trap doors.

    MotionGen looks an interesting app. It looks similar to David Rector's 'Linkage Mechanism Designer and Simulator' program.

    Are you aware of any good resources on kinematics for designing linkages like this ? I expect that a number of designs probably rely on existing known linkage mechanisms along with some trial and error. However some designs would appear to go far beyond that approach. This goes back to early automata long before simulation software was available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 over 2 years ago in reply to beacon_dave

    There is another complication with how I implemented threads, and that's because the threads are going over the hinge that is hanging out a few millimeters outside the ornament, there is a moment in the movement where the thread goes from straight to bent over the hinge, and the trap door can get stuck at those positions.

    I like the idea with gears as well, I'll try redesigning this at some point for sure, but I would love to go with a fully constrained approach with some levers or gears.

    I liked MotionGen because of its cartoonish graphic style, so it's fun to play around in! Just checked the program you suggested, and it looks great, I'll give it a go for sure.

    I honestly haven't checked anything before starting the design, I had the idea for the wheels and thought that the trap door would be just adding a few more linkages. However, I know of 2 great places for getting inspiration for all sorts of mechanisms (looking at it now, would have been smart if I had checked them before building this).

    1. 507 Mechanical Movements - I'm in love with this site, and the art style and they keep adding animations now as well: https://507movements.com/

    2. S. CRAFT Youtube Channel - I found this channel by accident, The content is mostly short videos of interesting linkages or gear systems, just a lot of great videos and ideas: https://www.youtube.com/@SCRAFTchannel/videos 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to milosrasic98

    507 I've come across before, S. Craft is a new one, thanks.

    'thang010146' on YouTube has a few thousand nice videos on linkages and mechanisms to add to the list. The trouble is finding the one you need Slight smile

    The only real lecture on kinematics for linkages that I've seen though is this MIT Tech TV one on designing a four bar mechanism to perform a specific motion:

    https://youtu.be/4dkng7zajGA?t=656 

    I'm sure there must be more however.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • milosrasic98
    milosrasic98 over 2 years ago in reply to beacon_dave

    Just checked the thang010146 YouTube Channel, I love it, and I'll go through a lot of them for sure!

    Thanks for sharing the lecture, I'll take a listen, if I find anything on this topic at some point, I'll make sure to link it here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • milosrasic98
    milosrasic98 over 2 years ago in reply to beacon_dave

    Just checked the thang010146 YouTube Channel, I love it, and I'll go through a lot of them for sure!

    Thanks for sharing the lecture, I'll take a listen, if I find anything on this topic at some point, I'll make sure to link it here.