Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Pripyat - DIY Geiger Counter -- Episode 352
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 24 Jul 2018 5:53 PM Date Created
  • Last Updated Last Updated: 27 Jul 2018 7:24 AM
  • Views 7073 views
  • Likes 11 likes
  • Comments 15 comments

Pripyat - DIY Geiger Counter -- Episode 352

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Matthew goes atomic punk in this video where he takes some old Soviet surplus Geiger-Muller tubes and builds his own recreation of a Civil Defense-style Geiger counter. The CDV-700 series survey meters were developed in coordination with the US government at the height of the Cold War for deployment to local Civil Defense authorities. With a few off-the-shelf parts, Matthew builds a high-voltage circuit to power the GM tube and uses an Arduino Nano to process the output signal, driving the characteristic click and dancing analog meter, then encloses it in a custom 3D-printed case completing the homage to this mid-20th century piece of vintage tech!

 

 

Product Name Quantity
Buy Kit

Perfboard

1 Buy Now

110V to 6V center-tap transformer

1 Buy Now

555 timer and socket

1 Buy Now

0.1uF 50V electrolytic capacitor

1 Buy Now

0.01uF 700VAC film capacitor

2 Buy Now

1N4007 diode

2 Buy Now
0.01 uF 1kV ceramic disc capacitor 3 Buy Now
4.7k resistor 4 Buy Now
12k resistor 1 Buy Now
100k resistor 2 Buy Now
BUZ71 MOSFET 1 Buy Now
2-pin screw-on connector set 1 Buy Now
SbM-20U Geiger-Muller tube (any tube will do, but you'll have to adjust for different input/output voltages) 1
1M resistor 2 Buy Now
330 resistor 1 Buy Now
2N2222 BJT 1 Buy Now
Arduino Nano 1 Buy Now
Piezo buzzer 1 Buy Now

5V moving magnet analog panel mount meter

1 Buy Now
SPST panel mount toggle switch 1 Buy Now

LED

1 Buy Now

Adafruit PowerBoost 1000

1 Buy Now

LiPo battery

1 Buy Now

Wire

1 Buy Now
Solder 1 Buy Now
3D Printer Filament 1 Buy Now

 

Matt Eargle is a cold war nut who loves historical technologies. He just happens to have some old Soviet surplus Geiger tube sitting around.   He’ll use it to build his own take on a Geiger counter.  It will be something like an updated CDV 700 series. The original CDV-700 Series models were in production from 1954 until 1974.  Later XXX series models were produced well into the 1980s. In order to build a homebrew version of a Geiger counter, he’ll need a couple of components in addition to his Geiger tube.  A Geiger tube has a sealed vial inside a sealed glass tube containing an inert gas. You take that and apply a really high potential, the one he’s using is about 400 volts. When your particle comes in and strikes the nucleus of the gas inside, it temporarily ionizes that gas, just enough to allow some of that voltage through that it can be measured.

 

He’ll need a high voltage source to feed his tube.  The cathode of the tube will run into an Arduino.  Running the high voltage source through batteries will require a transformer.  The transformer will require an AC current.  The easiest way to create an AC current would be to create a little oscillator with 555 timers and run that into an inductor.  The 555 timer will set up in astable mode to produce an alternating signal at 60 Hz that will get amplified by a MOSFET before running into the transformer. The current from the transformer will go into a diode laddering system which will drive the GM tube.  The signal from the Geiger tube will run into an NPN transistor.  The output pulse of the tube is around 200V, so it needs to have some level of conditioning before it can be counted by the Arduino. Once the output is run into ground they’ll have a digital signal that they can feed back into the Arduino.

 

He tests the circuit in a breadboard to make sure it works.  The output of the Geiger tube is hooked into an oscilloscope.  Matt uses an old aircraft instrument, an ADF with a glow in-the-dark radium dial to test to ensure that a signal is outputted to the scope.  Now that we know the signal is working, we can condition that signal to create a digital pulse that we can measure and count with the Arduino.  The tube output runs through a voltage divider so that it doesn’t fry the transistor.  All that’s left is to 3D print some parts and do some coding using the Arduino IDE.

image

element14 presents  |  About Matt |  Project Videos

  • mosfet
  • radiation detector
  • geiger tube
  • e14presents_airbornesurfer
  • voltage divider
  • oscillator
  • circuit
  • arduino ide
  • ac current
  • gm tube
  • 555 timer
  • breadboard
  • cathode tube
  • matt eargle
  • cdv-700 series
  • npn transistor
  • vcp
  • arduino
  • diode laddering system
  • friday_release
  • inductor
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • davegsm82
    davegsm82 over 8 years ago +4
    Loved the video, I work in Radiotherapy so work with Man-Made radiation, but have also been to Pripyat/Chernobyl etc. I've designed and built my own Geiger counter, which I've called the DMGC-02. Been…
  • davegsm82
    davegsm82 over 8 years ago in reply to airbornesurfer +4
    No worries, I'm quite happy to tell all about my time in Kiev/Pripyat/Chernobyl so please ask away, either here or in PM's, I'm sure others would be interested too! I'm actually in the UK, but there's…
  • 14rhb
    14rhb over 8 years ago +3
    An interesting video, thank you. After watching this I wondered if it was feasible to make the Geiger-Müller tube at home as well. In the past I managed to pull a really good vacuum with a homemade pump…
Parents
  • davegsm82
    davegsm82 over 8 years ago

    Loved the video, I work in Radiotherapy so work with Man-Made radiation, but have also been to Pripyat/Chernobyl etc.

    I've designed and built my own Geiger counter, which I've called the DMGC-02. Been working on it for a few years, features GPS location, SD logging, Nokia LCD display, rechargeable Li-ion battery, Micro USB for charging and Serial data logging. Runs on a PIC, rather than an arduino, but I recon you could easily incorporate some of the features I have. monitor the output voltage with a resistor string and use PWM to control the output to the HV driver transistor etc.




    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 8 years ago in reply to davegsm82

    That's awesome, dude! I'd love to chat about it sometime! That's part of why I used the Arduino: I figured that I could always add more features in the future if I ever wanted to revisit it. Admitted, by the end of the project, I was just glad to have something that worked, lol! One of these days I'll get over to Pripyat and take a tour (I also want to see the "Russian Woodpecker" that's located nearby) as I enjoy those weird quirks of geography--I also want to visit Centralia, PA, and the Northwest Angle, MN, to name but a couple of those spots!

     

    Thanks for watching!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davegsm82
    davegsm82 over 8 years ago in reply to airbornesurfer

    No worries, I'm quite happy to tell all about my time in Kiev/Pripyat/Chernobyl so please ask away, either here or in PM's, I'm sure others would be interested too! I'm actually in the UK, but there's loads of places in the USA that I'd love to visit. This counter has been to the states with me before and I've GPS Mapped a few areas but not found anything fun, I'd love to visit and do some mineral hunting for Uranium ore etc. I'm visiting San-Fran and Vegas, in a month or so, I really want to take a car out to some of the old mines and have a dig in the spoil heaps!

    I get what you mean about just getting something working, I've been there before. It look me long enough just to get the LCD display working on my project, then it skyrocketed from there.

    Re: the Woodpecker, or 'Duga' as it's known, yea I visited there on my trip, it was actually half of the reason for my visit, I really wanted to see the structure as there's some mutterings that it may be sold for scrap and torn down in the coming years. That probably won't happen for a while but be aware that it's possible as that area isn't really contaminated at all, despite it's proximity to the CNPP.

    image

     

    I made a huge album on Imgur with my photo's in it, if anyone would like a look through.

    https://imgur.com/a/4hvGU

    All the best, Dave.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • davegsm82
    davegsm82 over 8 years ago in reply to airbornesurfer

    No worries, I'm quite happy to tell all about my time in Kiev/Pripyat/Chernobyl so please ask away, either here or in PM's, I'm sure others would be interested too! I'm actually in the UK, but there's loads of places in the USA that I'd love to visit. This counter has been to the states with me before and I've GPS Mapped a few areas but not found anything fun, I'd love to visit and do some mineral hunting for Uranium ore etc. I'm visiting San-Fran and Vegas, in a month or so, I really want to take a car out to some of the old mines and have a dig in the spoil heaps!

    I get what you mean about just getting something working, I've been there before. It look me long enough just to get the LCD display working on my project, then it skyrocketed from there.

    Re: the Woodpecker, or 'Duga' as it's known, yea I visited there on my trip, it was actually half of the reason for my visit, I really wanted to see the structure as there's some mutterings that it may be sold for scrap and torn down in the coming years. That probably won't happen for a while but be aware that it's possible as that area isn't really contaminated at all, despite it's proximity to the CNPP.

    image

     

    I made a huge album on Imgur with my photo's in it, if anyone would like a look through.

    https://imgur.com/a/4hvGU

    All the best, Dave.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • airbornesurfer
    airbornesurfer over 8 years ago in reply to davegsm82

    Thanks for sharing your photos, Dave! Super rad!

     

    If you think you'll have time and be of mind to when you visit the area, I'll hook you up with the Desert Dogs (local spelunking group based at my shop)--those guys know where to find all the really cool stuff!

     

    Take care!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • davegsm82
    davegsm82 over 8 years ago in reply to airbornesurfer

    Hey Matthew,

    That sounds like a cool idea! are you based near the Nevada/Cali area? I need to check our Itinerary for the trip, but I think I might be able to convince the wife to do a little prospecting!

    Cheers, Dave.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • airbornesurfer
    airbornesurfer over 8 years ago in reply to davegsm82

    I'm based in Orange County, CA, yeah. The Desert Dogs go all over the SoCal and Nevada area. Send me a message if you're interested and I'll point you to the right person!