Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Raspberry Pi Fallout Terminal PC -- Episode 373
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: kellyhensen
  • Date Created: 20 Nov 2018 7:53 PM Date Created
  • Last Updated Last Updated: 21 Dec 2018 8:24 AM
  • Views 10689 views
  • Likes 9 likes
  • Comments 58 comments

Raspberry Pi Fallout Terminal PC -- Episode 373

image
Raspberry Pi Fallout Terminal PC

element14 Presents  |  DJ Harrigan's VCP Profile  |  Project Videos

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Typing a password by hand is so blase, so why not spice up your daily PC unlocking routine by creating an overly contrived password keeper? In the modern Fallout games, you find many a RobCo terminal lying about ready to reveal secrets from before the great war, but in order to gain access, you often need to “hack” the system. Let’s re-create our own mini terminal to emulate a keyboard and unlock a computer in “real life.”

 

 

Bill of Material:

 

Product NameManufacturerQuantity
Buy Kit

Raspberry Pi 3B+

RASPBERRY PI1Buy Now

PiTFT

ADAFRUIT1Buy Now
Speaker PhatPIMORONI1Buy Now
5VDC Power SupplyXP POWER1Buy Now
Pushbutton SwitchNTE ELECTRONICS1Buy Now
1141 -  Assembled Data Logging Shield For ArduinoADAFRUIT1Buy Now
OnOff ShimPIMORONI1Buy Now
Verbatim 3mm FilamentVERBATIM1Buy Now
Trinket 5V 16MhzADAFRUIT1Buy Now
Power AdapterXP POWER1Buy Now
DC Power ConnectorMCM1Buy Now

 

Additional Parts:

 

Product NameQuantity

M2x6 Screw Flathead

6

M2.5x6 Screw Philips

4

M2.5x10 Screw Philips

4

White, Charcoal, and Hammered Black Spray Paint

1

Micro USB B to USB A cable

1

6mm Tactile Switch

6

 



Attachments:
3D Files.zip
  • terminal
  • robco
  • fallout 3
  • fallout 4
  • bethesda
  • pimoroni
  • fallout
  • game
  • serial terminal
  • hacking minigame
  • curses
  • raspberry pi
  • fallout 76
  • fallout new vegas
  • miniature
  • friday_releasedj
  • hacking
  • friday_release
  • 3d printed
  • e14presents_djharrigan
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mrvolt
    mrvolt over 7 years ago in reply to dougw +2
    Thanks Doug. I think I want to make a slight redesign to make this a general purpose Pi Case for future development.
  • mrvolt
    mrvolt over 6 years ago in reply to skwirl42 +2
    Wow James, I'm stoked you're still going strong on this! Also, you can definitely post the game you're working on. It's only spam if that's the only thing you do post, but you're actually sharing and contributing…
  • mrvolt
    mrvolt over 5 years ago in reply to xxbigladxx +2
    Hi there, There are multiple ways to run a program at boot. Here's a good tutorial: https://www.dexterindustries.com/howto/run-a-program-on-your-raspberry-pi-at-startup/
Parents
  • skwirl42
    skwirl42 over 7 years ago

    I’ve been working on my own. Not having a 3D printer I had the parts printed by a local shop in the colours I wanted them. The print is exactly the same as yours, but I’m still collecting hardware and deciding what I want in there. I want it to have more utility than just the hacking game (such as running pico-8 games), so I’m making some hardware changes.

     

    Here the are the main differences with my plan:

    • Pi Zero, for cost reasons
    • no trinket, since it won’t be interfaced with a PC
    • power will be provided from a panel mount micro USB cable from the hole designed for the trinket (still have to figure out how I’m going to get that physically connected), and will probably have to widen the hole where the trinket was intended to be to make room for that panel mount, and drill screw holes to mount it
    • I reamed out the power jack hole in the back to fit a smaller power button
    • instead of the key caps from the print I’m going to make an 8x2 USB keyboard to fit in the spot, based off of this C64 keyboard hack and using an atmega8 I’ve had lying around for over a decade, and these switches
    • The keyboard will cost a fair bit extra, but it’s a good project on its own

     

    Other than those changes I’m going to stick to the original design.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mrvolt
    mrvolt over 7 years ago in reply to skwirl42

    Very cool, James!

     

    I'm excited to see your take on it. Do you have any photos of your build so far?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skwirl42
    skwirl42 over 7 years ago in reply to mrvolt

    This is the only decent shot I’ve got at the moment. The case still needs some sanding. It doesn’t show up very well in the photo, but the vent is a metallic grey. I also debated whether or not I should leave the washers on with the screws. And the Pi Zero is half visible there.

     

    Another difference, I’ll be using a cobbler to break out the pins from the back of the display. I’ll still need to deal with the I2C pins that the speaker phat uses, but I believe the additional pins are brought out as pads on the back of the display.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skwirl42
    skwirl42 over 7 years ago in reply to mrvolt

    I’ll take some more pics of the case tomorrow, although there’s not much new there. I think I wrecked either the Pi or the on/off shim while soldering them together, since when I connect power absolutely nothing happens. My guess is the shim board didn’t take kindly to the rough treatment it got as I was trying to get it flush with the Pi’s pin header. My soldering skills are not great. I’m a software developer by trade. I’ve got a fork of the hacking game and I made a pull request to your repo for some of my changes.

     

    When I realized that curses on Windows isn’t up to the task of properly displaying essential parts of the game I also started working on a platform abstraction to offer either curses or tcod as the display library. It also abstracts input, because I was considering having a gpio based input on the Pi, or just standard input if that’s not available.

     

    So I guess there is more to show, it’s just not hardware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skwirl42
    skwirl42 over 7 years ago in reply to mrvolt

    And I can’t find the implementation of the hacking game that works inside my RobCo OS system, so I must just have it locally. I’ll figure that out at some point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skwirl42
    skwirl42 over 7 years ago in reply to mrvolt

    Thinking further on this, if I use small snap-dome switches and a silicone membrane I can fit a QWERTY keyboard into the space for the keyboard. Granted, the keys would be small, but it'd have decent tactile feedback and let me use the terminal fully.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skwirl42
    skwirl42 over 7 years ago in reply to skwirl42

    Also, I'd definitely need to get this assembled by whoever makes the PCB, as it'd all need to be small, SMT parts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • skwirl42
    skwirl42 over 7 years ago in reply to skwirl42

    I added the abstracted version of the hacking game here https://github.com/skwirl42/robco-os , so those interested can take a look at the abstraction system and how I applied it in the case of the hacking game.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • skwirl42
    skwirl42 over 7 years ago in reply to skwirl42

    I added the abstracted version of the hacking game here https://github.com/skwirl42/robco-os , so those interested can take a look at the abstraction system and how I applied it in the case of the hacking game.