Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Altair 8800 Laptop -- Episode 419
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 29 Oct 2019 8:26 PM Date Created
  • Last Updated Last Updated: 8 Nov 2019 8:24 AM
  • Views 3777 views
  • Likes 7 likes
  • Comments 6 comments

Altair 8800 Laptop -- Episode 419

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Remember Matt's replica Altair 8800 build from a while back? It should come as no surprise that he's a fan of the retro electronics (see also: Project Hawthorne, Project Essex, and Project Pripyat), but due to lack of space, he keeps mainly portables and smaller form factor devices. Even at a reduced size, the Altair replica didn't sit quite right because it still required a full-sized terminal to function properly. So, in this project, Matt converts the desktop Altair into a self-contained laptop replete with emulated green phosphor screen, toggles, and glorious blinkenlights all in a handsome aluminum case that would not have been out of place during the disco era!

Supplemental Content:

  • Ben Heck's Apple 1 Laptop:
    • Episode 158: Ben Heck's Apple 1 Replica Part 1 Episode
    • Episode 159: Ben Heck's Apple 1 Replica Part 2 Episode
    • Episode 160: Ben Heck's Apple 1 Replica Part 3 Episode
  • Original Altair Replica Build (Project Wumpus):
    • Episode 377: Altair 8800 Replica
  • Project Pripyat:
    • Episode 352: Pripyat - DIY Geiger Counter
  • Project Essex:
    • Episode 409: Commodore SX-64 Restoration
  • Say Hi to Plasma:
    • Plasma2002

Bill of Material:

 

Product Name Manufacturer Quantity
Development Board, Arduino Due, AT91SAM3X8E MCU, 54 3.3V I/O, 12 Analogue Inputs, With Headers ARDUINO 1 Buy Now
Toggle Switch, (On)-Off-(On), SPDT, Non Illuminated, 1MS4T1B1M1 Series, Through Hole, 5 A Multicomp 8 Buy Now
Toggle Switch, On-On, SPDT, Non Illuminated, 1MS Series, Panel Mount, 5 A Multicomp 17 Buy Now
LED, Red, Through Hole, T-1 3/4 (5mm), 10 mA, 2.1 V, 650 nm Multicomp 36 Buy Now
Bipolar (BJT) Single Transistor, NPN, 40 V, 300 MHz, 625 mW, 600 mA, 35 hFE ON/Fairchild 36 Buy Now
Through Hole Resistor, 10 kohm, LR Series, 250 mW, ± 1%, Axial Leaded, 200 V TE 37 Buy Now
Through Hole Resistor, 150 ohm, MCMF0W4 Series, 250 mW, ± 1%, Axial Leaded, 250 V Multicomp 37 Buy Now
Ribbon Cable, Spectra Zipr Planar AMPHENOL SPECTRA-STRIP 1 Buy Now
Premium Female/Male Extension Jumper Wires, 40 x 6" (150mm) Adafruit 2 Buy Now
USB Connector, USB Type B, USB 2.0, Receptacle, 4 Positions, Through Hole Mount, Right Angle Multicomp 1 Buy Now
D Sub Connector, Right Angle, HD15, High Density, Receptacle, 15 Contacts, DE, Solder Multicomp 1 Buy Now
DIN Audio / Video Connector, 6 Contacts, Jack, PCB Mount, Through Hole Right Angle AMP/TE 1 Buy Now
IC & Component Socket, 28 Contacts, DIP Socket, 2.54 mm, 7.62 mm, Phosphor Bronze TE 1 Buy Now
Crystal, Through Hole, 8 MHz, Through Hole, 10.3mm x 5mm, 50 ppm, 18 pF, 30 ppm, AS Series Ralton 1 Buy Now
Microcontroller PIC/DSPIC, PIC32 Family PIC32MX Series, 32bit, 40MHz, 128KB, 32KB RAM, SDIP-28 Microchip 1 Buy Now
Fixed LDO Voltage Regulator, 2.3V to 6V, 178mV Dropout, 3.3Vout, 250mAout, TO-92-3 Microchip 1 Buy Now
LED, Red, Through Hole, T-1 (3mm), 30 mA, 2.1 V, 625 nm Multicomp 1 Buy Now
Ceramic Disc Capacitor, 27 pF, 1 kV, 561R Series, ± 5%, C0G / NP0, 6.4 mm Vishay 3 Buy Now
Multilayer Ceramic Capacitor, 0.1 µF, 50 V, MC Series, ± 20%, Radial Leaded, Y5V Multicomp 2 Buy Now
Tantalum Capacitor, 10 µF, 16 V, MCTA Series, ± 10%, Radial Leaded, 5 mm Multicomp 3 Buy Now
Through Hole Resistor, 82 ohm, MCCFR0W4J Series, 250 mW, ± 5%, Axial Leaded, 250 V Multicomp 1 Buy Now
Through Hole Resistor, 220 ohm, MCF Series, 250 mW, ± 5%, Axial Leaded, 250 V Multicomp 1 Buy Now
Through Hole Resistor, 470 ohm, MCCFR0W4J Series, 250 mW, ± 5%, Axial Leaded, 250 V Multicomp 1 Buy Now
Through Hole Resistor, 4.7 kohm, MCCFR0W4J Series, 250 mW, ± 5%, Axial Leaded, 250 V Multicomp 4 Buy Now
Through Hole Resistor, 100 kohm, MCCFR0W4J Series, 250 mW, ± 5%, Axial Leaded, 250 V Multicomp 1 Buy Now
Electrolytic Capacitor, 10 µF, 16 V, MCGPR Series, ± 20%, Radial Leaded, 5 mm Multicomp 1 Buy Now
DC Power Connector, Socket, 4 A, Cable Mount, Screw Velleman 1 Buy Now
DC Power Connector, Plug, 4 A, Cable Mount, Screw Velleman 1 Buy Now
Jumper (Busbar), Jumper, TSW, MTSW, TLW, DW, EW, ZW, HW, & TSM Series Headers, 2 Positions, 2.54 mm SAMTEC 2 Buy Now
Matrix Board, 1.2 mm, 160 mm, 100 mm Multicomp 1 Buy Now
PCB, Pad-per-hole, Epoxy Glass Composite, 1.57mm, 152.4mmx228.6mm Vector 1 Buy Now

 

Additional Parts:

 

Product Name

header pins: right angle & straight

ps2/usb adapter

USB 84-key mini keyboard

briefcase style laptop case

acrylic

8-inch 4:3 LCD VGA monitor

image
Altair 8800 Laptop

element14 presents  |  About Matt |  Project Videos

  • vt-100 emulator
  • altair-duino
  • DIN Audio/Video
  • terminal emulator
  • te
  • portable altair
  • microchip
  • altair laptop
  • e14presents_airbornesurfer
  • altair arduino laptop
  • 70s laptop
  • ralton
  • altair emulator
  • element14 presents
  • matt eargle
  • mits
  • multicomp
  • altair 8800
  • retrocomputer
  • altair 8800 replica
  • arduino
  • friday_release
  • retro computing
  • 1970s computer
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 6 years ago +1
    Nice episode. I think every engineer will admit that they know how to build a better system after they finally get their original design working. You always learn new things with every build. DAB
  • xeonaj
    xeonaj over 6 years ago +1
    That was just COOOOOOOOOOOOL! (even if I didn't understand the whole thing!)
  • airbornesurfer
    airbornesurfer over 6 years ago in reply to phoenixcomm +1
    Constructive criticism is constructive, and I appreciate that. The keyboard was a bit of an academic exercise as much as it was a technical one--a challenge to myself to build one from scratch (or as much…
Parents
  • xeonaj
    xeonaj over 6 years ago

    That was just COOOOOOOOOOOOL! (even if I didn't understand the whole thing!)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • xeonaj
    xeonaj over 6 years ago

    That was just COOOOOOOOOOOOL! (even if I didn't understand the whole thing!)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • airbornesurfer
    airbornesurfer over 6 years ago in reply to xeonaj

    Thanks! It's okay not to understand as long as you ask the right questions!