Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents How To Make A Custom PCB From Design To Assembly -- Episode 485
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 4 Feb 2021 12:45 AM Date Created
  • Last Updated Last Updated: 12 Feb 2021 8:24 AM
  • Views 11146 views
  • Likes 13 likes
  • Comments 18 comments

How To Make A Custom PCB From Design To Assembly -- Episode 485

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A lot of our videos contain custom PCBs, and those don‘t appear magically out of thin air. In this episode Clem takes you through every step of Custom PCB design and assembly! In a mere 20ish minutes you get a grasp of how much work is in that one building block of a project.

 

Supplemental Content:

 

  • Episode 485: Bonus Content: How To Make A Custom PCB From Design To Assembly - Full Video

  • Episode 385: 20 PCB Design Pitfalls
  • Screaming LM386:  An Audio Amplifier with PCB Art by fmilburn 
  • LockNFC - PCB design by Fred27 
  • Get the EI.O.T Pcb at Aisler.net and solder it yourself:  https://aisler.net/p/TRSDCBZR 
  • Get notified when the EI.O.T is available for purchase or gets a major Update: https://tinyletter.com/mayermakes

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
Fixed LDO Voltage Regulator, 2.1V to 6V, 210mV Dropout, 1.2Vout, 500mAout, SOT-223-3 Microchip 1 Buy Now
USB Connector, USB Type C, USB 3.1, Receptacle, 24 Positions, Surface Mount, Right Angle molex 1 Buy Now

 

Additional Parts:

 

Product Name
ESP32-S2-WROOM
Attachments:
PCBDesign_Resources.zip
element14 presents
How To Make A Custom PCB From Design To Assembly

element14 Presents  |  About Clem  |  Project Videos

  • molex
  • clem
  • microchip
  • e14presents_mayermakes
  • custom pcb
  • pcb design
  • friday_release
  • mayermakes
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 5 years ago +2
    Good episode Clem. Building PCB's are a lot easier than they were in my day. We had to have all of the traces routed by hand. DAB
  • mayermakes
    mayermakes over 5 years ago in reply to kmikemoo +2
    glad you like it, once you made the jump into pcbs you will getthe ideas. just start by recreating a simple desing you already have, maybe a breakout board for a chip. little projects add up to full blown…
  • mayermakes
    mayermakes over 5 years ago in reply to DAB +2
    I have deep respect for all the work that went into making pcbs by hand drwing and etching, so of course I also did it myself with a pen and etching. Knwoing where aprocess came from also helps understand…
Parents
  • Abhinav_937
    Abhinav_937 over 4 years ago

    I'm new to Embedded systems, I have a doubt.

    Why didn't you use a CP2102 USB to UART IC?

    What is the use of that IC IN ESP32 Dev boards?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 4 years ago in reply to Abhinav_937

    this board is designed to use the native USB capabilities of the ESp32S2, a single CP2102 costs more than all the parts on this board combined at current pricing.
    So this design does not need it and it is made specifically to explore the more advanced functionalities that were under development at the time I designed the board.

    Of course you can still communitcate over UART but that would require a USB to Uart bridge like the CP2102. In fact both can be used at the same time, which I sometimes do for debugging.

    that leads me to the second question:
    a normal ESP32 does not have the same USB capabilites as the S2 or S3 /C3, a normal Esp32 needs a USB to uart chip to communicate with a pc as it only has a normal UART port.

    the standard Manufacturer Made Esp32s2 Saola dev kit is basically the same as the old ESP32 variant just with a different chip, that means it does NOT use the native USB port at all. youd need to port it out yourself. this was most likely done to get dev kits out on the market as fast as possible while the native USB stuff was stuill under heavy development.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mayermakes
    mayermakes over 4 years ago in reply to Abhinav_937

    this board is designed to use the native USB capabilities of the ESp32S2, a single CP2102 costs more than all the parts on this board combined at current pricing.
    So this design does not need it and it is made specifically to explore the more advanced functionalities that were under development at the time I designed the board.

    Of course you can still communitcate over UART but that would require a USB to Uart bridge like the CP2102. In fact both can be used at the same time, which I sometimes do for debugging.

    that leads me to the second question:
    a normal ESP32 does not have the same USB capabilites as the S2 or S3 /C3, a normal Esp32 needs a USB to uart chip to communicate with a pc as it only has a normal UART port.

    the standard Manufacturer Made Esp32s2 Saola dev kit is basically the same as the old ESP32 variant just with a different chip, that means it does NOT use the native USB port at all. youd need to port it out yourself. this was most likely done to get dev kits out on the market as fast as possible while the native USB stuff was stuill under heavy development.