Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Bike Speedometer with Arduino and GPS -- Episode 513
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 24 Aug 2021 1:38 PM Date Created
  • Last Updated Last Updated: 27 Aug 2021 7:24 AM
  • Views 13733 views
  • Likes 13 likes
  • Comments 41 comments

Bike Speedometer with Arduino and GPS -- Episode 513

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A bike speedometer and distance display unit, which will let you know the current time, speed you're traveling, and distance you have traveled.

 

Supplemental Content: 

  • Link to the Github: https://github.com/hifromkatie/Speedometer

Bill of Material:

Product Name Manufacturer Quantity Buy Kit
2.85mm Silver Cosmic PLA Filament FILAMENTIVE 1 Buy Now
Arduino Nano 33 IOT ARDUINO 1 Buy Now
PIXXILCD-13P2-CTP-CLB 4D SYSTEMS 1 Buy Now
MIKROE-1714 GPS3 Click GPS module MIKROELEKTRONIKA 1 Buy Now
ANSMANN Battery, Powerbank, 5400 MAH, 5 V, 1A, 2.1A, 2 Port, 120 mm x 12 mm x 67 mm ANSMANN 1 Buy Now
Power Bank, 5V, 5.2 Ah Capacity, 2 Ports, 102 mm x 15.8 mm x 66 mm MULTICOMP PRO 1 Buy Now
CONNECTOR, 3.5MM, PHONO, PLUG, 4POLE LUMBERG 1 Buy Now
SOCKET, 3.5MM, JACK, 4WAY LUMBERG 1 Buy Now
TR FASTENINGS Set Screw, High Tensile, M5, 25 mm, Bright Zinc, Steel 8.8, Hex Head TR FASTENINGS 2 Buy Now
TR FASTENINGS Wing Nut, M5, Steel, Bright Zinc TR FASTENINGS 2 Buy Now

Additional Parts:

Product Name Manufacturer Quantity
Bike frame bag, available from local bike shop Any 1

 

element14 presents
Bike Speedometer with Arduino and GPS

element14 presents  |  About Katie |  Project Videos

Resources-ep513.zip

  • distance
  • push bike
  • bicycle
  • e14p_KD
  • lumberg
  • e14presents_kdumont
  • speedometer
  • tr fastenings
  • e14presents_katiedumont
  • bike
  • filamentive
  • element14 presents
  • katie
  • multicomp
  • gps
  • time
  • arduino
  • friday_release
  • speed
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • baldengineer
    baldengineer over 5 years ago +5
    Great use of the screen. I need to build one of these! (and buy a bike.)
  • beacon_dave
    beacon_dave over 5 years ago +4
    Nice ! Perhaps could move the unused front wheel sensor onto the chainwheel so as you can get a readout of cadence (crank RPM) alongside speed ? Perhaps add a 'change up' / 'change down' alert if the cadence…
  • maxgolmsted
    maxgolmsted over 5 years ago +3
    Love this! Very useful and great use of the circular screen.
  • hifromkatie
    hifromkatie over 3 years ago in reply to beacon_dave

    That looks interesting, the problem with distance travelled is it doesn't always equate to work you put in to travel that distance, so being able to gauge the work you've put in would be really cool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago

    I was watching this presentation from Analog Devices about a bicycle power meter and thought it may be of interest as a possible enhancement to this project.

    Bicycle Power Meter
    https://www.analog.com/en/education/education-library/videos/6310433088112.html

    At first, I thought they were going to using a custom crank with built-in strain gauge, but instead they have attached a couple of strain gauges to an existing crank.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Adam_A
    Adam_A over 4 years ago in reply to hifromkatie

    Yes, the main idea is that I pick a project then I modify it by code and shape, however he wants it so there is a detailed tutorial on how to make that project work. 
    afterword I would modify things like the 3D case, or the internal code (like adding more features to the speedometer) he still wants to it be kind of identical to the original project however with minor modifications.

    (the goal being to replicate a project "make it work" then modify it in different ways) This is to guarantee that you have a working project work off from then modify it. 

    The idea of me using a different display would be great however I have no guarantee of it working, like If I do not get the parts to work together that would be a big issue as I may not have anyone to get help from (as I'm not the best at coding) then I would not pass the project. So it would be risky to use something which isn't in the original project, furthermore I would have to also convince my teacher how I can change the part and code it to work (which I'm not sure of).

    In the meantime I'm defiantly going to have a look at the smaller display you used and see if I would be able to figure out how to use it with this project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 4 years ago in reply to Adam_A

    If it's for a school project then modifying the code to use a different screen is probably what the teacher would want.
    I guess it's a project to show your electronics/coding, so the ability to modify something from another person would probably get you more marks than just following the instructions to make the project.

    The other cost saving modification I can think of would be to drop the LCD screen and change the project to display the speed and/or distance travelled on a set of 7 segment displays,
    or yyou could use a much cheaper little oled screen (I've used a nice little one in a recent project, a MIDAS Graphic OLED, 128 x 32 Pixel size. You can find that project here: /challenges-projects/element14-presents/project-videos/w/documents/27787/episode-568-how-to-make-a-custom-soundboard-with-the-stm32f4-using-freecad as that has a link to the part

    You would need to modify the case design to fit the screen you pick though as they are all rectangular options

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Adam_A
    Adam_A over 4 years ago in reply to hifromkatie

    Thank you for the reply, I'm currently adding all the project costs together and it's adding up to $225 USD (delivered to my school) so im not sure on what to do as this is out of budget, the most expensive part being the 4D systems Display, 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to hifromkatie

    There are a couple of nice examples of the GC9A01 display in the videos here:

    Boat gauges:
    https://www.youtube.com/watch?v=y_H7HM0oyoo

    Smart Watch:
    https://www.youtube.com/watch?v=XM_6qEAdFnM

    The code used for each is linked in the description.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • hifromkatie
    hifromkatie over 4 years ago in reply to Adam_A

    Hi, this sounds like a great school project.
    You could use a screen like that instead, however, the dimensions on the 3D print files may need to be changed to fit the alternative part, and more importantly the code would need a rewrite to work with that screen.
    I used the 4D systems screen workshop software to configure the screen, and translate the values passed to it to the graphics displayed, but this wouldn't work with that screen. I've never used that particular screen, so I couldn't tell you how easy it would be to display the information either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Adam_A
    Adam_A over 4 years ago

    Hello I'm doing this as a school project, would it be possible to use this display instead https://a.co/d/h9Gr9c7 (GC9A01 Driver SPI Interface for Arduino) ? this one is much more affordable and accessible, if possible to use it how would I be able to integrate it? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • MwanyamakiJr
    MwanyamakiJr over 4 years ago in reply to cstanton

    when i try to compile i get an error that say 'Serial1'was not declared in this scope.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 4 years ago in reply to lucart84

    The zip file has been replaced with the correct version.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>