Project Videos
  • Challenges & Projects
  • element14 presents
  • Project Videos
  • More
  • Cancel
Project Videos
Documents Modding a Super 8 Camera into a Digital One -- Episode 382
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Project Videos to participate - click to join for free!
Related
Recommended
Engagement
  • Author Author: Matt
  • Date Created: 19 Dec 2018 4:20 AM Date Created
  • Last Updated Last Updated: 23 Jun 2025 12:39 PM
  • Views 13463 views
  • Likes 9 likes
  • Comments 30 comments

Modding a Super 8 Camera into a Digital One -- Episode 382

Watch the Episode

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

One mans trash is a makers treasure! Clem found a super8 camera in the trash, and soon realised that the original analogue films and the processing is crazy expensive nowadays. So he creates a drop in replacement for the film cartridge that turns the super8 camera into a digital one! But that is easier said than done!

Clem's Frequently Asked Questions

Why is the image quality so bad compared to modern cameras?

This super 8 camera is 47 years old. The films originally used were very light sensitive (much more than any modern sensor that could fit in there) and even with the correct film home videos filmed in super 8 looked like that. The lens is what determines picture quality for the most part. if you want to see the difference a lens makes check out videos on my personal channel (http://youtube.com/mayermakes) and watch some the oldest and newest videos those were shot with the exact same camera(Nikon D3300) but with different lenses(old: Kit lens f4.5, new Nikkor 35mm prime lens f1.8) and more light. you may understand it better if you see it for yourself.

So the look of the footage I've taken with the Super8 camera is pretty authentic for "1970s home video". that is just how it was when your Parents were young, or even grandparents depending on how old you are.

Couldn't you just remove the lens of the picam and put it directly in place of the film?

No.Tried that in multiple version, but no the focal distance and the sensor width are extremely different, you can only get a blotch of light by doing that+ you can't even get to the exact same plane because of parts that would hold the original film and should not be damaged. 

How did you get it to focus then?

Extended the picam lens to near maximum and found a position that allowed me to get alignment with the shutter by trial and error, focused to UE and pushed back and forth until the image was mostly sharp. this ended up being a position multiple centimetres back which resulted in the need to extend the case.


Why the big case?

See above + I damaged multiple flat flex cables when fitting everything in the tiny version ,with only a day left until deadline i had to make sure that won't happen again + easier to install the buttons.

Will you do another version?

I plan to but It may be  a longer term project with dedicated self developed hardware.

if you would like to see that leave it in the comments below.

Supplemental Images and Links:

-  Episode 382 Resource Files  

-  Super 8 Camera Digitizer -- Episode 505  

{gallery} My Gallery Title

image

image

image

image

 

Bill of Material:

 

Part

Raspberry Pi 3A+

Raspberry Pi 1 Buy Now

Raspberry Pi Camera

Raspberry Pi 1 Buy Now
Adafruit powerboost 1000 Adafruit 1 Buy Now
Tactile Switch, B3F Series, Top Actuated, Through Hole, Round Button, 100 gf, 50mA at 24VDC OMRON 1 Buy Now
Signal Relay, 3 VDC, DPDT, 1 A, TQ Series, Through Hole, Non Latching Panasonic 1 Buy Now
METAL FILM RESISTOR, 1KOHM, 500mW, 1% TT Electroniks Welwyn 1 Buy Now
LED, Red, Through Hole, 5mm, 20 mA, 1.8 V, 643 nm MULTICOMP 1 Buy Now
molex Board Connector FFC / FPC Board 1 mm, 15 Contacts, Receptacle, Easy-On 52610, Surface Mount molex 2 Buy Now
molex Premo Flex Jumper FFC / FPC Cable, 14 Core, 1 mm, Same Sided Contacts, 12 ", 305 mm, White molex 1 Buy Now

 

Additional Parts

Product Name

Stranded Wire

Used Super 8 camera

Kodak Super 8 Film cartridge for Size and Position Reference

3D printed Case and Buttons (files are available for download)

image
Modding a Super 8 Camera into a Digital One

element14 Presents  |  MAYER MAKES VCP Profile  |  Project Videos

  • clem
  • super 8
  • e14presents_mayermakes
  • element14 presents
  • camera
  • upcycling
  • friday_release
  • mayermakes
  • e14p_CMM
  • Share
  • History
  • More
  • Cancel
Actions
  • Share
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 7 years ago in reply to davedarko +2
    yes, but you need it to compensate the focal distance and sensor widht inside the camera. without the original lens you can´t see anything. it is extended to nearly it´s maximum.
  • mayermakes
    mayermakes over 7 years ago +2
    on popular demand here are some FAQs: Why is the imagequality so bad compared to modern cameras? this super 8 camera is 47years old. The filmes originally used were very light sensitive (much more than…
  • devinlhardy
    devinlhardy over 5 years ago +2
    Hi Clem, My name is Devin L. Hardy, I am a filmmaker/writer living in Los Angeles, CA. My resume consists of stints at 21st Century Fox, Academy of Motion Picture Arts and Sciences, and Netflix, just to…
Parents
  • DAB
    DAB over 7 years ago

    Very good episode Clem.

     

    I have considered doing something similar.

    I think you are right about not using the RPi camera without its lens. The normal footprint for the lens is 8-mm and your RPi camera is much smaller than that.

    What your doing now is called eyepiece projection. You will need to position the RPi camera very precisely so that the focal point of the RPi lens is at the focal point of the 8-mm camera lens.

    To do this well, you will need to set up the 8-mm camera with a well illuminated image about ten or so feet away. It is not a full far field, but it might be good enough if you have focus control on the 8-mm lens.

    Then you adjust the position of the RPi camera until the image is in focus. Then run through the zoom range of the 8-mm lens to see how well the image stays in focus.

    When you are happy with it, lock it down.

    It will never be a great camera, but it will be a one of a kind retro looking digital camera.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to DAB

    You are desribing my procedure in the best way anyone could phrase it. it was a huge feat of trial and error to get close to the right combination of "inner lens" and Super8 lense.
    The projection idea also came to my mind but I could not pull it off, even shining a studio light directly into the lense did not generate an easy to focus image in the close range,  so I got back to triying out a few combinations until I got something that was recognizable as an image (seen in the video as the direct stream from the pi)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago in reply to mayermakes

    Hi Clem,

     

    If you can remove the 8-mm camera lens, you can set it up on an optical bench to get a better measurement as to where the focal point is.

    After that, you can bench test the RPi camera to find its focal point in relation to the other lens.

    The problem is the poor quality of the RPi lens. It really limits your performance. That and the low sensitivity of the sensor.

     

    Still, it is a good way to repurpose an old camera.

     

    FYI, if you try to go for an IR camera with this set up, be aware that the focal point will shift, so you will have to refocus the RPi camera using IR light only.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 7 years ago in reply to mayermakes

    Hi Clem,

     

    If you can remove the 8-mm camera lens, you can set it up on an optical bench to get a better measurement as to where the focal point is.

    After that, you can bench test the RPi camera to find its focal point in relation to the other lens.

    The problem is the poor quality of the RPi lens. It really limits your performance. That and the low sensitivity of the sensor.

     

    Still, it is a good way to repurpose an old camera.

     

    FYI, if you try to go for an IR camera with this set up, be aware that the focal point will shift, so you will have to refocus the RPi camera using IR light only.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mayermakes
    mayermakes over 7 years ago in reply to DAB

    good idea, but the lens is not detachable from the camera