The Learning Circuit
  • Challenges & Projects
  • element14 presents
  • The Learning Circuit
  • More
  • Cancel
The Learning Circuit
Documents Series & Parallel Circuits -- The Learning Circuit 02
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join The Learning Circuit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 28 Nov 2017 9:34 PM Date Created
  • Last Updated Last Updated: 29 Nov 2017 8:24 AM
  • Views 5738 views
  • Likes 9 likes
  • Comments 12 comments
Related
Recommended

Series & Parallel Circuits -- The Learning Circuit 02

image

element14's The Ben Heck Show

Join Karen as she shares her enthusiasm for teaching STEM subjects, gives you what you need to know to get started on electronics projects, and more.

Back to The Ben Heck Show homepage image

The Learning Circuit
sudo Sergeant
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In a previous episode, Karen made a simple circuit using some common everyday items.  Now she’ll demonstrate the difference between parallel and series circuits by adding additional voltage and another bulb to her simple circuit.  She’ll also cover the difference between stranded and solid wire and use a multimeter to demonstrate the difference in how voltage is distributed in a parallel and series circuit.

Make Your Own!

Parts & Products:

Product Name

Part Link

Hookup Wire - Red, 22 AWG, 25ft, solidBuy NowBuy Now
Hookup Wire - Black, 22 AWG, 25ft, solidBuy NowBuy Now
2 AA Battery HolderBuy NowBuy Now
AA Batteries (4pk)Buy NowBuy Now
Lamp Holder (10pk)Buy NowBuy Now
2.47V Miniature Screw Incandescent Lamp Bulbs (10pk) Buy NowBuy Now
Tenma Digital MultimeterBuy NowBuy Now

 

Additional Materials

Product Name

Metal Paper Clips
Brass Paper Fasteners
Cardboard

 

 

Download the Introduction to Circuits featuring Karen in eBooks!

 

 

Simple circuits such as the ones Karen demonstrates are an easy way to learn about the difference between simple and parallel circuits. In a Series Circuit, all components are connected end-to-end to form a single path for electrons to flow.  In a Parallel circuit, all components are connected across each other to form two sets of electrically common points.

 

Another consideration you’ll need to understand when getting started with electronics projects is your choice between using stranded or solid wires.  Both types of wiring are effective means of transmitting electricity, however, a stranded wire is more efficient in sending the electrons through your circuit.  It’s also better suited for more intricate usages such electronic devices and circuit board where it offers the flexibility to be bent or twisted to connect electronic components.  Solid wire is frequently used for outdoor or rugged applications where wire may be exposed to corrosive elements, adverse weather conditions, or frequent movement. It’s also a good choice for smaller projects where the flexibility of stranded wire makes it difficult to use.

 

Karen uses solid wire to demonstrate the difference between series and parallel circuits because it’s stiff and stays attached better.  In electronics, a node refers to any point on a circuit where two or more circuit elements meet. In a schematic, the node will be the wires between the components.  In a circuit the current flows from high voltage to a lower voltage. The current flows through every path it can take to the point of lowest voltage (commonly referred to as ground).  Two components are said to be in series if they share a common node and the same current flows through them.  If the components share two common nodes then they are said to be in parallel.

 

What other basic electronic concepts would you like to learn about?

 

Let us know in the comments below! 

  • learn electronics
  • parallel circuit
  • the learning center
  • e14presents_makerkaren
  • passive_featured
  • nodes
  • theheckwithkaren
  • starter projects
  • serial circuit
  • battery
  • voltage
  • schematic
  • stem projects
  • thelearningcircuit
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +2
    Nice episode Karen. One slight slip at the end. The parallel lights get the same voltage, not necessarily the same power from the batteries. You might want to add a quick view of Kirchoff's Law as you…
  • Sean_Miller
    Sean_Miller over 8 years ago +1
    Yep...like they say, Complex is easy, Simple is hard! Funny story...my boy and I started adlibbing our (embarrassingly small) channel recently to be more casual in our videos. After putting 5 hours into…
  • Sean_Miller
    Sean_Miller over 8 years ago +1
    I'll definitely take a look and feed back. Your last video had a lot of positive comments - that's a good sign for the style of delivery, although definitely not the only metric to watch. For our channel…
Parents
  • Sean_Miller
    Sean_Miller over 8 years ago

    Great video series.  Stick to it as it will add to the channel greatly over time as well as Sudo Sergeant. 

     

    Similar to DAB's comment, one thing I would be sensitive to is the use of phrases like "volts of power" and "its getting volts".  When folks are learning for the first time, they analyze every word for its exact meaning.  In this case, the loose terms may cause for confusion or a misunderstanding between volts, current, and power - and the effect on voltage along the path with components in series. 

     

    For "volts of power", just say "volts". 

     

    For "it's getting volts", avoid describing volts like its an independent entity of "force" or "power".  Using the common water example, you want them to think of voltage as the height of a dam, not the size of the lake.

     

    Just as others recommended on YouTube, ohms law would be a great next video - and going back to the demo circuits to drive the principles home.  In particular, it would be a good practical example to explain why the two voltages were different in the series bulbs.

     

    Feel free to bounce your scripts out here early for collaboration.

     

    See ya',

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • makerkaren
    makerkaren over 8 years ago in reply to Sean_Miller

    That's a very good point, Sean. Thank you. I've worked with kids a lot and I struggle to explain basic concepts in a simple manner with terms that don't seem too foreign or overwhelming. I often use "power" as a lazy out, which obviously is a terrible idea since it has a specific meaning once you get past the very basics. I get stuck in a chicken and egg loop in that I want to use the correct terminology, but to do that, I have to take the time to explain what all of it means and then I fall down a well of tangents. Thanks for the feedback! I'm still working on a good path of explaining basics in small, bite-sized pieces that are factually accurate, but simple to understand without having to explain EVERYTHING at once.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • makerkaren
    makerkaren over 8 years ago in reply to Sean_Miller

    That's a very good point, Sean. Thank you. I've worked with kids a lot and I struggle to explain basic concepts in a simple manner with terms that don't seem too foreign or overwhelming. I often use "power" as a lazy out, which obviously is a terrible idea since it has a specific meaning once you get past the very basics. I get stuck in a chicken and egg loop in that I want to use the correct terminology, but to do that, I have to take the time to explain what all of it means and then I fall down a well of tangents. Thanks for the feedback! I'm still working on a good path of explaining basics in small, bite-sized pieces that are factually accurate, but simple to understand without having to explain EVERYTHING at once.