Products
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
VCP Program
  • Challenges & Projects
  • element14 presents
  • VCP Program
  • More
  • Cancel
VCP Program
Documents A Bald Engineer Video: MOSFET Tutorial
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join VCP Program to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: pchan
  • Date Created: 20 Jun 2018 5:32 PM Date Created
  • Last Updated Last Updated: 1 Sep 2019 2:51 PM
  • Views 1703 views
  • Likes 3 likes
  • Comments 1 comment
Related
Recommended

A Bald Engineer Video: MOSFET Tutorial

image
MOSFET Tutorial

Back to Bald Engineer's VCP Profile  |  Learning Center

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

MOSFETs are the most common transistors used today. They are switches that can be used an Arduino, BeagleBone, or Raspberry Pi. When it comes down to it, MOSFETs are pretty complicated devices. This video will cover the basics of what you need to use them in your circuit, including calculating if you need a heat sink or not. Learn what they are and how to use them.

 

 

  • bald_engineer
  • e14presents_baldengineer
  • jlewis
  • vcp program
  • mosfet_tutorial
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 8 years ago +4
    This video is misleading in that it confuses Vgs(th) with the Vgs for some specified Gate-Source resistance, for example on the IRLI540N Vgs(th) is between 1 and 2 V for 250uA drain current but eh on resistance…
Parents
  • michaelkellett
    michaelkellett over 8 years ago

    This video is misleading in that it confuses Vgs(th) with the Vgs for some specified Gate-Source resistance, for example on the IRLI540N Vgs(th) is between 1 and 2 V for 250uA drain current but eh on resistance is specified for Vgs = 4V, 5V or 10V.

     

    The video keeps referring to Vgs threshold as if it were the working Vgs for low on resistance, which it is not.

     

    Vgs(th) is the gate source voltage below which the device is turned off, it is not the working gate source voltage for switching applications.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 8 years ago

    This video is misleading in that it confuses Vgs(th) with the Vgs for some specified Gate-Source resistance, for example on the IRLI540N Vgs(th) is between 1 and 2 V for 250uA drain current but eh on resistance is specified for Vgs = 4V, 5V or 10V.

     

    The video keeps referring to Vgs threshold as if it were the working Vgs for low on resistance, which it is not.

     

    Vgs(th) is the gate source voltage below which the device is turned off, it is not the working gate source voltage for switching applications.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down