WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Blog Making an Analog Discovery 3 prop to "tear down."
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: baldengineer
  • Date Created: 26 Jul 2023 3:56 PM Date Created
  • Views 2202 views
  • Likes 11 likes
  • Comments 2 comments
Related
Recommended

Making an Analog Discovery 3 prop to "tear down."

baldengineer
baldengineer
26 Jul 2023
Simple Analog Discovery 3 3D printable model

In Workbench Wednesdays #76, I looked at Diglent's Analog Discovery 3. This device is a long-anticipated, by me anyway, update to their incredibly powerful and useful Analog Discovery 2.

One of the first things that struck me about the AD3 is that there were no screws like the AD2. Nor were the screws needed on the Analog Discovery 2 since you could see inside.

Initially, I planned to open up the Analog Discovery 3. But after struggling with the plastic pieces for a few minutes, I decided I was more likely to damage it than open it.

Fortunately, before I tried to open it up, I had the idea to "bash" it open on video. I was going to do some clever editing to slip the PCB inside a pile of broken plastic pieces as the "tear down."

I had already created the breakable mock-up before I realized I couldn't open it. So, I decided to do the joke anyway.

Real analog discovery 3 on left and 3d printed on right

I made the model using two pieces. One for the outer frame and one for the "lid." The outer edge has a small lip where I glued the "lid." Physically, this matched the real AD3 reasonably well. But, it had two significant problems. First, my green filament was nowhere near the dark Digilent color. And the lid had noticeable 3d printing artifacts.

real ad3 next to my painted frame

The color was an easy fix. I found some green paint at a craft supply store. Without mixing it, the result was shockingly close to the original color. And with a few coats, the 3D-printed lines mostly went away.

multiple 3d printed ad3s getting painted

Also, I remembered one of my favorite lines from the movie "Contact." It goes something like: "Why have one when you can have two for the price of double?" Basically, always build a spare. So, I printed and painted enough parts to make three AD3 mock-ups. I planned to break two of them and save the third. (And that is what I did!)

3d printed ad3 lids

Dealing with the fill artifacts on the lid was complicated. Ironing the top layer made the artifacts worse! And I couldn't just add more layers or even go for a solid fill. I needed the lid to be fragile. So I filled the defects with some XTC resin and several layers of paint. It wasn't perfect, but the lids looked much better after that.

adding a layer of matte paint

Also, I went one step further and painted the edge of the lid with matte-black paint. The real AD3's top has a similar two-tone style to it. The very top layer is shiny, and the "lower" layer is matte.

image

After that, I went bashy-bashy with my weighted hammer.

image

Contrary to some belief, the inside was not printed with a fill. However, I did "fill" it manually with random 3D-printed pieces and torn in-fill. I hoped to get more pieces flying around after the hammer's impact.

You can download the STLs here.

Anyway, the Analog Discover 3 is a great tool. And I would never consider breaking a real one. But it was a lot of fun to 3d print one and then hit it with a hammer.

  • Sign in to reply
Parents
  • DAB
    DAB over 3 years ago

    I detect a level of frustration relief in that comment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 3 years ago

    I detect a level of frustration relief in that comment.