WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Forum What has been your experience with low-temperature solder?
  • Episodes
  • Blog
  • Forum
  • Quiz
  • Files
  • Members
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 114 subscribers
  • Views 14978 views
  • Users 0 members are here
  • low-temp
  • solder
  • soldering
  • reflow soldering
Related

What has been your experience with low-temperature solder?

baldengineer
baldengineer over 5 years ago

Recently I found Chip Quik Sn Bi Ag Solder PasteChip Quik Sn Bi Ag Solder Paste. It is a low-temp alloy with Bismuth (and Silver.) When using hot air to solder parts, or during re-work, it makes the process go so much faster. It melts around 140C. It also does not appear to need refrigeration and has a long shelf-life. With all of those positives, I'm wondering what the downsides to using it are compared to more "traditional" solder alloys.

 

So whether positive or negative, what has been your experience when using "low temp" solder?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +5
    It is pretty useful when removing components with an iron because it replaces the existing solder and stays molten long enough to move the iron around to heat up and melt the solder at all pins. The down…
  • geralds
    geralds over 5 years ago +5
    Hi James baldengineer Well for me: For many decades I have deliberately not used low-temperature solder because that has several problems. First: the alloy. If this is not adapted to the material of the…
  • shabaz
    shabaz over 5 years ago +4
    Hi James, I've not used it much, but did find it useful for QFN, where it can take me ages to put on a part and I may need to rework it a few times, because I don't use QFNs often enough to get good at…
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 5 years ago

    One has to be very careful when using low-temp solder on existing leaded solder joints. Apparently, if there’s any lead involved, such as with pre-tinned wires or leads, the combination of Bi58Sn42 and the lead can lower the melting point to 95 C and create very weak and brittle joints that can be pried apart with a toothpick.

     

    I use low-temp solder for all tricky to solder ICs on prototype boards only. It can never leave the lab bench! As shabaz said, it is perfect to solder QFNs, I also did BGA with hot air and low temp solder successfully.

    - W.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 5 years ago in reply to wolfgangfriedrich

    Yes, that's an important point.

     

    Solder - Wikipedia

    Different elements serve different roles in the solder alloy:

    • Bismuth significantly lowers the melting point and improves wettability. In presence of sufficient lead and tin, bismuth forms crystals of Sn
      16Pb
      32
      Bi
      52
      with melting point of only 95 °C, which diffuses along the grain boundaries and may cause a joint failure at relatively low temperatures. A high-power part pre-tinned with an alloy of lead can therefore desolder under load when soldered with a bismuth-containing solder. Such joints are also prone to cracking. Alloys with more than 47% Bi expand upon cooling, which may be used to offset thermal expansion mismatch stresses. Retards growth of tin whiskers. Relatively expensive, limited availability.

     

     

    Eutectic system - Wikipedia

     

    Gerald

    ---

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • geralds
    geralds over 5 years ago in reply to wolfgangfriedrich

    Yes, that's an important point.

     

    Solder - Wikipedia

    Different elements serve different roles in the solder alloy:

    • Bismuth significantly lowers the melting point and improves wettability. In presence of sufficient lead and tin, bismuth forms crystals of Sn
      16Pb
      32
      Bi
      52
      with melting point of only 95 °C, which diffuses along the grain boundaries and may cause a joint failure at relatively low temperatures. A high-power part pre-tinned with an alloy of lead can therefore desolder under load when soldered with a bismuth-containing solder. Such joints are also prone to cracking. Alloys with more than 47% Bi expand upon cooling, which may be used to offset thermal expansion mismatch stresses. Retards growth of tin whiskers. Relatively expensive, limited availability.

     

     

    Eutectic system - Wikipedia

     

    Gerald

    ---

    • Cancel
    • Vote Up +4 Vote Down