WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Forum What has been your experience with low-temperature solder?
  • Episodes
  • Blog
  • Forum
  • Quiz
  • Files
  • Members
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 114 subscribers
  • Views 14977 views
  • Users 0 members are here
  • low-temp
  • solder
  • soldering
  • reflow soldering
Related

What has been your experience with low-temperature solder?

baldengineer
baldengineer over 5 years ago

Recently I found Chip Quik Sn Bi Ag Solder PasteChip Quik Sn Bi Ag Solder Paste. It is a low-temp alloy with Bismuth (and Silver.) When using hot air to solder parts, or during re-work, it makes the process go so much faster. It melts around 140C. It also does not appear to need refrigeration and has a long shelf-life. With all of those positives, I'm wondering what the downsides to using it are compared to more "traditional" solder alloys.

 

So whether positive or negative, what has been your experience when using "low temp" solder?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 5 years ago +5
    It is pretty useful when removing components with an iron because it replaces the existing solder and stays molten long enough to move the iron around to heat up and melt the solder at all pins. The down…
  • geralds
    geralds over 5 years ago +5
    Hi James baldengineer Well for me: For many decades I have deliberately not used low-temperature solder because that has several problems. First: the alloy. If this is not adapted to the material of the…
  • shabaz
    shabaz over 5 years ago +4
    Hi James, I've not used it much, but did find it useful for QFN, where it can take me ages to put on a part and I may need to rework it a few times, because I don't use QFNs often enough to get good at…
Parents
  • Andrew J
    Andrew J over 5 years ago

    Sometimes the most innocuous question leads to some really useful insights. 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 5 years ago in reply to Andrew J

    No kidding!

     

    I love the responses from the community on questions like these.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 5 years ago in reply to Andrew J

    No kidding!

     

    I love the responses from the community on questions like these.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 5 years ago in reply to baldengineer

    For prototypes I would normally use tin/lead for convenience and good results in a prototype process and then we would use standard lead free for production

     

     

    I've been looking at using Tin/Bismuth solder for a new production process.

    We need lead free and low melting point (because we have a special component that can't take more than 220C).

     

     

    geralds  raises some interesting points:

     

    The lead issue - not a problem - the whole point is to have a lead free process, all components are bought lead free.

    Care should be taken with whatever other coatings are used on compent pads.

    Could be a problem with mixed assemblies (like BGA where the solder balls and the solder paste get mixed together).

     

    Temperature range - unless a max joint temperature of 85C is OK - then forget it. We are OK since ours is an ultra low power product with a limited temperature range.

     

    Adding silver, massively improves joint strength and stability.

     

    I'll be trying some: Sn42/Bi57.6/Ag0.4 when it arrives.

     

    Using low mp solder to "wash" other solder off a board for repair is fine if the alternative is a dead board.

    The reliability of the repair will depend on the skill of the operator and other things that may be hard to estimate.

     

    MK