WorkBench Wednesdays
  • Challenges & Projects
  • element14 presents
  • WorkBench Wednesdays
  • More
  • Cancel
WorkBench Wednesdays
Documents How to Decide Which Type of Flux to Use and How to Use Flux! - Workbench Wednesdays 59
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join WorkBench Wednesdays to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: tariq.ahmad
  • Date Created: 21 Jul 2022 3:42 PM Date Created
  • Last Updated Last Updated: 17 Aug 2022 7:24 AM
  • Views 643303 views
  • Likes 3 likes
  • Comments 13 comments
Related
Recommended

How to Decide Which Type of Flux to Use and How to Use Flux! - Workbench Wednesdays 59

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Flux makes soldering easier. It removes oxide layers, gets contaminants out of the way, and makes for better joints. But there are so many different types of flux and even more ways to apply it. This video goes over the different types of Rosin (R, RA, RMA), Resin, Organic, and Inorganic flux. Then it shows what kind of residue gets left over. And explains why “NO Clean Flux” actually needs to be cleaned (in most cases). Not sure which flux to get? Check out this video.

See lots more information, videos and member advice on PCB Design and Prototyping

Supplemental Content:

  • WorkBench Wednesday 30: Ceramic Capacitor Voltage Effect
  • Workbench Wednesday 06: Health and Fumes
  • Datasheet for CHIP QUIK SMD 291 Flux Gel
  • Datasheet for CAIG Flux Paste
  • Datasheet for GC Electronics Liquid Rosin
  • Datasheet for Kester Water Soluble Pen
  • Datasheet for MG Chemicals Liquid Rosin
  • Chemtronics: What is Flux
  • MG Chemicals Flux Removal Guide
  • IPC J-STD-004 Table of Contents

Bill of Material:

Bill of Materials

Product Name Manufacturer Quantity Buy Kit
Solder Flux RMA, Soldering, Jar, 56 g CAIG LABORATORIES 1 Buy Now
Solder Flux, Rosin, Soldering, Tub, 2 oz GC ELECTRONICS 1 Buy Now
Solder Flux, No Clean, Soldering, Syringe, 10 g CHIP QUIK 1 Buy Now
Needle Tips, Dispensing, Assorted, 1/2 " Length, 16g - 27g, 30 Piece CHIP QUIK 1 Buy Now
Solder Flux, Water Soluble, Soldering, Pen Applicator KESTER 1 Buy Now
FLUX BRUSH, ROUND HANDLE, PK25 WELLER 1 Buy Now
Solder Flux, Rosin Activated RA, Soldering, Bottle, 125 ml MG Chemicals 1 Buy Now
Clean Room Wipes (Polyester) 1 Buy Now
 


element14 presents

element14 Presents  |  About James |  Workbench Wednesdays

  • rosin
  • No Clean
  • Water Soluble
  • soldering
  • workbench wednesdays
  • flux
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • koudelad
    koudelad over 2 years ago

    I would appreciate an advice on choosing flux / cleaning after soldering. I have a sensor board with a capacitive sensor. This sensor got damaged by an exposure to alcohol. I need to replace the sensor, getting if off the board will be simple, but how to solder a new one? I should use flux, but I can't clean it with alcohol after that. Or is the only option using a precisely placed solder paste? The sensor package is DFN6 / DFN8.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to koudelad

    I am curious to know how alcohol caused a failure.

    Manufacturer's often use an aqueous wash stage after soldering, It needs a proper drying stage as well.

    There are other chemicals that can clean flux, but I'm not sure they are more benign than alcohol.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 2 years ago in reply to dougw

    It is a general, but know very well known effect harmful to all capacitive sensors. I haven't heard about it until last year, when I bought a new humidity sensor (manufactured and calibrated in the same facility as another one) and there was a perfect match of temperature measurements, but difference in humidity measurement). The difference was higher at low relative humidity levels and lower at high relative humidity levels. As an example, have a look at this document, section Exposure to chemicals: https://sensirion.com/media/documents/6D95AA80/616446E3/Sensirion_AppNotes_Humidity_Sensors_Handling_Instructions.pdf

    The only way to get out of it is to bake the sensor at 100-105 Centrigrades for 10 hours - which might damage connectors / displays and other components on the PCB.

    Here is an example of my measurements, the azure color belongs to a new sensor, purple to the contaminated one.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 2 years ago in reply to koudelad

    I'm not sure I understand. The performance of many types of sensor is adversely affected by ingress of many liquids and particulates. Such sensors are generally masked (with a sealed cover) if the circuit board is to be exposed to such liquids during the manufacturing and assembly processes. There should be no flux in the sensor, so flux cleaner doesn't need to go in there either. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • koudelad
    koudelad over 2 years ago in reply to dougw

    The sensor gets a non-linear offset when exposed to alcohol. I exposed it to too much alcohol apparently and have two options. Bake the sensor for 10 hours at 100-105 Centigrades (and damage the rest of the PCB) or replace it. If I replace it, it is a good idea to use flux, so it needs to be cleaned after soldering, which gets me to my starting point - there is a new sensor damaged by too much alcohol.

    I should probably try to remove it without flux and place it back also without flux, or using some solder paste. (I haven't done this before, I always use flux.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • koudelad
    koudelad over 2 years ago in reply to dougw

    The sensor gets a non-linear offset when exposed to alcohol. I exposed it to too much alcohol apparently and have two options. Bake the sensor for 10 hours at 100-105 Centigrades (and damage the rest of the PCB) or replace it. If I replace it, it is a good idea to use flux, so it needs to be cleaned after soldering, which gets me to my starting point - there is a new sensor damaged by too much alcohol.

    I should probably try to remove it without flux and place it back also without flux, or using some solder paste. (I haven't done this before, I always use flux.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 2 years ago in reply to koudelad

    Pure isopropyl alcohol does not leave a residue. If something has been dissolved in it or it has picked up contaminants, those will remain after the alcohol evaporates. Alcohol could presumably get trapped in the sensor so the bake period is to get it to evaporate even though there is not much air in the sensor. Any elevated temperature would speed evaporation - it probably doesn't need to be 100 degrees. 100 degrees sounds like they are trying to get water to turn to steam. Some alcohol is diluted with water, but even water will evaporate well below 100 degrees.

    Try warming it up to about 50 degrees C (which is pretty warm but not too hot to touch) for an hour or two - to see if your readings improve.

    If you do replace it, find out how the manufacturer recommends protecting it from cleaning fluids (which are used in almost every assembly operation).

    I've seen adhesive labels and tape used to cover ports during cleaning.