Project Introduction - Part 1 | Breadboard Basics - Part 2 | The Build - Part 3 | Giving it a Try - Part 4
Thank you for joining me again for the final part of my Halloween build. It's finally here, to hook up all the electronics and polish the final script!
There is a lot going on in the final script, so I figure it is best to break down the elements of it:
Video Control:
I was intending to make something really cool for the video, and still hope to have it done for the 31st! Unfortunately, I was a little behind with the big reveal. I ended up hacking together two small video clips, one that looped every 45 Seconds of a "twitchy zombie", and the other of the "zombie" rush toward the door. As the looping video is largely in the same position, the "jump" from the loop to the "rush" doesn't seem out of place with the sounds and lights.
To control the video playback from Python:
import os #Import operating system control
from subprocess import Popen #Import Process Open
loopVid = ("/home/pi/Desktop/loop.mp4") #Name the file and path of the looping video
rushVid = ("/home/pi/Desktop/rush.mp4") #Name the file and path of the "rush" video
os.system('killall omxplayer.bin') #Stop and video that is currently playing
omxc = Popen(['omxplayer', '-b --loop',looptVid]) #Set up the looping video
This has set up the video that can play in a loop until the capacitive touch is triggered. When it is, we stop the loop, play the "rush" video, then restart the loop after it has played:
os.system('killall omxplayer.bin') #Stop playing the loop video
omxc = Popen(['omxplayer', '-b', rushVid]) #play the "rush" video
time.sleep(5) #wait the length of the "rush" video
print("Reset") #output to the console that the loop is being reset
os.system('killall omxplayer.bin') #ensure that the rush video is removed
omxc = Popen(['omxplayer', '-b --loop', loopVid]) #restart the loop video
Remember that the video playback only shows on the HDMI output. I was using VNC at this point, and thought it wasn't working!
Relay Control:
Relay control is really easy, that is just using the GPIO control to write an output high and low. With the GPIO control already in the script, there is no need to import any additional controls. However, I did add the pin I was using for control to the variables declared at the begining, then switch it!
relay_output=26 #Define the GPIO number as a variable GPIO.setup(relay_output, GPIO.OUT) #Add this to the script where we define the GPIO modes GPIO.output(relay_output,GPIO.HIGH) #Used to turn the relay off (because of the way i wired mine) GPIO.output(relay_output,GPIO.LOW) #Used to turn the relay on (your "HIGH" and "LOW" may be the other way)
"Smart Light" Control:
This is very specific to the equipment I have, but it is useful for other things too (local network unsecure communications). Once I have set up my home device with the MAC address of the PI (Which i did twice, once for the WIFI and once for the LAN I had used in testing!) I could send some UDP strings that it would respond to.
import socket #Import the socket library for network connections
UDP_IP = "192.168.1.7" #define the local IP of the home device
UDP_PORT = 9760 #The port that the device listens on
sock = socket.socket(socket.AF_INET, socket.SOCK_DGRAM) #Configures the type of network socket I want to open
sock.sendto("11,!R1D1F0", (UDP_IP, UDP_PORT)) #Send the command to turn off the light
sock.sendto("11,!R1D1F1", (UDP_IP, UDP_PORT)) #Send the command to turn on the light
Capacitive Sense:
Tuning the times, resistance and capacitance of the sensor was the last part of the puzzle. I ended up needing to reduce the resistance (added another 10MΩ resistor in parallel to give 5MΩ) to my circuit as the capacitance was so high, the lag was longer than the pulse time.
With that all in place, all I need are some unsuspecting trick or treaters!
Final Thoughts?
I had an enormous amount of fun building this project, and hope that it will be even more fun come Halloween.
I am very pleased with the actual build, how it functions and the modular nature of the project, allowing for additions and modifications for next year. Once again, I feel I have stretched my knowledge and learned from it, which is key for me with anything I undertake.
If I were to start the project again or make large improvements, I think I would replace a lot of the internal wiring and internal perf board with a custom PCB. This is not something I have experience in, but would definitely improve the quality of the build.


Top Comments
-
three-phase
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
three-phase
-
Cancel
-
Vote Up
+1
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children