• Products and Partners
    Products and Partners
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
Build a Present
  • Challenges & Projects
  • Project14
  • Build a Present
  • More
  • Cancel
Build a Present
Blog EL Wire Christmas Tree
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
  • Author Author: scottiebabe
  • Date Created: 18 Dec 2021 3:46 AM Date Created
  • Views 42180 views
  • Likes 15 likes
  • Comments 13 comments
Related
Recommended

EL Wire Christmas Tree

scottiebabe
scottiebabe
18 Dec 2021

Soft 404

  • Sign in to reply

Top Comments

  • scottiebabe
    scottiebabe over 4 years ago in reply to beacon_dave +1
    Deleted
  • beacon_dave
    beacon_dave over 4 years ago in reply to scottiebabe +1
    If it is silicone sleeving then perhaps not the easiest to glue unless you prime the surface first with something like Loctite 770. However if you use enough hot glue then you might get a C-clip type mechanical…
Parents
  • fmilburn
    fmilburn over 4 years ago

    That's pretty neat.  I'll be making a visit to the dollar store tomorrow.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to fmilburn
    This comment was deleted.
    • Cancel
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to scottiebabe

    I've seen some examples of where the silicone strip has been inserted into a laser cut  slot in Perspex/Plexiglass, which works well.

    The LED filament wire can often be found in the 'squirrel cage' style LED lamps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to beacon_dave
    This comment was deleted.
    • Cancel
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to scottiebabe

    A lot of potential for those decorative projects.

    Perhaps though there needs to be a semiflexible version so that you can bend it into a shape and it will then hold that shape, otherwise we are back to the EL wire problem you had. Also perhaps an easier way to cut it to different lengths.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago in reply to beacon_dave
    This comment was deleted.
    • Cancel
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago in reply to scottiebabe

    If it is silicone sleeving then perhaps not the easiest to glue unless you prime the surface first with something like Loctite 770. However if you use enough hot glue then you might get a C-clip type mechanical connection with it once it solidifies. Perhaps difficult to keep neat and tidy though. "exhibit e14: 'sculpture in light (with stringy bits)' "

    I was thinking more of open wireframe type skeleton designs with the LED filament shapes mounted between two points of the frame, but that's not going to work on its own.

    Spraying it with some sort of lacquer that encapsulates it and hardens once it dries might work. Or inserting it into clear tubing which can then be manipulated with a bit of heat.

    Engraving Perspex/Plexiglass and inserting it into the groove could work quite good in some cases but the light may bleed in such a way that you don't want it to, and you are likely to get reflections which you may not want. (Although I would like to find out more about various edge-lighting techniques.)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 4 years ago in reply to scottiebabe

    If it is silicone sleeving then perhaps not the easiest to glue unless you prime the surface first with something like Loctite 770. However if you use enough hot glue then you might get a C-clip type mechanical connection with it once it solidifies. Perhaps difficult to keep neat and tidy though. "exhibit e14: 'sculpture in light (with stringy bits)' "

    I was thinking more of open wireframe type skeleton designs with the LED filament shapes mounted between two points of the frame, but that's not going to work on its own.

    Spraying it with some sort of lacquer that encapsulates it and hardens once it dries might work. Or inserting it into clear tubing which can then be manipulated with a bit of heat.

    Engraving Perspex/Plexiglass and inserting it into the groove could work quite good in some cases but the light may bleed in such a way that you don't want it to, and you are likely to get reflections which you may not want. (Although I would like to find out more about various edge-lighting techniques.)