Cheer Us Up
  • Challenges & Projects
  • Project14
  • Cheer Us Up
  • More
  • Cancel
Cheer Us Up
Blog WRONGCO Wake 'N Shower Travel Alarm Clock
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cheer Us Up to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 9 May 2021 9:52 PM Date Created
  • Views 1876 views
  • Likes 12 likes
  • Comments 4 comments
  • cheerusupch
  • arduino
Related
Recommended

WRONGCO Wake 'N Shower Travel Alarm Clock

robogary
robogary
9 May 2021

Rube Goldberg style alarm clock system,The entire system is powered from a 12V battery and a 100W inverter. There is a solar panel for recharge.

while the alarm clock radio is ON or Wake to Music, radio stations play as normal, with a light organ providing visual entertainment

HOWEVER 

the alarm setting gives a 10 second (or more) cold shower to the sleeper when the alarm goes off.

The light organ is Arduino based and MSGEQ7 control .

The light organ software is updated (from its orginal 2015 program) to detect the alarm audio signature and then turns on a relay to drive the sizable 11 gallons/minute aquarium pump.

image

imageimage

 

 

 

You Gotta watch the hilarious video:

https://youtu.be/A5MiU3C9NaM

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

imageimage

schematics & Arduino Nano software attached

imageimage

image

/*

 

  EqiilizerLEDsWakeNshower

  is started from EquilizerLEDsRev1_Working is  EquilizerLEDsRev0_Working with bands 1 and 7 with lower thresholds

 

  EquilizerLEDsRev0_Working is a relabled version of Test 3 Working, based on Test2Working

  showing the MSWGEQ7 is reading an analog input from a ipod earphone jack, and providing volts from the multiplexor.

  -> added pot to analog input 1 for threshold adjust on LED trigger

  -> add a PB to D6 to run a test routine that strobes the lights

  -> add ULN2803 driver for LEDS, requires to un-invert the HIGH LOW states

 

  control interface to MSGEQ7 IC

  strobe control for equalizer bands, read in multiplexed voltage per band, drive outputs LEDs

 

  Arduino D4 wires to MSGEQ7 pin 4 strobe

  Arduino D5 wires to MSGEQ7 pin 7 reset

 

  all ins have pull ups

 

  Arduino D7 = 63Hz LED , LOW = ON

  Arduino D8 = 160Hz LED

  Arduino D9 = 400Hz LED

  Arduino D10 = 1kHz LED

  Arduino D11 = 2.5 kHz LED

  Arduino D12 = 6kHz LED

  Arduino D13 = 16kHz LED

 

  Arduino A0 wires to MSGEQ7 pin 3 Vout

 

 

The WakeNShower audio input comes from an alarm clock, tapped from its speaker thru an audio transformer.

The code adds a relay output to D3.

The alarm sound is a loud 1kHz square wave that triggers D10 thru D13.

Use those signals to determine if the alarm sounded, and to pick up the relay.

The relay activates a water pump for the shower.

 

*/

int BandMagnitude[8];

int Vin =0 ;

int LEDThreshold = 500;

int strobeBit=1;

int pausetime =1000;

 

 

int AlarmCnt=0;// how many consecutive times AlarmCnt is seen

int value=0; // setup register for checking for alarm sound

 

 

// the setup function runs once when you press reset or power the board

 

 

void setup()

{

  Serial.begin(9600);          //  setup serial

 

  // initialize digital output pins for LEDS.

  pinMode(13, OUTPUT);

  pinMode(12, OUTPUT);

  pinMode(11, OUTPUT);

  pinMode(10, OUTPUT);

  pinMode(9, OUTPUT);

  pinMode(8, OUTPUT);

  pinMode(7, OUTPUT);

  pinMode(3, OUTPUT);

  // initialize digital output pins for strobe and reset MSGEQ7

    pinMode(5, OUTPUT); //reset MSGEQ7 WHEN HIGH, LOW enables STROBE

    pinMode(4, OUTPUT); //strobe MSGEQ7 output, edge triggered LOW is active state for strobe

 

 

// defines and integer array for the 7 band values, array location 0 is unused

 

 

   pinMode(6, INPUT_PULLUP); //tie pin D6 to ground to run the strobe LED routine

 

int BandMagnitude[8];

int Vin =0 ;

}

 

 

// the loop function runs over and over again forever

void loop()

{

  digitalWrite(3, HIGH);   // turn off pump, relay LOW activates

  value = 0; // initialze alarm buzzer detector

  // initialze the strobe and reset after every scan to ensure synchronization

 

    initializeMSGEQ7 ();

    //delay (1);

     delayMicroseconds(100); // minimum delay is 72 usec for strobe reset

     LEDThreshold = analogRead(1) ;

  

    for (int i=1; i <= 7; i++)

     {

       digitalWrite(4, LOW);   // strobe is edge trigger LOW active

       delayMicroseconds(30); // minimum delay is 18 usec for strobe reset

          // delay (1);

           Vin = analogRead(0) ;

          BandMagnitude[i] = Vin ;

           digitalWrite(4, HIGH);   // strobe off,  strobe is edge trigger LOW active

           //          Serial.println("BandMagnitude[i] =");             // debug value  

           //          Serial.println(BandMagnitude[i]);             // debug value

            //         Serial.println("[i] =");             // debug value 

            //         Serial.println(i);             // debug value

 

       if (i==7) LEDThreshold = 150 ; // fire the hi band at a lower threshold

 

       if (BandMagnitude[i]>LEDThreshold)

          { digitalWrite((6+i), HIGH);

            if ((6+i)==10) { value=value+1; }

            if ((6+i)==11) { value=value+2; }

            if ((6+i)==12) { value=value+4; }

          }

       if (BandMagnitude[i]<LEDThreshold)

           { digitalWrite((6+i), LOW);      }

       if ((i==7)&& (value ==7)){ runpump(); }

           delayMicroseconds(30); // minimum delay is 18 usec for strobe reset

   //    delay (90); // delay time with strobe low for the next read cycle

 

}

strobeBit = digitalRead(6);

if (strobeBit == LOW) { strobe();}

//          Serial.println("BandMagnitude[i] =");             // debug value  

          Serial.println("[strobebit] =");             // debug value 

           Serial.println(strobeBit);

 

 

}

 

 

void initializeMSGEQ7 ()

{

   digitalWrite(5, HIGH);   // make RESET line HIGH

   digitalWrite(4, HIGH);   // turn on strobe bit

  delayMicroseconds(30); // minimum delay is 18 usec for strobe width

  digitalWrite(4, LOW);   // turn off strobe bit

   delayMicroseconds(1); // minimum delay is 100 ns

//   delay(1);   

  digitalWrite(4, HIGH);   // turn off strobe bit

//  delay(1);

   digitalWrite(5, LOW);   // make RESET line LOW to enable the strobe line

delayMicroseconds(100); // minimum delay is 72 usec for strobe reset

// digitalWrite(5, LOW);   // make RESET line LOW to enable the strobe line

// delay (1);

//  digitalWrite(4, HIGH);   // turn off strobe bit (low is active)

// delay(1);

}

 

 

void strobe ()

{ pausetime=500;

   for (int j=1; j <= 15; j++)

   {

      pausetime=(pausetime/2);

       if (pausetime<8){pausetime=8;}

         for (int i=1; i <= 7; i++)

            { digitalWrite((6+i), HIGH);

             delay (pausetime);

             digitalWrite((6+i), LOW);

             delay (5);

            }

         for (int i=0; i <= 7; i++)

           { digitalWrite((12-i), HIGH);

             delay (pausetime);

              digitalWrite((12-i),LOW);

             delay (5);

             }  

      }

   }

 

 

void runpump ()

  {

       digitalWrite(3, LOW);   // turn on pump

       delay (5000); // leave on for 10 secs

       digitalWrite(3, HIGH);   // turn off pump

       value=0;

   }

  • Sign in to reply

Top Comments

  • robogary
    robogary over 5 years ago +1
    I peed my pants laughing at this video. Nice job.
  • javagoza
    javagoza over 5 years ago +1
    Very funny!
  • dubbie
    dubbie over 5 years ago +1
    All you need now is to add it to a mobile robot and then it can follow you around while providing a wonderful refreshing morning shower. Dubbie
Parents
  • robogary
    robogary over 5 years ago

    I peed my pants laughing at this video. Nice job. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • robogary
    robogary over 5 years ago

    I peed my pants laughing at this video. Nice job.