DIY Test Instrumentation
  • Challenges & Projects
  • Project14
  • DIY Test Instrumentation
  • More
  • Cancel
DIY Test Instrumentation
Blog Viewing Noise with a Measurement Amplifier
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join DIY Test Instrumentation to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 16 Jul 2021 4:25 AM Date Created
  • Views 13549 views
  • Likes 20 likes
  • Comments 39 comments
  • opa209
  • diytestinstrumentationch
  • opa1611
  • noise measurement
  • lab amplifier
  • test amplifier
  • opa211
Related
Recommended

Viewing Noise with a Measurement Amplifier

shabaz
shabaz
16 Jul 2021

Table of Contents

  • Introduction
  • Block Diagram
  • Circuit Diagram
    • Power Entry
    • Input Stage
    • First Gain Stage
    • Filter Stage
    • Attenuator
    • Second Gain Stage
    • Offset Null
    • Low Power Indicator
  • Proto Area
  • Circuit Board and Construction
  • Enclosure
  • Frequency Response
  • Output Noise Performance
  • Trying it out: 5V Regulator Noise Measurement
  • Summary

 

Introduction

A measurement amplifier is a piece of test equipment that can be used for, as the name suggests, measurement of signals. Usually it is combined with a multimeter or an oscilloscope to actually display the measurement or signal. A good use-case for such an amplifier is to measure noise on power supply rails.

 

A while back I hacked together an amplifier using a circuit board that was originally intended for a microphone amplifier. Although it functioned, that revision 1 design had limitations.

 

Since then, after some suggestions from  jw0752  and others, I wanted to improve the design, improve the frequency response, add DC amplifier capability, selectable filtering, and also make the design easier to assemble, with reduced wiring.

 

I sketched up a revision 2 design but I never got around to building that. This blog post presents a revision 3 design. It is different enough that it deserves its own blog post to prevent confusion, but the first blog post Building a Measurement Amplifier  can be consulted to see more detail about measurement amplifiers, and the discussions that resulted in the current design. Also, see  jc2048  very nice discrete design Noise: Transistor Preamp 3  for more information about noise measurement amplifiers.

 

See the five-minute video for a quick explanation of the circuit, and a demonstration of it being used to measure the noise from a LD1117S50CTR LD1117S50CTR Low Drop-Out (LDO) voltage regulator.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This revision 3 design has a reasonable (I think) mix of features. It isn't entirely tested however, and there is tons that could be improved.

 

So far the main features are:

 

  • AC or DC input, and AC or DC output
  • DC input to 500 kHz frequency response flat to within about +- 0.15 dB
  • AC input between 2 Hz to 500 kHz, has similar specification
  • 100 Hz, 1 kHz and 10 kHz selectable low-pass filters
  • Null adjust capability (for DC output mode)
  • Selectable gain (x100 or x200)
  • Max input before clipping/distortion: 100 mVp-p (200 gain) or 50 mV p-p (100 gain) (higher may be possible but it wasn't tested)
  • Zeroing button to settle quicker in AC output mode
  • Low-Voltage indicator
  • 2 x 9V PP3 supply
  • Optional proto-board area for expanding the design

 

image

 

Block Diagram

The diagram below shows what was implemented. It is mostly self-explanatory (more detail in the next section).

image

 

Circuit Diagram

Here is the entire circuit (click to enlarge), but it is explained step-by-step.

image

 

Power Entry

The circuit is powered from two 9V batteries, used to provide a positive and negative rail.

image

 

Input Stage

The input circuitry provides selectable AC or DC input, 22 kohm input impedance, and overload protection. I wanted to be able to use the measurement amplifier for monitoring AC noise on power supply rails, so overload protection was needed.

image

 

Capacitors C5 and C17 are paralleled for 24 uF of capacitance that can be shorted out for DC input mode. For monitoring noise on DC power rails, the AC mode should be selected.

 

First Gain Stage

The first gain stage consists of a non-inverting amplifier with a gain of 20 (actually it's just slightly less than 20, to compensate for other losses and gains in the overall circuit). The design doesn't have any trimming resistors, so in places resistors need to be paralleled to provide the more unusual resistance values. Resistor R2 requires piggybacking of three resistors on top of each other, because I didn't put three footprints on the board unfortunately. Anyway, it's not hard to do with large 0805 sized surface-mount resistors. In theory R2 could have be replaced with a trimmer resistor but then things need calibration.

image

 

Although the two gain stages were supposed to use two OPA1611 op-amps for U1 and U2, I only had one, and global component shortages meant that I had to use an OPA211 IC instead for U1. They appear to be near-identical anyway.

 

Filter Stage

Rotary switches can be expensive/awkward to use, so push-button switches were used throughout the design instead. This limited what I could do in terms of filtering capability, however it was possible to use two switches to provide three filtering settings. Resistor R18 and capacitor C16 create an RC filter. When either switch is pushed in, additional capacitors are paralleled with C16. The particular capacitor values result in selectable 1 kHz and 10 kHz filtering, or 100 Hz when both switches are pressed.

image

 

Attenuator

Resistor R24 is switched in/out of the circuit to optionally attenuate the signal by half, before the signal reaches the second gain stage. R24 consists of two piggybacked resistors.

image

 

Second Gain Stage

The second stage is fairly identical to the first, except for a different gain value of just over 10. To achieve the correct gain, resistor R15 is actually two piggybacked resistors.

 

The output from the second gain stage can be directly connected to a multimeter, or connected to an oscilloscope. R5 and R25 offer some protection against output short-circuits. A push-switch is used to short the AC output to ground, in order to more rapidly discharge the output capacitor, otherwise there could be a long wait before the circuit settles.

 

There's actually not much need for the AC output, since the DC output can be null-adjusted as discussed next.

image

 

Offset Null

In order to operate in DC amplifier mode, it was desirable to be able to remove any offset when the input is at 0V. This is achieved with a potentiometer and unity gain buffer circuit. This circuit applies a small offset voltage to the second gain stage. In AC amplifier mode use, it is not critical to adjust the potentiometer, since the offset will get removed by the output capacitor.

image

I didn't have a 50-ohm variable resistor, so I used a 1 kohm one, and soldered a 22 ohm resistor (22 ohm or 47 ohm or thereabouts will do fine) across the two ends of it, on the underside of the board.

 

Low Power Indicator

The battery voltage is monitored using a TL431 IC. The IC acts as a shunt when the voltage across resistor R8 exceeds a threshold voltage (2.5V) that is hard-coded inside the IC. When the voltage reduces, the IC stops acting as a shunt and it causes enough current to flow into Q1 to switch on the LO-BAT LED.

image

 

Proto Area

It could be interesting to one day extend functionality, or apply this project for a different use-case. For that reason, there is space for soldering an optional SOIC footprint IC, and through-hole components, to patch in features or fix errors.

image

 

Circuit Board and Construction

The files are attached to the blog post, ready for sending to any PCB factory. Although this rev 3 board requires piggybacked resistors, I don't think it requires a re-spin because it is easy to do the piggybacking and doesn't merit creating a modified board layout.

 

The render here shows the top side of the board (there are no components on the underside).

image

 

It gets annoying having to use wires to attach switches and connectors, so I tried to put everything on the board. Apart from the AC output connector, and the battery connectors, everything is soldered to the PCB.

image

 

Enclosure

The board width is 160 mm, intended to slide into the same enclosure as the revision 1 measurement amplifier, Hammond 1455T16011455T1601 which is annoyingly expensive. I'd like to find a cheaper enclosure (it needs to be metal to provide shielding).

 

The diagram below shows the locations of the board holes and the connectors, LEDs and switch positions. The actual hole diameters for the switches depends on the switch cap diameter. Caps could be 3D printed, or low-cost ready-made caps from Aliexpress could be used, although they may require gluing on.

 

 

image

A PCB front-panel design could be used for eliminating the need to drill accurate holes. The PCB Gerber files for an example front panel are attached to this blog post, but I have not tried it, so there are no guarantees yet that it is alright. The underside of the front panel has a copper layer, with space to solder a wire from there to the PCB (since the surfaces of anodized enclosures are not conductive).

image

 

 

Frequency Response

Plenty of testing still needs to be done, however I wanted to check what the frequency response looked like. I applied a sine-wave signal using a function generator, and observed the input and output signals on an oscilloscope (8-bit, but set to high-res mode), for 'good-enough' measurements.

 

At first glance the response doesn't look very flat but actually the y-axis just covers a few percent. For a first attempt I think it's not bad, but it could be improved. Capacitors  C1 and C15 may need adjusting; the output from the first op-amp stage would need to be observed on an oscilloscope, and then C1 would be selected. Then, once the response was flat, the output from the second stage would be monitored and C15 would be selected. Trimmer capacitors could be bodged into place if desired. The response is already flat to within a few percent, so I figured this part of the testing could be for future optimization.

image

 

Output Noise Performance

I don't currently have an enclosure for the project, so I placed it in a biscuit/cookie tin to provide shielding. A 50 ohm terminator was attached to the input, and the output was connected to an oscilloscope.

 

For all of the 'scope screenshots in this section, the timebase was set to 100 msec/div; there are ten horizontal divisions so 1 second of the output signal can be observed. The gain of the amplifier was set to 200.

 

The screenshot below shows the 'scope trace with the measurement amplifier set to its maximum bandwidth. The 'scope reported 11.4mVp-p, which with a gain of 200 is the equivalent of about 60uVp-p (or 6.5 uV RMS) of noise at the input, which is a lot.

image

 

The chart below helps interpret it, by trying to look at the contribution of different frequency content in the noise. The chart shows what would have been the output noise amplitude, if the output was filtered. Were the output to be filtered at 500 kHz, then the peak-to-peak noise would have been half, i.e. about 30uVp-p equivalent at the input. So, one improvement that would be very worthwhile, would be to include such a filter in the circuit.

image

 

The chart below is the same as above, but just zoomed into the 0-500kHz area of interest. Now it can be seen more clearly that there will be much reduced noise on the output if a filter is enabled for 10kHz or 1kHz.

image

 

And that's exactly what the 'scope trace shows, when the 10 kHz filter button is pressed. Now the output noise is under 2mVp-p, or just under 10uV equivalent noise at the input. That's a lot more usable!

image

 

In a similar vein, setting the amplifier filter to 1 kHz also results in reduced noise, 1.5mVp-p at the output, which is about 7.5uVp-p equivalent at the input:

image

 

These noise levels are not state-of-the-art, but I think acceptable for (say) typical power supply rail noise measurements.

 

Trying it out: 5V Regulator Noise Measurement

An LD1117S50CTR voltage regulatorLD1117S50CTR voltage regulator (it is similar to the popular LM1117 voltage regulator) was wired as advised in the datasheet. The 'typical' RMS noise is supposed to be around 150uV RMS according to the datasheet.

image

 

The output from the LDO was connected to the input of the measurement amplifier (set to AC mode), and the output of the measurement amplifier was connected to an oscilloscope.

 

The measurement amplifier was set to a gain of 100, and the 10 kHz filter setting was enabled (to compare more closely with the datasheet since that provided the noise specification with 10Hz to 10 kHz bandwidth).

 

As can be seen in the screenshot below, the automated oscilloscope measurement indicates that the RMS noise is 10.9mV, which divided by 100 is 109uV RMS. This seems reasonably close to the typical value in the datasheet.

image

 

A 'True RMS' multimeter could be used for this measurement if an oscilloscope was not handy. The U1282A multimeterU1282A multimeter has 20Hz (in practice usable down to 10 Hz) to 100kHz bandwidth for RMS measurements, but for a lower bandwidth, there are more options. The Tenma 72-2995 multimeterTenma 72-2995 multimeter should be usable from at least 45 Hz to 20 kHz; it is a very good range for price. Anyway, a true RMS multimeter is not needed here if a 'scope is available.

 

Summary

Although additional testing needs to be done, I think this revision 3 design looks acceptable enough to now start drilling a front panel, so I can give this project a proper enclosure.

EDIT: In the end, I used the Hammond enclosure and a very low-cost aluminium PCB front-panel, to save drilling and printing labels. It still needs plastic button caps from Aliexpress (search term for those is Button cap round inner diameter 2.8mm square ). See the comments below for more information on the front panel, etc., and the front panel files are also attached, in two versions (for different filter setting labels).

image

 

The final amplifier in use Magnetic Sensors, Swatch Watch and a Measurement Amplifier  :

image

 

 

The BoM and PCB and front panel files are attached below in case anyone wishes to replicate or improve it!

Thanks for reading!

Attachments:
export-meas-amp-rev3.zip
bill-of-materials-rev3-board.xlsx bill-of-materials-rev3-board.xlsx
export-front-panel.zip
export-alu-100k.zip
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 5 years ago +6
    Quick photo showing the front panel assembled! The enclosure could do with a rubber surround : ) I finally found some suitable button caps on Aliexpress and have ordered them, currently I'm having to push…
  • shabaz
    shabaz over 5 years ago +5
    These arrived earlier (within 7 days of ordering!), so I propped it up against the enclosure to quickly test for fit. Also in the foreground in the photo below, is the underside of the alu front panel…
  • fmilburn
    fmilburn over 5 years ago +4
    Hi Shabaz, That is a useful instrument and the project is very well done. Thanks for the great writeup and documentation as I am going to look into building one but need to finish off my current backlog…
Parents
  • jc2048
    jc2048 over 5 years ago

    I enjoyed reading this. Thanks for blogging it.

     

    Your op amp is much more precise than the three-transistor cicrcuit I was playing with. The OPA1611 looks like a very nice device.

     

    If it's of any interest, this is my transistor circuit response in more detail. My test equipment and measurements by hand aren't really quite up to this, but it gives an idea for comparison.

     

    image

     

    Perhaps I had better have a break from the 'Summer of FPGAs' and build the other two transistor circuits I wanted to try and see how they all compare.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 5 years ago in reply to jc2048

    Hi Jon,

     

    That's a really good flat response. To be honest even with the OPA1611 circuit with the large capacitances, it's of questionable use having the response to much lower frequencies than 10 Hz or so, since then the 1/f noise becomes an issue. Currently I have 24 uF at the input, but I might remove one of the capacitors since 12 uF is good enough, for the flat response down to approx 10 Hz pretty much like you have.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to shabaz

    I think I got a little lucky with my free-form construction. I expected it to peak a little at the top end, but it didn't.

     

    Notice that the gain is much less precise than yours. In the simulator, that was almost spot-on 40dB (gain of 100), but built it's half a dB out.

     

    I wasn't very sure what to do about the input coupling. The original circuit didn't show a coupling capacitor, but I wanted it to be able to measure noise on a rail as well as close to ground potential. I didn't think of your solution of having a switch so that it was selectable (anyone would think that I've never used a traditional oscilloscope, as it used to stare me in the face most days).

     

    Whether you want the 1/f noise depends, I think, on what you're measuring and what you're using it for. Here you measure a regulator and give us a figure for the total noise at the output, so, to my mind, that should be all the noise. It's a somewhat artificial figure for design purposes because, as soon as you connect it to a whole load of decoupling on a board, you would hope that the noise figure would go down, but it's a useful way to compare different regulators, and give a feel for a worst case figure.

     

    If you were measuring an op amp and trying for a device-comparison figure for the input-referred white noise, then you'd probably want the low end to roll off higher up (and you'd need to know the overall noise bandwidth accurately). From what I can make out, professional noise meters use a filter with quite a narrow bandpass to do this, often centred on 1kHz.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago in reply to shabaz

    I think I got a little lucky with my free-form construction. I expected it to peak a little at the top end, but it didn't.

     

    Notice that the gain is much less precise than yours. In the simulator, that was almost spot-on 40dB (gain of 100), but built it's half a dB out.

     

    I wasn't very sure what to do about the input coupling. The original circuit didn't show a coupling capacitor, but I wanted it to be able to measure noise on a rail as well as close to ground potential. I didn't think of your solution of having a switch so that it was selectable (anyone would think that I've never used a traditional oscilloscope, as it used to stare me in the face most days).

     

    Whether you want the 1/f noise depends, I think, on what you're measuring and what you're using it for. Here you measure a regulator and give us a figure for the total noise at the output, so, to my mind, that should be all the noise. It's a somewhat artificial figure for design purposes because, as soon as you connect it to a whole load of decoupling on a board, you would hope that the noise figure would go down, but it's a useful way to compare different regulators, and give a feel for a worst case figure.

     

    If you were measuring an op amp and trying for a device-comparison figure for the input-referred white noise, then you'd probably want the low end to roll off higher up (and you'd need to know the overall noise bandwidth accurately). From what I can make out, professional noise meters use a filter with quite a narrow bandpass to do this, often centred on 1kHz.

    • Cancel
    • Vote Up +3 Vote Down