• Products and Partners
    Products and Partners
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
Electromagnetism
  • Challenges & Projects
  • Project14
  • Electromagnetism
  • More
  • Cancel
Electromagnetism
Blog The KLINGMAGON Subspace Probe
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Electromagnetism to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 8 Apr 2019 2:13 AM Date Created
  • Views 2509 views
  • Likes 17 likes
  • Comments 8 comments
  • arduino thermometer
  • klingmagon
  • air core transformer
  • doug wong
  • wireless power transfer
  • pcb printed coil
  • power scavenging
  • electromagnetismch
Related
Recommended

The KLINGMAGON Subspace Probe

dougw
dougw
8 Apr 2019

No wires, no batteries, no solar panels, no screws, no glue and no suction cups, but a Klingmagon Subspace Probe can scavenge power to operate and cling to a vertical window without supports.

I have been planning to build an outdoor digital thermometer for a long time that uses a temperature sensor and digital display without requiring periodic battery replacement. I originally planned to use solar power and super capacitors, but hadn't gotten around to figuring out what would actually be required to make it work. Problems like keeping the solar panels clean were looking like they were as much work as replacing batteries.

My work with Qi chargers suggested maybe I could use wireless power transfer to eliminate wires going through the walls. I had most of the needed parts already collected and I had it all worked out in my head, so I figured I could whip a system together in a few hours..... wow, was I ever wrong...

I was out to lunch in assuming a Qi charger would work through double glazed windows. I had to make a completely custom power transfer system.

I was out to lunch assuming I could plug in a Nokia 5110 display (that I've used many times) and have it work. It took 2 days to figure out there was some hardware issue in the display that was producing random garbage. Fortunately I had an extra display.

I was out to lunch assuming I could drop in an arduino Pro Micro and have it work. It took another day to figure out some of the pins were blown.

I took so long trying to force this idea to work, I am now desperately behind on all my other projects, so I just have to dash off a video and then get on with other things.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

In the end the system used 2 interesting ideas (wireless power transfer and magnetic mounting) to make a clean outdoor instrumentation device that could be simply installed and would never need battery maintenance. Both ideas worked very well, and I am happy with the result, just not quite so happy with how long it took me.

The project has a custom interface card to connect an arduino to a temperature sensor and an LCD. This card also has a footprint for a Bluetooth radio which can also go through windows, so there is room for expansion.

The system also has two custom PCBs to create a wireless power transfer system.

Here is the simple 5V power oscillator circuit that drives a printed coil that has 9 turns on it in a square spiral:

There are links to some PCB spiral coil inductance calculators in the links section.

The MAX256 is a neat little 3W chip that includes an oscillator and a power H-bridge driver designed to drive the primary side of transformers.

image

Here is the Power scavenging circuit, also with a 9 turn printed coil in a square spiral.

It has a charge pump to convert the AC input signal to DC and boost it to a higher voltage:

image

I will try to find some time to comment the arduino code and insert it here.

Hopefully these techniques will help pave the way for others to exploit them in their own projects.

 

Relevant Links:

Electromagnetism

Project14 | The Force of Electromagnetism: Anything from Solenoids, Motors, to Wireless Transfer!

temperature sensortemperature sensor

PCB coil inductance calculator

PCB Spiral Coil Calculator

MAX256 Datasheet

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +6
    Hi Doug, That is pretty impressive. Nice demo of what it is capable of. Frank
  • jw0752
    jw0752 over 7 years ago +6
    Hi Doug, Sorry about all the extra time the project cost you but from my point of view it was worth it. It was awesome and if I saw a temperature display like this on the retail market I would buy it.…
  • dougw
    dougw over 7 years ago in reply to three-phase +6
    No, but it will probably be necessary to figure out the power when I expand the system with Bluetooth. I know the oscillator draws about 3 Watts (I didn't build in a way to adjust the power) and I smoked…
Parents
  • jw0752
    jw0752 over 7 years ago

    Hi Doug,

     

    Sorry about all the extra time the project cost you but from my point of view it was worth it. It was awesome and if I saw a temperature display like this on the retail market I would buy it. As Frank already indicated your presentation was really well done.

     

    John

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 7 years ago

    Hi Doug,

     

    Sorry about all the extra time the project cost you but from my point of view it was worth it. It was awesome and if I saw a temperature display like this on the retail market I would buy it. As Frank already indicated your presentation was really well done.

     

    John

    • Cancel
    • Vote Up +6 Vote Down