Energy Harvesting
  • Challenges & Projects
  • Project14
  • Energy Harvesting
  • More
  • Cancel
Energy Harvesting
Blog Solar powered IoT device with Cayenne
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Energy Harvesting to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: luislabmo
  • Date Created: 14 Oct 2019 8:11 PM Date Created
  • Views 5516 views
  • Likes 13 likes
  • Comments 19 comments
  • internet of things
  • super capacitor
  • energyharvestingch
  • ltc3106
  • linear technology
  • energy harvester
  • iot
  • luislab
  • rechargeable battery
Related
Recommended

Solar powered IoT device with Cayenne

luislabmo
luislabmo
14 Oct 2019

IoT connected devices have to rely mostly on battery power for operation which may increase their cost and limit how effective they are on their intended use. There are also situations where reliable power is not easily accessible or simply put, could be an undesirable source of power, making battery life one of the biggest challenges to IoT solutions today.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

    • Energy Harvesting as a Solution
    • Key elements of the Project
      • A solar panel
      • Energy Harvester
        • LTC3106's Features
      • Backup battery
      • IoT sensor
      • Mosfet
      • Cayenne Software
    • Assembly
      • The energy harvester (custom PCB)
        • BOM
        • Schematics
      • Wi-Fi Module
      • Solar Panel
      • Main Schematic
      • Source Code
      • 3D Printed Mount
        • 3D print settings
    • LTC3106 custom PCB settings
      • JP1 – Programmable output voltage (VOUT)
      • JP2 – Maximum Power Point Control (MPPC)
      • JP3 – Battery backup Over/Under voltage threshold
      • JP4 – Current limit input select (ILIMSEL)
      • JP5 – Input Turn ON/OFF Thresholds (RUN)
      • JP6 – Isolation mode (VSTORE/VCAP)
      • A more friendly approach (Breakout)
    • How this project can be improved

 

Energy Harvesting as a Solution

In most cases, IoT sensors will outlast the life of a battery, leaving the designers with mostly 3 factors to consider:

  • Reducing the amount of data that will be gathered by the sensor
  • Finding a strategy to replace batteries
  • Introducing an alternate source of power to increase the amount of time the sensor spends collecting/transmitting data

One technology that can help counter the issues above is Energy Harvesting, which is the process of capturing/scavenge energy from external sources (e.g., solar power, wind, vibration, thermal, kinetic) to later power small devices like wearables and wireless sensors.

 

With the help of Internet of Things (IoT) and energy harvesting devices, wireless communications can represent the ideal communication scenario to easily and reliably connect devices in a system by bringing network capability, data collection, and management with little human intervention.

image

The Solar powered IoT device illustrates a concept: harvesting energy from a solar panel by storing it in a rechargeable battery or super-capacitor and then using it to power a sensor connected to an IoT cloud provider.

 

Key elements of the Project

A solar panel

For this project, the energy harvester takes power from a 5V, 2.5W Solar panel.

image

Energy Harvester

Will gather and store the energy provided by the solar panel. Driven by the LTC3106 from Linear TechnologyLTC3106 from Linear Technology, which is implemented in a custom made PCB, allowing some features of the chip to be programmed such as the output voltage (JP1), MPPC - Maximum Power Point Control (JP2 and VR2), Over/Under voltage threshold for the rechargeable backup battery (JP3), Low/High Current limit Input (JP4) and Input Turn On/Off thresholds (JP5 and VR1).

image

 

LTC3106's Features

These are the key features that made the LTC3106 a good choice for this project:

  • Dual input: a primary and a backup source of power can be implemented
  • Compatible with rechargeable batteries
  • Low start-up voltage
  • Regulated output

image

 

Backup battery

Excess input energy will be stored in one or more 1F, 5.5V radial super-capacitors1F, 5.5V radial super-capacitors for this particular scenario.

image

 

IoT sensor

The SparkFun ESP8266 Thing - Dev Board provides IoT connectivity to a Vegetronix VH400 Soil moisture Sensor.

image

Mosfet

A NTR4003N N-Channel mosfetNTR4003N N-Channel mosfet (Q1) will be driving the power from the energy harvester to the IoT device once the output threshold has been reached.

{gallery:width=648,height=432,autoplay=false} NTR4003 N-Channel mosfet

image

NTR4003N: N-Channel Mosfet

image

NTR4003N: Testing the Load with LEDs

image

NTR4003N: N-Channel, 560 mA, 30 V, 1.5 ohm Mosfet

 

Cayenne Software

The Cayenne software is used to monitor the data collected by the sensor (Ch4), the ESP8266's sleep setup (Ch0) and up-time (Ch1) -when sleep mode is not enabled-.

image

 

Assembly

 

The energy harvester (custom PCB)

Most of the components of the custom PCB are SMD (I used the LTC3106 in QNF-20 package which was available at the time I started working on this project).

{gallery:width=648,height=432,autoplay=false} Energy Harvester custom PCB

image

Energy Harvester PCB: LTC3106 Energy Harvester PCB ready for hot-air rework

image

PCB: Energy Harvester

image

PCB: Energy Harvester

BOM

  • C1, C4, C5, C6: 330μF, 6.3V radial electrolytic capacitor (6.3mm diameter, through-hole)
  • C2: 2.2µF, 10V ceramic Capacitor, 0603[1608]
  • C3: 0.1μF, 6.3V ceramic capacitor 0603[1608]
  • C7, C9: 1μF, 16V ceramic capacitor 0603[1608]
  • C8: 100μF, 10V radial electrolytic capacitor (6.3mm diameter, through-hole)
  • R1: 1Mohm, 1/10W, 1% resistor 0603[1608]
  • R2: 820kohm resistor 0603[1608]
  • R3: 33ohm resistor 0603[1608]
  • VR1, VR2: 2Mohm trimmer potentiometer, through-hole
  • D1: Schottky Diode ZLLS400ZLLS400 SOD-323
  • D2: Zener Diode 5.1V SOD-323
  • JP1, JP3: 2x3 through-hole header (2.54mm pitch)
  • J3, JP2, JP4, JP5: 1x3 through-hole header (2.54mm pitch)
  • J1, J2, JP6: 1x2 through-hole header (2.54mm pitch)
  • L1: 10µH, minimum saturation current 750mA
  • U1: Linear Technology LTC3106 (QFN-20)
  • 2.54mm pitch, 2 position jumperstic.

 

Schematics

image

Wi-Fi Module

A 2-pin male header is required for the JUMPER_EN on the SparkFun ESP8266 Thing - Dev Board, this way it can wake up by itself from deep sleep mode -it will "sleep" for an interval of time defined in the source code-, headers may be soldered to connect the sensor(s).

image

Solar Panel

The Solar panel requires wires to be soldered. I recommend to isolate their connections from the elements with some epoxy.

image

Main Schematic

Once the soldering job has been completed and all the components are ready, all the modules are assembled together with jumper wires following the main schematics.

image

Source Code

Source code for the ESP8266. Will push the sensor's data to the Cayenne Dashboard and will manage the deep sleep cycle (when active).

 

// Code for the IoT Energy Harvester
//
// Luis Ortiz - luislab.com
// October 4, 2017
// This sketch will publish analog sensor readings, uptime and DeepSleep status (Enabled/Disabled) to the Cayenne dashboard
//
// When deep sleep is enabled, set a jumper on the SLEEP-EN of the Sparkfun ESP8266 - Dev Board
// To upload the sketch. Jumper must be removed from the SLEEP-EN.

//#define CAYENNE_DEBUG
#define CAYENNE_PRINT Serial       // Comment this out to disable prints and save space
#define SLEEP_ENABLE_PIN 4         // Pin to manually Enable/Disable Deep Sleep.
#include <CayenneMQTTESP8266.h>

RF_MODE(RF_NO_CAL)

// WiFi network info.
char ssid[] = "ssid";
char wifiPassword[] = "wifiPassword";

// Cayenne authentication info. This should be obtained from the Cayenne Dashboard.
char username[] = "Cayenne-username";
char password[] = "Cayenne-password";
char clientID[] = "Cayenne-clientID";

unsigned long lastMillis = 0;

// To enable deep sleep: SLEEP_ENABLE_PIN is high or left disconnected -INPUT_PULLUP-. Jumper is required on SLEEP-EN
// To disable deep sleep: connect SLEEP_ENABLE_PIN to GND. Jumper is not required on SLEEP-EN.
const int sleepTimeS = 60;    //Publish interval or sleep time in seconds. See comments above

byte sleepEnabled;

void setup() {
  Serial.begin(9600);

  pinMode(SLEEP_ENABLE_PIN, INPUT_PULLUP);
  pinMode(BUILTIN_LED, OUTPUT);
  digitalWrite(BUILTIN_LED, HIGH);            //Led Off

  //Add static IP to reduce the WiFi startup time -reduces WiFi startup time, lowering power consumption-
  Cayenne.begin(username, password, clientID, ssid, wifiPassword);
}

void loop() {
  Cayenne.loop();

  sleepEnabled = digitalRead(SLEEP_ENABLE_PIN);
  if (sleepEnabled == LOW) {
    if (millis() - lastMillis > 10000) {
      lastMillis = millis();

      //Write data to Cayenne here.
      cayenneSendData();
    }
  } else {
    cayenneSendData();
    Serial.print("[LuisLab] deepSleep: "); Serial.print(sleepTimeS); Serial.println(" seconds.");
    Serial.println();
    delay(100);
    ESP.deepSleep(sleepTimeS * 1000000, WAKE_RF_DEFAULT);
  }
}

unsigned int Ch4Value;

void cayenneSendData () {
  Ch4Value = analogRead(A0);

  Cayenne.virtualWrite(0, sleepEnabled, "digital_sensor", "d");         //Sends sleepEnable status to button on Dashboard
  Cayenne.virtualWrite(1, round(lastMillis / 1000), "counter", "null"); //Sends the current uptime in milliseconds.
  Cayenne.virtualWrite(4, Ch4Value);
  if (sleepEnabled == LOW) {
    digitalWrite(BUILTIN_LED, LOW);     //Led will be On when Deep Sleep disabled
    Serial.println("[LuisLab] Ch0: Deep Sleep disabled");
  }
  Serial.print("[LuisLab] Ch4: "); Serial.println(Ch4Value);
  Serial.println();
}

//Default function for processing actuator commands from the Cayenne Dashboard.
//You can also use functions for specific channels, e.g CAYENNE_IN(1) for channel 1 commands.
CAYENNE_IN_DEFAULT() {
  CAYENNE_LOG("CAYENNE_IN_DEFAULT(%u) - %s, %s", request.channel, getValue.getId(), getValue.asString());
  //Process message here. If there is an error set an error message using getValue.setError(), e.g getValue.setError("Error message");
}

 

3D Printed Mount

Mount is straight simple with slots for the custom PCB and for the Sparkfun ESP8266 Thing with space for the sensor wire routing. STL attached to this entry.

{gallery:width=648,height=432,autoplay=false} 3D printed mount

image

Enclosure: IoT Energy Harvester 3D-printed enclosure

image

STL: IoT Energy Harvester 3D enclosure design

3D print settings

  • Printer: Lulzbot Mini
  • Material: PLA Translucent
  • Infill: 15%, grid
  • Adhesion: Skirt
  • Supports: No
  • Layer height: 0.2mm

 

LTC3106 custom PCB settings

As mentioned before, I designed a custom PCB for the LTC3106 (QFN-20) allowing its key features to be programmed by adjusting some Jumpers, the Potentiometers (VR1 and VR2) and the value of R2.

image

For this project, the following settings were used:

  • Output voltage to 3.3V (JP1).
  • MPPC disabled (JP2) -this will ignore VR2 and R2-.
  • Battery Over Voltage to 4V and Under Voltage (UV) to 2.78V (JP3)
  • On/Off threshold on VIN (JP5)
  • On/Off threshold set to 2.95V (VR1)
  • To properly test the energy harvester: the load and the SOLAR input are connected and once the Super-capacitors are fully charged -their voltage matches the Over Voltage threshold programmed (JP2)- the SOLAR input can be disconnected; the load connected to the VOUT should keep working for a brief period.

JP1 – Programmable output voltage (VOUT)

image

JP2 – Maximum Power Point Control (MPPC)

image

When the MPPC is enabled, it sets the optimal input voltage operating point by adjusting VR2 (VR2 is configured as a variable resistor with R2 in series):

image

To set a precise resistance value for MPP, the jumper JP2 must be removed, then adjust the VR2 value by measuring its resistance between the CCW/Input Pin (top-right corner in the PCB) and the Wiper/Output Pin (middle), then add the R2 value.

 

JP3 – Battery backup Over/Under voltage threshold

image

The custom PCB for this project was designed to connect rechargeable batteries only to VSTORE (J1). To use a super-capacitor as a backup battery, the most suitable Over Voltage (OV), Under Voltage (UV) setting should be used.

 

JP4 – Current limit input select (ILIMSEL)

image

JP5 – Input Turn ON/OFF Thresholds (RUN)

JP5 programs a predictable regulator turn-on at a specified input voltage by adjusting VR1 (acting as a voltage divider).

image

To set a precise resistance value for VR1, jumpers JP4 and JP5 must be removed then the divider value is adjusted by measuring its resistance (CW/Ground pin of the divider is the closest to JP3 in the PCB):

image

  • VIN (J2): sets the turn ON/OFF threshold from the solar input VIN (J2)
  • VSTORE (J1) : sets the turn ON/OFF threshold from the input VSTORE (J1)

 

JP6 – Isolation mode (VSTORE/VCAP)

The PCB was designed to work in NONISOLATED mode only; a jumper must be present on JP6 at all times.

image

A more friendly approach (Breakout)

If you are feeling that you are not ready for an QFN-20 SMD challenge and/or want to approach this project with a Breadboard instead, I'm also providing a breakout for the LTC3106 in its TSSOP-20 version.

{gallery:width=648,height=432,autoplay=false} LTC3106 Breakout

image

LTC3106 Breakout: LTC3106 Breakout TSSOP-20

image

LTC3106 Breakout: LTC3106 Breakout TSSOP-20

 

How this project can be improved

This project is far from perfect for every single situation out there but illustrates a powerful concept that can be expanded on other projects. For demonstration purposes, I've decided to store the excess energy into super-capacitors but rechargeable batteries is ideal: JP3 should be enabled accordingly.

 

Bypassing the voltage regulator and the FTDI chip of the ESP8266 Thing - Dev Board may improve power consumption since the LTC3106 already has a 3.3V regulated output (JP1).

 

Using static IP is the best practice since this takes only a fraction of a second; when using DHCP the WiFi connection takes a longer startup time and thus consumes more power.

 

Thanks for reading along.

 

Luis

Attachments:
imageIoT solar harvester main schematic.pdf
IoT Energy Harvester Enclosure.zip
  • Sign in to reply

Top Comments

  • three-phase
    three-phase over 7 years ago +4
    Interesting project and a great write up. That LTC3106 is certainly an interesting little device. Kind regards.
  • genebren
    genebren over 7 years ago +4
    Luis, Very nice project and blog! I will have to look into the LTC3106 chip for some solar power projects that I plan for our garden. Well done, keep up the good work! Gene
  • luislabmo
    luislabmo over 7 years ago in reply to genebren +4
    Thank you Gene!. The LTC3106 certainly seemed like a good option back in 2017 when I worked on this project. Probably there are better/newer options now that a few years have passed. Luis
Parents
  • sriram98143
    sriram98143 over 6 years ago

    Thanks for your time to  respond for my previous comment.

    can you share the library file for this pcb design with bom library.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • luislabmo
    luislabmo over 6 years ago in reply to sriram98143

    Hi,

     

    I can't share the libraries as these are custom-made parts and I keep renaming, changing them all the time so they won't get recognized.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • luislabmo
    luislabmo over 6 years ago in reply to sriram98143

    Hi,

     

    I can't share the libraries as these are custom-made parts and I keep renaming, changing them all the time so they won't get recognized.

     

    Luis