Fun & Games
  • Challenges & Projects
  • Project14
  • Fun & Games
  • More
  • Cancel
Fun & Games
Forum P-Channel MOSFET High-Side Switch Not Fully Turning Off (ESP32 rail at 2.9V)
  • News
  • Projects
  • Forum
  • Leaderboard
  • More
  • Cancel
  • New
Join Fun & Games to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 50 subscribers
  • Views 1210 views
  • Users 0 members are here
Related

P-Channel MOSFET High-Side Switch Not Fully Turning Off (ESP32 rail at 2.9V)

arvindsa
arvindsa 8 months ago

I’m using a DMP2045U P-channel MOSFET as a high-side switch to control 3.3V power to an ESP32-S3-WROOM module. The gate is driven by an STM32.

image

Connections

  • Source → 3.3V (measured 3.289V)

  • Drain → ESP32 3V3 pin

  • Gate → STM32 GPIO

  • 10k pull-up from gate to 3.3V

Measurements

When gate is LOW (~0.009V):

  • Source = 3.289V

  • Gate = 0.009V

  • Drain = 3.289V

  • Vgs ≈ −3.28V → MOSFET turns fully ON (as expected)

When gate is HIGH (3.287V):

  • Source = 3.289V

  • Gate = 3.287V

  • Vgs ≈ 0V → MOSFET should be OFF

However:

  • Drain measures ~2.89V

I added a 47k pulldown resistor from drain to GND. This reduced the drain voltage to ~2.4V — but not to 0V.

  • All STM32 GPIOs connected to the ESP32 are driven LOW.

  • If I completely remove the MOSFET, the ESP32 3V3 rail stays at 0V (no floating voltage).

Question

Is this expected off-state leakage/floating behavior for a discrete P-MOSFET in this configuration, or is there something wrong with my circuit?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps 8 months ago +1
    Is it possible you have active signals on the digital lines when the ESP32 is off, that seep to the power rail?
  • michaelkellett
    michaelkellett 8 months ago +1
    You have about 50uA leakage through the MOSFET when it's supposed to be turned off - the spec says it should be less than 1uA. Try shorting the MOSFET gate to source (I know its already meant to be at…
Parents
  • dougw
    0 dougw 8 months ago

    It sounds like the FET is damaged.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • arvindsa
    0 arvindsa 8 months ago in reply to dougw

    I had simultaneously soldered two boards. Using standard reflow profile on miniwares hotplate, yet both showing same behaviour. I will try replacing it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • arvindsa
    0 arvindsa 8 months ago in reply to dougw

    I had simultaneously soldered two boards. Using standard reflow profile on miniwares hotplate, yet both showing same behaviour. I will try replacing it.