• Products and Partners
    Products and Partners
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
Hardware Hacking
  • Challenges & Projects
  • Project14
  • Hardware Hacking
  • More
  • Cancel
Hardware Hacking
Blog Pong is Alive
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hardware Hacking to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 7 Jun 2020 11:11 PM Date Created
  • Views 4119 views
  • Likes 12 likes
  • Comments 13 comments
  • ay-3-8500-1
  • pong on a chip
  • hardwarehackingch
Related
Recommended

Pong is Alive

ralphjy
ralphjy
7 Jun 2020

As part of the Hardware Hacking Challenge I thought that I'd try to resurrect a Pong game that I built back in 1978.  My intro blog is here: Pong Game Circa 1978

 

Since it came out of my junk box and seemed to be in poor condition I thought that I probably should have proof of life before I invested too much effort in restoring it.  I was somewhat surprised that the 30 AWG wirewrap wire that I had used had oxidized and become brittle.  Some of the wires were actually broken.  I still use 28 AWG wire of the same vintage and the unused wire seems like new.  I guess maybe the wire may have reacted with the metallization of the wirewrap pins.  Anyway, I decided I should rebuild the circuit from scratch - just reusing the ICs and the crystal.

 

So, I cut the circuit board out of the case (who used connectors back then image).

 

Top of the board:

image

 

  • Pong chip AY-3-8500-1 (-1 for NTSC)  Date code 7707
  • 4072 CMOS Dual 4 input NOR
  • 4001 CMOS Quad 2 input NOR (might be a 4011 Quad NAND - can't read the marking)
  • 2MHz crystal
  • 6.3V zener - I had used 9V batteries for power (I probably could have run the parts directly but the typical voltage for the Pong chip is +6V to +7V)

 

The bottom of the board:  You can see the blackened wire ends wrapped on the pins.

image

 

Switches and jacks viewed from inside the case:

image

 

To verify life I thought that I'd just power it up and verify the clock circuit and that the video sync and composite outputs were working.

 

2 MHz oscillator waveform:

image

 

Video sync:

image

 

Composite video:

image

 

So looks good to proceed.  Hope to have a functioning game soon.  I just realized that I'll have to scare up a composite monitor......

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +4
    It is encouraging to see that technology this old can still be brought back to life. I was intrigued by the wire wrap as I started in my design days using wire wrap, mainly because it didn't use a soldering…
  • ralphjy
    ralphjy over 6 years ago in reply to dubbie +4
    We used to build test systems with large multi slot backplanes. Used a lot of automation back then. Too bad I don’t have pictures - the wire wrap machines were essentially large robots moving the wire…
  • jw0752
    jw0752 over 6 years ago +3
    Hi Ralph, This looks like fun. Another cause of the blackening might have been storage. Some papers and other materials will have a small amount of sulfur compounds which can cause blackening. Even if…
Parents
  • jw0752
    jw0752 over 6 years ago

    Hi Ralph,

     

    This looks like fun. Another cause of the blackening might have been storage. Some papers and other materials will have a small amount of sulfur compounds which can cause blackening. Even if the monitor proves to be a little challenge at least you have the key ingredient needed,  someone who still knows how to play pong.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago in reply to jw0752

    Hi John,

     

    I've seen that too, on stripped silver-plated wires.. In my case, they were just stored bare, in a plastic drawer for about 5 years, and that was sufficient to visibly darken them.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to shabaz

    I think that the 30 AWG wire is silver plated so you guys are probably right.  Not sure what the plating on the 28 AWG wire is but it could be different as it also has the upgraded kapton insulation to prevent cut-through.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 6 years ago in reply to shabaz

    I think that the 30 AWG wire is silver plated so you guys are probably right.  Not sure what the plating on the 28 AWG wire is but it could be different as it also has the upgraded kapton insulation to prevent cut-through.