IoT: In the Cloud
  • Challenges & Projects
  • Project14
  • IoT: In the Cloud
  • More
  • Cancel
IoT: In the Cloud
Blog Arduino MKR WIFI 1010 and Amazon Web Services: Safe MQTT with SSL and Certificate
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join IoT: In the Cloud to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 15 Mar 2019 5:04 PM Date Created
  • Views 5335 views
  • Likes 13 likes
  • Comments 13 comments
  • mqtt
  • mkr_1010
  • arduino mkr 1010
  • p14 mkr 1010
  • arduino_iot_cloud
  • aws
  • ssl
  • iotcloudch
  • certificate
  • secure
  • iot
  • arduino
Related
Recommended

Arduino MKR WIFI 1010 and Amazon Web Services: Safe MQTT with SSL and Certificate

Jan Cumps
Jan Cumps
15 Mar 2019
image

IoT: In the Cloud

Enter Your Project for a chance to win an Arduino MKR WAN 1300 Kit with a Compatable Lora Gateway or an MKR 1400 GSM with a Shield Combo + a $100 shopping cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

I'm preparing a project for Arduino Day.

I'll need to connect an Arduino MKR 1010 (thank you element14!) with AWS IoT.

And good news: the Arduino example is safe. An example where the safety is embedded from the get go.

Respect.

image

The exercise is easy. I just had to follow the tutorial from arduino.cc to make it work. And that proves that it isn't impossible to get everyone started with safe solution. The supplier just has to put the effort in to write the instructions and have no example where security is omitted.

 

What do you need?

 

You'll have to get a free AWS account, a Arduino MKR 1010 and a WiFi connection to the internet.

I am not repeating the excellent tutorial. If you haven't done so, read it now. Just follow it step by step.

There's one correction: where the tutorial says to download ArduinoMqtt, you actually have to install ArduinoMqttClient.

The example did compile out of the box on Arduino IDE 1.8.8. I had a compile error with version 1.8.1.

 

What does it do?

 

The sketch first logs on to your WiFi router. It will then make an SSL connection to AWS.

 

WiFiClient    wifiClient;            // Used for the TCP socket connection
BearSSLClient sslClient(wifiClient); // Used for SSL/TLS connection, integrates with ECC508
MqttClient    mqttClient(sslClient);

 

 

 

image

 

It uses certificates for authentication.

Once that's successful, it'll send messages to the topic arduino/outgoing and subscribe to messages posted on arduino/incoming.

 

Here you see messages from the MKR1010 arriving in AWS:

image

 

And this is a message from AWS retrieved by the MKR1010.

 

image

 

 

related blog posts
Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - How Long until the Next Recharge?
Arduino MKR WIFI 1010 and Amazon Web Services: Safe MQTT with SSL and Certificate
Project14 | IoT in the Cloud: Make Use of a Wireless Technology and a Cloud Provider!
Keithley DMM6500: Measure Amp-Hours of an Arduino MKR WIFI 1010
Manage Arduino MKR WIFI 1010 Battery Life in the Cloud - AWS, Graphs and Alerts
Arduino MKR 10xx, ETH Shield and Amazon Web Services: Safe MQTT with SSL and Certificate
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +2
    Jan, I want to get a better understanding of IoT so I will follow your advice and work through the tutorial. Do you know if it will work with a MKR 1000 (rather than MKR 1010) as that is what I have. …
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to dubbie +2
    no idea, Dubbie. I have this one since a few days and followed the tutorials. I don't have a 1000.
  • fmilburn
    fmilburn over 7 years ago in reply to fmilburn +2
    I went back this morning and started over and now it is working and I have no clue what is different. I have set up WiFi numerous times on Arduino, TI, and ESP microcontrollers without a problem. I usually…
Parents
  • fmilburn
    fmilburn over 7 years ago

    Hi Jan,

     

    I have not been able to connect the MKR 1010 to WiFi.  I am using the WiFiNINA library.  I ran the utility File/Examples/WiFiNINA/Tools/CheckFirmwareVersion from inside the IDE which gives the following output:

     

     

    WiFiNINA firmware check.

    Firmware version installed: 1.0.0
    Latest firmware version available : 1.2.0

    Check result: NOT PASSED
    - The firmware version on the module do not match the
       version required by the library, you may experience
       issues or failures.

     

    I tried to run the firmware updater unsuccessfully.  Did you have to update the firmware or have any problems?

     

    Thanks,

    Frank

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 7 years ago

    Hi Jan,

     

    I have not been able to connect the MKR 1010 to WiFi.  I am using the WiFiNINA library.  I ran the utility File/Examples/WiFiNINA/Tools/CheckFirmwareVersion from inside the IDE which gives the following output:

     

     

    WiFiNINA firmware check.

    Firmware version installed: 1.0.0
    Latest firmware version available : 1.2.0

    Check result: NOT PASSED
    - The firmware version on the module do not match the
       version required by the library, you may experience
       issues or failures.

     

    I tried to run the firmware updater unsuccessfully.  Did you have to update the firmware or have any problems?

     

    Thanks,

    Frank

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to fmilburn

    I'm using the same WiFiNINA lib.

    It is part of the Amazon Web Sevices example, and I used that sketch as base of my code.

    I didn't check the firmware version, everything 'just worked'.

     

    edit: everything in your WiFi settings seems to be case sensitive. SSID, passphrase

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to fmilburn

    Frank,

     

    I had something similar when I tried my MKR system. After some great frustration I realised that I had a MKR 1000 and not a MKR 1010. You might want to check you actually have a MKR 1010. Once I realised I had a MKR 1000 I had to change the library and it worked first time.

     

    Dubbie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to dubbie

    Thanks Dubbie,

    It is a MKR 1010.  I also have a MKR 1000 though which came with the Arduino Engineering Kit I won here on e14 a while back.  If I can’t get the 1010 to work I will try that.

    Frank

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to fmilburn

    I went back this morning and started over and now it is working and I have no clue what is different.  I have set up WiFi numerous times on Arduino, TI, and ESP microcontrollers without a problem.  I usually go back and make an effort to find where the problem was but have already invested too much time on this one.  Must have made a silly mistake somewhere....  I am using the V1.0.0 firmware that came on the board as I was unsuccessful in updating it.