Month of Robots
  • Challenges & Projects
  • Project14
  • Month of Robots
  • More
  • Cancel
Month of Robots
Blog Month of Robots - MeArm test update
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Month of Robots to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: aspork42
  • Date Created: 17 Jun 2019 2:40 AM Date Created
  • Views 2406 views
  • Likes 6 likes
  • Comments 1 comment
  • battery usage
Related
Recommended

Month of Robots - MeArm test update

aspork42
aspork42
17 Jun 2019

This is a follow-up post to this one from Project 14. The goal was to analyze the battery life of my Dirty Smart Button diaper logger. I meant to post this before the end of the month but left this sitting partially done in my "Drafts" until it was too late. I still wanted to post the follow up, so here it is!

 

Well it looks like I got 500 button presses exactly in the first round of tests. The MeArm was very useful in doing the lion's share of the work by laboriously pressing buttons time after time. I checked the SQL database and see /exactly/ 500 presses since I replaced the batteries last month (prepping for the Home Automation contest).

My estimates at the time of that article were based around 1000 mAh per battery x 4; so 4000 mAh available. That worked out to ~over 4 years of idle or roughly 2-4000 button presses. That seemed very optimistic at the time which is why I decided to actually test it. So since I got 25% of the estimate in the first round of testing, I started digging deeper.

 

Once the unit stopped waking up when the button was pressed, I measured the voltage battery pack. It was 2.65 VDC for 4x AAA batteries. Each cell was at .65 volts. So this was clearly lower that was is required to run the linear regulator of the Pro Mini at 3.3 volts. I didn't check the voltage until the next day, and I could see the until trying to do its power-up sequence as the LEDs kept trying to come on; but then it would fail. The DATASHEET for the voltage regulator on the Pro Mini (MIC5205) notes that dropout voltage; while load dependent; should be V-Out + ~.275 mV. So perhaps the Pro Mini was operating outside its spec of 3.3v for a while and/or the battery continued to drain while stuck in this loop before I got back to check it. I checked with my bench power supply and found that the system could work at 3.00 VDC but would fail at 2.9; so it was likely stuck in a power draining situation overnight before I came back to check it.

 

The next step was to pull the actual data sheet for the battery. I was running a Duracell AAA, model MN2400MN2400 Alkaline battery. Here is the datasheet.

image

 

According to this chart, a 1.5V AAA cell would really have more like 0.75-0.9 mAh instead of the 1,000 mAh that Google showed me. So a big fail on my part for not looking up the actual specs and trusting a quick google search. If I calculate the total run time of the system, 500 button presses @ 37 seconds works out to 308 minutes of run time; or 5.13 hours. If we look at the graph of current usage for my application, it looks like I fall between 100 and 250 mA. So that would probably land me right smack where I should be for a load of about 200mAh. Another calculation mistake I had done was adding the current for each battery. However since they were in series instead of parallel, that shouldn't have been done.

 

Additionally, according to some websites like this one, newborns can use about 10 diapers per day. Our actual usage was higher than that, but not all was logged through the Dirty Smart Button. With 500 presses, that gets 50 days or just shy of 2 months of exclusive use.

 

So I actually came out right where I should be, although I would still have liked to see some more usage available.

 

A big thanks to the entire E14 team for sponsoring the contest! I received a finisher package of a RaspberryPi, GraspIO, some stickers, and my favorite - a wind-up action figure - which I've wanted for some time now!

 

image

 

- James

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 7 years ago +3
    James, Well done on working out battery life and getting it accurate. I have done some battery calculations like this myself and gettingaccurate results is quite difficult. It can depend on the current…
  • dubbie
    dubbie over 7 years ago

    James,

     

    Well done on working out battery life and getting it accurate. I have done some battery calculations like this myself and gettingaccurate results is quite difficult. It can depend on the current flow when in operation, how long you use the current for and the time between uses. Being a chemical process there are all sorts of osmosis, depletion areas and recovery times to consider. My best result was a system that came on once every hour using an interrupt to move out of sleep mode, which flashed an LED if it was dark, comprised of a an low voltage 8 pin PIC powered by two AA batteries. It had an engraved block of Perspex above the LED with a logo on, which was created as a give-away for a conference. The case/holder was a 3D printed spring affair. It was all designed to promote the electronics, programming, manufacturing and design capability of the University. My prototype lasted for over two years with the same batteries and I retired before the batteries ran out so I never found out it's maximum life.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down