• Products and Partners
    Products and Partners
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
Movers and Shakers
  • Challenges & Projects
  • Project14
  • Movers and Shakers
  • More
  • Cancel
Movers and Shakers
Blog Jumbo Servo
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Movers and Shakers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 31 Jul 2018 1:20 PM Date Created
  • Views 20182 views
  • Likes 20 likes
  • Comments 23 comments
  • ardintermediate
  • moversshakersch
  • arduino_projects
  • questionofscalech
Related
Recommended

Jumbo Servo

Workshopshed
Workshopshed
31 Jul 2018

I was building a big project and wanted to move the nozzle of a squirting flower, and the only servos I had were micro servos which did not have enough power to move the mechanism, so I decided to build something, a Jumbo Servo.

image

As mentioned in Motor Drive Control for Makers  a servo consists of a motor with some kind of position feedback and a control circuit. I decided that a potentiometer and an arduino should be capable of this. I found a 12v gearbox motor in the spares drawer and after a little cleaning and lubrication got that running. There was a gear on the output shaft that could be used for driving a the potentiometer. I added a mounting plate and determined where I could add a potentiometer. A 3D printed gear was added to slip onto the pot and mesh with the output gear. Also something to drive the motor would be needed and I had a suitable L298 H-Bridge module which fitted the spec.

image

 

 

So that my jumbo servo would look the part, I made a wooden case and wooden servo horn. A 3D printed output shaft was also added.

imageimage

Next up was the electronics. I decided to go with I2C for communication rather than the analogue PWM which is typically used by a servo. This allows me to stop the motor when the servo has reached it's destination rather than constantly seeking position, it also means that I can read back the position to the controlling software and avoid that twitch you get when you first power on a servo.

 

To test this I used two arduinos and used the examples from Arduino to work out what code was needed. Because I was using a long cable (for I2C at least) I added some low value pullups on the servo end.

image

Here's my first draft of the code.

 

#include <Wire.h>

const int slaveAddress = 8;

const int sensePin = A0;
const int drivePin1 = 3;
const int drivePin2 = 4;
const int speedPin = 5; //Needs to support PWM

short registers[5];
int readCmd;
int blink = 0;

enum readRegisters { Target = 0,
  Running = 1,
  Position = 2,
  Speed = 3,
  Direction = 4
  };

enum commands { CmdStop = 1,
  CmdAngle = 2,
  CmdSpeed = 3,
  };

void setup() {
  stop();

  pinMode(drivePin1, OUTPUT);
  pinMode(drivePin2, OUTPUT);
  pinMode(speedPin, OUTPUT);
  pinMode(13, OUTPUT); //Onboard LED
  pinMode(sensePin, INPUT);

  Wire.begin(slaveAddress); // join i2c bus with address #8
  Wire.onReceive(receiveEvent); // write data
  Wire.onRequest(requestEvent); // requests to read data

}

void loop() {
  digitalWrite(13, blink);
  blink = !blink;  
  
  registers[Position] = analogRead(sensePin);

  if (registers[Running]) {
       if (registers[Direction] == 1) {
            if (registers[Position] >= registers[Target]) {
                 stop();
            }
       }
       if (registers[Direction] == -1) {
            if (registers[Position] <= registers[Target]) {
                 stop();
            }
       }
  }
}

void stop() {
  digitalWrite(drivePin1, LOW);
  digitalWrite(drivePin2, LOW);
  analogWrite(speedPin, 0);
  registers[Running] = false;
}

// function that executes whenever data is received from master
// this function is registered as an event, see setup()
void receiveEvent(int bytesReceived) {
  char command;
  int value;
  int lowB;
  int highB;

  switch (bytesReceived) {
  case 1:
  //Read request register
  readCmd = Wire.read();
  break;
  case 3:
       command = Wire.read(); // receive byte as a character
       //Pi is low endian
       lowB = Wire.read();
       highB = Wire.read();
       value = (highB << 8) | lowB;

       switch (command) {
       case CmdStop:
            stop();
            break;
       case CmdAngle:
            registers[Target] = value;
            registers[Running] = true;
            if (registers[Target] > registers[Position]) {
                 digitalWrite(drivePin1, LOW);
                 digitalWrite(drivePin2, HIGH);
                 registers[Direction] = 1;
            }
            else {
                 digitalWrite(drivePin2, LOW);
                 digitalWrite(drivePin1, HIGH);  
                 registers[Direction] = -1;
            }
       break;
       case CmdSpeed:
            registers[Speed] = value;
            analogWrite(speedPin, registers[Speed]);
       break;
       }
  break;
  default:
       for (int a = 0; a < bytesReceived; a++) {
            Wire.read(); // throw buffer away so we can read again
       }
  }
}

// function that executes whenever data is requested by master
// this function is registered as an event, see setup()
// Don't add serial print to this routine, it will error!!

void requestEvent() {

  short value = registers[readCmd];
  Wire.write((uint8_t *)&value, sizeof(value));
}

 

I've got myself an AdaFruit "ItsyBitsy" which is basically a small form factor Arduino Leonado. So the next step is to wire this in, instead of the Arduino.

 

image

I'll also need to do some simple calibration to turn the 0-1023 value into a degrees value. Because of the gearing on the pot the servo can do a bit more than 180 degress so I should be able to set it up with a safe limit so I don't over drive the pot.

image

Have added a breakout board for the ItsyBity and completed some further testing with some LEDs in place of the H-Bridge,

imageimage

I then did some testing with the H-Bridge. I used back to back LEDs to check that the circuit was wired correctly and the software was working. After a few loose connections I got that working. However, swapping the motor in caused my 2A PSU to shutdown.

 

So I plugged these into the bench power supply (thanks again Secret Santa) and set the voltage and current limit. Luckily I happened to have a slightly smaller motor that had the same size shaft and screw holes that took a lot less current. Next up I'll swap that in.
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
The gearbox I used is available on CPC.

  • Sign in to reply

Top Comments

  • korn
    korn over 8 years ago +8
    Love the RC servo looking enclosure. I made a big servo to steer a power wheels jeep. Now I want to make a box like that for mine.......
  • beacon_dave
    beacon_dave over 8 years ago in reply to mcb1 +7
    Nice servo upgrade, but I'm sure you can go bigger ... Hmmm... now that could be the basis for a future theme... "go bigger" "big, bigger, biggest" "max it up" "supersize" "size matters" Equally it could…
  • jw0752
    jw0752 over 8 years ago +6
    Hi Andy, Really cool build. I like how you even went for the visual and made it look like a micro servo. John
Parents
  • dgashby
    dgashby over 7 years ago

    Nice build Andy, looking forward to seeing a video of the complete watering system in action. :-)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dgashby
    dgashby over 7 years ago

    Nice build Andy, looking forward to seeing a video of the complete watering system in action. :-)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Workshopshed
    Workshopshed over 7 years ago in reply to dgashby

    Hi Dean, I'm afraid the project got decomissioned at the end of last year as it was taking up too much space in the shed.  It did not spray particularly far so I'd suggest connecting it to a hose rather than a sprayer if you want maximum fun.

     

    You can read more about how it was made at https://hackspace.raspberrypi.org/issues/9

     

    I was also hoping that the BCS would publish the video of my servo demo but that seems to have got lost so I'll see if I can record one of the servo and control panel in action.

    • Cancel
    • Vote Up +3 Vote Down