Music Time
  • Challenges & Projects
  • Project14
  • Music Time
  • More
  • Cancel
Music Time
P14 Music Time Blog 215 Instrument MIDI Synthesizer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Music Time to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 13 Feb 2023 6:49 AM Date Created
  • Views 11896 views
  • Likes 19 likes
  • Comments 17 comments
  • dougw
  • musictimech
  • anthems
  • VS1053
  • MIDI synthesizer
Related
Recommended

215 Instrument MIDI Synthesizer

dougw
dougw
13 Feb 2023

image

Intro

In my ongoing quest for a cheap MIDI synthesizer, I came across the VS1053 chip which is a pretty spectacular audio chip. It has many features like encoding and decoding many audio standards and implementing several different interface standards. The datasheet is linked below for those interested, however I was specifically interested in its ability to play any note from 215 different synthesized instruments. In fact it can play up to 16 notes or instruments at the same time.
I also found that there are many suppliers who have used this chip in low cost audio modules, unfortunately none of them really cater to its MIDI capabilities. Almost none of them even make the MIDI selection pin available to be jumpered, and of course none of them have a MIDI connector. They all seem to implement the chip as an MP3 player, which is fine, but why ignore the synthesizer capabilities?
So naturally I had to design my own synthesizer around this chip. All the "music" in this blog is produced by this synthesizer, except the percussion intro. I played that on a PC to contrast it with this synthesizer. The percussion sequences may only loosely be called music, because I made them all up and I am not a musician. Fortunately a program called Hydrogen makes fooling around with percussion sequences a lot of fun. I am not playing popular music in this blog since we have to wait until the musicians involved have been dead for a century or two to play that music. Of course that music may no longer be popular then, but hopefully some of the music capabilities of this chip will come through just playing some old classical music. This synthesizer can play just about any real music and it all sounds great, although I have to say it sounds better playing modern music. About the audio setup, my microphone system is adding plenty of noise because my audio lab is not set up yet and also these speakers are not hi-fi. I don't quite get how some web sites will play just about any music ever written down, but every expert on the subject indicates that it is illegal to do so.
Anyway, if you have some unencumbered MIDI music and want to hear what this device sounds like playing it, enclose it below, and I will post it.

The Circuit Card

image

Design Features
This system is based on the VS1053 audio processor. The custom PCB for this chip is designed to provide a full breakout of every pin on the chip to 0.1" pitch connector pads that will insert directly into a standard breadboard. In fact it can be used as a breakout card for any 48 pin QFN footprint chip of the same physical size. The PCB does not stop there, however, it also breaks out a full microcontroller interface to allow it to have a display and SD card to store music or audio. It also has an auxiliary audio input connector, a stereo power amplifier and an optically isolated MIDI connector. There is a USB connector to supply power to the circuit and regulators to step down to 3.3V and 1.8V as required by the chip.

Description and Demo Video
The first video plays a percussion sequence I made using Hydrogen, first with a PC then using this synthesizer. Then the device is opened up to explore what is inside, followed by an explanation of the 3D printed case.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Anthems
Here are excerpts from a selection of anthems just to show that the synthesizer can play a bunch of instruments. How many anthems do you recognize? I have a tenuous connection to most of these countries but on a good day I would not recognize more than 4 of these. If your anthem is not included, indicate in the comments which one is missing and I will add more to the blog.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Classical Music
In case you didn't recognize any of the anthems, here are a few excerpts from some classical pieces everyone is familiar with:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

MIDI Tools & Synthesizer Connections

image

This video shows how the synthesizer connects to MIDI sources:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Schematic
Here is the schematic

image

In case it isn't clear what relationship this project has with clocks, everything about music has to do with clocks, especially digital music. Every note is made up of frequencies which in a synthesizer are generated by clocks. The timing between notes is controlled by clocks and even the software that is running is all based on clocks. This circuit includes a 12.288 MHz crystal clock that is used in the synthesis of instrument sounds and notes. The note timing is coming from the MIDI source, which is also a clock driven computer.

PCB Layout
Here is the PCB layout

image

BoM
Here is the parts list:

Part Value Package Description MFR FARNELL NEWARK #
C1, C6, C14, C15 4.7nf C0805 CAPACITOR
C2-C4,C9,C12,C13,C16,C20 1uf C0805 CAPACITOR
C5,C8,C22-C30 .1uf C0603K CAPACITOR
C18 .1uf C0805 CAPACITOR
C7, C19, C21 10uf C0805 CAPACITOR
C10, C11 18pf C0805 CAPACITOR
C17 .01uf C0805 CAPACITOR
D1 4148 SOD123 DIODE
J1, J2 RCA1 RCA1 RCA Connector
J4 MTA10-100 10-100 AMP MTA connector AMP
J5 PG203J PG203J MIC/HEADPHONE JACK
J6 MAB5SH MAB5SH Female CONNECTOR 809883
J7 USB-MB-H USB Connectors
LED LED5MM LED
LED1 LED5MM LED
M2 PAM8403V PAM8403V PAM8403 Stereo Amplifier
Q1 12.288MHz HC49/S CRYSTAL 1667008 75Y2298
R1,R2,R4,R9,R10,R13,R14,R15 1K M0805 RESISTOR
R3, R8 100K M0805 RESISTOR
R5 220 M0805 RESISTOR
R6 4.7K M0805 RESISTOR
R7 270 M0805 RESISTOR
R11 1M M0805 RESISTOR
R12, R16 10K M0805 RESISTOR
U1 VS1053 LQFP48 VS1053 synthesizer VLSI
U2 3.3V SOT223 LDO regulator
U3 1.8V SOT223 LDO regulator
U4 6N138 DIL08 Optocoupler ONSemi 93R4620
F1-F4 DTRPOF-40059 Push on rubber feet Duratool 43Y4284

Enclosure
The 3D print files used to make the case are enclosed:

Discussion
This project ended up to be a very neat, very useable, and very low cost MIDI synthesizer capable of playing any MIDI music. The PCB has lots of flexibility to be used in different applications, but this application is focused on its MIDI capabilities.
I am extremely happy with the way it turned out. It works and sounds better than expected, and the 3D printed box ties it all up into a fully deployable device. Now I need to get busy learning how to compose real music and perhaps building a MIDI controller. Hopefully members will contribute some MIDI files they want this device to play.

Enclosure STL Files

MIDIsynthSTLfiles.zip

Links

/challenges-projects/project14/musictime?ICID=P14main-feature-widget

/challenges-projects/project14/musictime/b/blog/posts/project14-music-time-build-projects-involving-clocks-and-musical-instruments?ICID=musictime-p14-3step

http://hydrogen-music.org/downloads/

http://www.midieditor.org/

https://www.vlsi.fi/fileadmin/datasheets/vs1053.pdf

  • Sign in to reply

Top Comments

  • dougw
    dougw over 3 years ago in reply to robogary +1
    I use Autodesk 123D Design for 3D design. (because it is free and simple to use) I use Hydrogen to create music which is saved as a MIDI file. I use MIDI Editor on a PC (I will put a link in the blog…
  • javagoza
    javagoza over 3 years ago in reply to dougw

    Thanks dougw , I'll go for a USB-to-MIDI port cable. I thought it was still possible to skip that step to attack from a virtual COM port, but it might be hard to meet the MIDI timing requirements.

    I just asked ChatGPT what a parser for MIDI in SystemVerilog would look like, ha ha!

    module midi_parser (
      input  wire          rx,
      output reg [7:0]     data_out,
      output reg           data_valid
    );
    
      typedef enum {
        RX_WAIT,
        RX_STATUS,
        RX_DATA
      } rx_state_t;
    
      reg [2:0] rx_bits;
      reg [3:0] rx_count;
      reg [7:0] rx_data;
      reg [2:0] rx_state;
      reg [7:0] last_status;
    
      always @(posedge rx) begin
        rx_bits <= rx_bits + 1;
    
        case (rx_state)
          RX_WAIT: begin
            if (rx_bits >= 8'b0000_0001) begin
              rx_count <= 3'b001;
              rx_data <= 8'b0;
              rx_state <= RX_STATUS;
            end
          end
          RX_STATUS: begin
            rx_data <= {rx_data[6:0], rx};
            if (rx_bits == 8'b0000_1001) begin
              if ((rx_data >= 128'b10000000) && (rx_data <= 128'b10111111)) begin
                last_status <= rx_data;
                rx_count <= 3'b000;
                rx_state <= RX_DATA;
              end else begin
                rx_state <= RX_WAIT;
              end
            end
          end
          RX_DATA: begin
            rx_data <= {rx_data[6:0], rx};
            rx_count <= rx_count + 1'b1;
            if (rx_count == ((last_status[4:0] == 4'b11111) ? 3'b001 : 3'b000)) begin
              data_out <= rx_data;
              data_valid <= 1'b1;
              rx_state <= RX_WAIT;
            end
          end
        endcase
      end
    
      always @(posedge rx) begin
        rx_bits <= 8'b0;
      end
    
      assign data_valid = (rx_state == RX_DATA) && (rx_count == ((last_status[4:0] == 4'b11111) ? 3'b001 : 3'b000));
    
    endmodule
    

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to robogary

    I should mention this synthesizer can be connected directly to any MIDI controller like a keyboard or MIDI drum pads without needing a computer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to robogary

    I use Autodesk 123D Design for 3D design. (because it is free and simple to use)

    I use Hydrogen to create music which is saved as a MIDI file.

    I use MIDI Editor on a PC (I will put a link in the blog) to view the MIDI files (or edit them) and send (play) MIDI commands to a USB port.

    I use a USB-to-MIDI cable to connect the USB port to the MIDI synthesizer. (I'll put a block diagram of the whole system in the blog)

    The videos show what the MIDI Editor screen looks like when "playing" MIDI to a USB port. It can also play internally on a PC with the built-in MIDI player in Windows.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dougw
    dougw over 3 years ago in reply to dang74

    I will be beefing up the material in the blog - those references indicate some of what I am planning to add.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • robogary
    robogary over 3 years ago

    Really nice project.

    What 3D modeling tool pkg do you use ? 

    I'm a bit confused on the controls, does the MIDI run by itself, or does it need to interface to Hydrogen on a PC, or is a bit of both ? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>