NanoRama
  • Challenges & Projects
  • Project14
  • NanoRama
  • More
  • Cancel
NanoRama
Blog TinyML on Arduino Nano 33 BLE Sense - Gesture Recognition
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NanoRama to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jomoenginer
  • Date Created: 6 Apr 2020 6:27 AM Date Created
  • Views 15950 views
  • Likes 15 likes
  • Comments 7 comments
  • tensorflow
  • python
  • tinyml
  • nano 33 ble sense
  • nanoramach
  • tensorflow lite
  • arduino
Related
Recommended

TinyML on Arduino Nano 33 BLE Sense - Gesture Recognition

jomoenginer
jomoenginer
6 Apr 2020
image

NanoRama

Enter Your Project for a chance to win a Nano Grand Prize bundle for the most innovative use of Arduino plus a $400 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

Overview

 

This is to chronicle my experience with running TinyML on the Arduino 33 BLE Sense.

 

I initially followed the TensorFlow Lite for Microcontrollers examples using a STM32F746G Discovery kit, but moved to the Arduino TinyML Workshop Examples created by Sandeep Mistry and Dominic Pajak to gain familiarity with running TinyML on the Nano board for the NanoRama thing. This includes both an Arduino and TensorFlow post as well as using Google's Colaboratory , or 'Colab' to run Python code in Jupyter Notebooks. This eliminates the need to install all the dependencies on a system or use a Docker Container to run the examples.

 

What is TinyML

 

TinyML came about when Pete Warden joined Google in 2014 and discovered how the OK Google group was using neural networks that were just 14  kilobytes (KB) running on DSP's to process the 'OK Google" wake word from Android smart phones. Warden's background was from the image side of the house so seeing something run in such a limited space stirred a bit of curiosity in him.  He initially worked on getting TensorFlow to run on Android and iOS devices and then later moved to TensorFlow Lite but then sought to use even smaller devices.  Warden discovered in the audio arena there was Pixel’s Music IQ for predictive maintenance (like PsiKick) and on the vision side Qualcomm’s Glance camera module which combines image sensor and a low-power processor that runs computer-vision algorithms.  After conversations with colleagues, Warden focused on getting a neural network to run on a device that consumes only 1 mW of power and without the need of wired power.  The other constraint was that the processor should cost less than $1. The main focus for TinyML use is for edge devices where a sensor can be deployed with little or no maintenance. A phrase that pops up with regards to devices running TinyML is “peel-and-stick  sensors”.  This is the concept that the device is to run for years without the need of a battery change and be placed and forgot except when data is needed from it.  An area that Warden mentions where these sort of devices could be used is in Industrial Production lines where running power to a device is not very feasible.

 

The 3 main devices that are used to run TinyML examples are the Sparkfun Edge Board, STM32F746G Discovery kit, and the Arduino Nano 33 BLE Sense.  There are others that are moving to use TinyML but in this post the Arduino Nano 33 BLE Sense will be used.

 

Related Post:

TinyML on Arduino Nano 33 BLE Sense - Fruit Identification

TinyML on Arduino Nano 33 BLE Sense - Person Detection with BLE

 

References:

 

  TensorFlow for Microcontrollers

  https://www.tensorflow.org/lite/microcontrollers

 

  How-to Get Started with Machine Learning on Arduino

  https://blog.tensorflow.org/2019/11/how-to-get-started-with-machine.html

 

  Get started with machine learning on Arduino

  https://blog.arduino.cc/2019/10/15/get-started-with-machine-learning-on-arduino/

 

  TinyML on Arduino Workshop 2019

  https://github.com/sandeepmistry/aimldevfest-workshop-2019

 

  TinyML Book

  https://tinymlbook.com/

 

   What’s TinyML good for (video)

  https://www.youtube.com/watch?v=Wuq2aP5O5Z0

 

  How-to Get Started with Machine Learning on Arduino (Colab example)

   https://blog.tensorflow.org/2019/11/how-to-get-started-with-machine.html

 

Hardware

- Arduino Nano 33 BLE Sense

         https://store.arduino.cc/usa/nano-33-ble-sense

 

 

Prepare Arduino IDE

 

1. Install Arduino Nano 33 BLE Sense Board Libraries

- Arduino nRF528x Boards (Mbed OS)

 

2. Install Arduino Nano 33 BLE Sense Peripheral Libraries

- ST LSM9DS1 - 3-axis accelerometer and 3-axis gyroscope and 3-axis magnetometer

Library: Arduino_SM9DS1

- ST MP34DT05 - Digital MEMS microphone

Library: AudioSound

- ST LPS22HB - barometer sensor

Library: Arduino_LPS22HB

- BC APDS9960 - Gesture sensor

Library: Arduino_APDS9960

- ST HTS221 - Relative humidity and temperature sensor

Library: Arduino_HTS221

- Nano 33 BLE

Library: ArduinoBLE

 

3. Install TensorFlow Lite library (Arduino IDE)

  Library: Arduino_TensorFlowLite

image

 

4. Download IMU_Capture.ino example and load into Arduino IDE :

    https://blog.tensorflow.org/2019/11/how-to-get-started-with-machine.html

    https://github.com/arduino/ArduinoTensorFlowLiteTutorials/blob/master/GestureToEmoji/ArduinoSketches/IMU_Capture/IMU_Capture.ino

 

image

 

5. Use Arduino IDE Serial Plotter to view sensor data

  Tools→Serial Plotter

image

 

  a.  Pickup the Nano 33 BLE Sense and simulate a punch or arm flex movement to see the data plotted in the Serial Plotter:

 

image

 

 

Get started with machine learning on Arduino

https://blog.arduino.cc/2019/10/15/get-started-with-machine-learning-on-arduino/

 

1. Capture gesture data

Collected data for the following files from the Serial Monitor

- punch.csv (10 times)

- flex.csv (10 times)

NOTE: Ensure to disable “Show timestamp” from Serial Monitor

 

Example Punch:

a. Pickup the Nano 33 BLE Sense and simulate a punch motion with the board in your hand.

b. Repeat 10 times

c. Notice the data that is collected in the Serial Monitor.

image

 

  d. Copy the data from the Serial console and create a .csv file associated with the action: either punch.csv or flex.csv.

      NOTE: Ensure the first line in the file looks like the following:

              aX,aY,aZ,gX,gY,gZ

 

 

2. Go to Colab for Jupyter notebook

 

   Arduino Example:

   https://colab.research.google.com/github/arduino/ArduinoTensorFlowLiteTutorials/blob/master/GestureToEmoji/arduino_tinyml_workshop.ipynb

 

   GitHub Examples:

   https://github.com/arduino/ArduinoTensorFlowLiteTutorials/


  image


      NOTE: When first loading the Jupyter Notebook, a Warning screen will appear.

                  Just click RUN ANYWAY

image

 

3. Run Setup Environment.

     NOTE: This will result in the install of a number of required packages

image

 

4. Upload the capture data

- punch.csv

- flex.csv

 

  Select the Folder icon in the left Window Pane to upload the .csv files

 

image

 

5. Graph Data (Optional)

image

 

image

 

6. Train Neural Network based on .csv data

Output if successful:

 

TensorFlow version = 2.0.0-rc1
   
 Processing index 0 for gesture 'punch'.
  There are 10 recordings of the punch gesture.
 Processing index 1 for gesture 'flex'.
  There are 10 recordings of the flex gesture.
 Data set parsing and preparation complete.

 

 

 

7. Randomize and split the input and output pairs for training

 

  Output if successful:

   Data set randomization and splitting complete.

 

8. Build and Train the Model

  From Notebook:

  - Build and train a TensorFlow model using the high-level Keras API

 

  Output when run:

Train on 12 samples, validate on 4 samples
 Epoch 1/600
 WARNING:tensorflow:Entity <function Function._initialize_uninitialized_variables.<locals>.initialize_variables at 0x7fe172912ae8> could not be transformed and will be executed as-is. Please report this to the AutoGraph team. When filing the bug, set the verbosity to 10 (on Linux, `export AUTOGRAPH_VERBOSITY=10`) and attach the full output. Cause: module 'gast' has no attribute 'Num'
 WARNING: Entity <function Function._initialize_uninitialized_variables.<locals>.initialize_variables at 0x7fe172912ae8> could not be transformed and will be executed as-is. Please report this to the AutoGraph team. When filing the bug, set the verbosity to 10 (on Linux, `export AUTOGRAPH_VERBOSITY=10`) and attach the full output. Cause: module 'gast' has no attribute 'Num'
 12/12 [==============================] - 1s 50ms/sample - loss: 0.3119 - mae: 0.5501 - val_loss: 0.2502 - val_mae: 0.4998
 Epoch 2/600
 12/12 [==============================] - 0s 3ms/sample - loss: 0.2653 - mae: 0.5116 - val_loss: 0.2498 - val_mae: 0.4994
 Epoch 3/600
 12/12 [==============================] - 0s 3ms/sample - loss: 0.2620 - mae: 0.5116 - val_loss: 0.2493 - val_mae: 0.4991
 Epoch 4/600
 12/12 [==============================] - 0s 3ms/sample - loss: 0.2628 - mae: 0.5082 - val_loss: 0.2488 - val_mae: 0.4985

 

 

9. Verify

    Graph the models performance vs validation

 

- Graph Loss

image

 

 

- Graph the loss again, skipping a bit of the start

image

 

- Graph the mean absolute error

image

10. Run with Test Data

image

 

11. Convert the Trained Model to Tensor Flow Lite

 

- Output from Notebook

WARNING:tensorflow:Entity <function Function._initialize_uninitialized_variables.<locals>.initialize_variables at 0x7fe16a17d598> could not be transformed and will be executed as-is. Please report this to the AutoGraph team. When filing the bug, set the verbosity to 10 (on Linux, `export AUTOGRAPH_VERBOSITY=10`) and attach the full output. Cause: module 'gast' has no attribute 'Num' WARNING: Entity <function Function._initialize_uninitialized_variables.<locals>.initialize_variables at 0x7fe16a17d598> could not be transformed and will be executed as-is. Please report this to the AutoGraph team. When filing the bug, set the verbosity to 10 (on Linux, `export AUTOGRAPH_VERBOSITY=10`) and attach the full output. Cause: module 'gast' has no attribute 'Num' Model is 147764 bytes 

 

 

12. Encode the Model in an Arduino Header File

- Output from Notebook

/bin/bash: xxd: command not found

Header file, model.h, is 35 bytes.

 

Open the side panel (refresh if needed). Double click model.h to download the file.

 

NOTE: The model.h file has a blank array from the Colab exercise.

Issues were seen while running the example and an issue was filed on GitHub:

https://github.com/arduino/ArduinoTensorFlowLiteTutorials/issues/11

 

- Found I had to copy the files to a Linux system and run the commands manually:

 

- create_content.sh

#!/bin/bash
 
  
 echo "const unsigned char model[] = {" > content/model.h
 cat gesture_model.tflite | xxd -i >> content/model.h
 echo "};" >> content/model.h

 

- get_header_size.py

#!/usr/bin/env python3
  
 import os
 model_h_size = os.path.getsize("./content/model.h")
 print(f"Header file, model.h, is {model_h_size:,} bytes.")
 print("\nOpen the side panel (refresh if needed). Double click model.h to download the file.")

 

 

    - Once complete, copy the contents of the model.h file to the model.h in the Arduino IDE

 

13. Classifying IMU Data

- Switch back to tutorial

https://blog.arduino.cc/2019/10/15/get-started-with-machine-learning-on-arduino/

 

14. Down load the IMU_Classifier.ino Sketch and create a model.h tab in the IMU Arduino IDE project to load the model.h code from step 12.

https://github.com/arduino/ArduinoTensorFlowLiteTutorials/blob/master/GestureToEmoji/ArduinoSketches/IMU_Classifier/IMU_Classifier.ino


  image

 

 

15. Compile and Upload the Sketch to the Nano 33 BLE Sense


 

16. Open the Serial Monitor and perform the punch or flex motions again.

 

The results from the model will be shown in the Serial console:

NOTE: This example resulted in about 50/50 split when doing a punch or flex

 

image

 

That is it for this example.

 

NEXT:  Fruit Identification

  • Sign in to reply

Top Comments

  • jomoenginer
    jomoenginer over 6 years ago in reply to dubbie +3
    Thanks. The step about running the script on Linux should not be necessary if the Colab project was working properly. What I provided was a workaround since it did not work as is. I filed a bug issue to…
  • jomoenginer
    jomoenginer over 6 years ago in reply to ankur608 +3
    Thanks. I plan to merge an BLE example with the Fruit ID (or color id) example so the results can be viewed remotely. The end goal is to add a ArduCam and to add vision recognition to the mix.
  • ankur608
    ankur608 over 6 years ago +2
    Great implementation of TinyML, maybe you can combine 'punch-emoji' & 'fruit-id' codes into a sort of 'fruit-slash classifier' like Fruit Ninja.
Parents
  • ankur608
    ankur608 over 6 years ago

    Great implementation of TinyML, maybe you can combine 'punch-emoji' & 'fruit-id' codes into a sort of 'fruit-slash classifier' like Fruit Ninja.image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jomoenginer
    jomoenginer over 6 years ago in reply to ankur608

    Thanks.

     

    I plan to merge an BLE example with the Fruit ID (or color id) example so the results can be viewed remotely.

     

    The end goal is to add a ArduCam and to add vision recognition to the mix.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jomoenginer
    jomoenginer over 6 years ago in reply to ankur608

    Thanks.

     

    I plan to merge an BLE example with the Fruit ID (or color id) example so the results can be viewed remotely.

     

    The end goal is to add a ArduCam and to add vision recognition to the mix.

    • Cancel
    • Vote Up +3 Vote Down