Photography
  • Challenges & Projects
  • Project14
  • Photography
  • More
  • Cancel
Photography
Blog Finding Nemo - Field Day
  • Blog
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Photography to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: scottiebabe
  • Date Created: 28 Jul 2021 3:15 PM Date Created
  • Views 2363 views
  • Likes 10 likes
  • Comments 6 comments
  • photographych
Related
Recommended

Finding Nemo - Field Day

scottiebabe
scottiebabe
28 Jul 2021

The day arrived to finally put the Nemo Discovery Apparatus out into the wild! I lashed up the solar panel to my backpack and headed down to the river.

 

I can't help but laugh when I see this photo, the solar panel is borderline too big for a backpack, but it does put out the watts!

image

 

Putting the solar panel in the water was really just to validate the proof of concept. The pool noodle pontoons could drastically be improved for a long-term deployment.

 

image

 

Placing the camera into the water for the first time! No Leaks image

 

image

 

Giving the system a final test from motioneye on my phone.

image

 

Everything looks good.

 

To capture video I ssh'd into the PI on the nemo WIFI network and executed the raspivid command as:

 

raspivid -t $((10*60*1000)) -o nemo.h264 -v

 

I used some inline bash arithmetic since the time parameter is taken in ms. Luckily I didn't get burned, but as soon as I got to the river I realized I should have installed the screen terminal. If WIFI were to have dropped out between the laptop and PI, the ssh session would have forced raspivid to close prematurely. Thankfully, this did not happen to me image. Perhaps there is other Linux foo to avoid this problem too.

 

Looking down into the water I could see everything very clearly. Here is a riverside photo where I can see a crayfish walking around.

 

image

 

Assorted Clips Captured

This is just a collection of raw clips captured with the HQ Camera, feel free to fast-forward.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I had to lower the lens aperture to try and get a usable depth of field. At first I was filming in f/8. Later on I knocked down the aperture to somewhere midway between f/8 and f/16.

 

Next time I place a Newark order I will add a 6mm Wide Angle Lens6mm Wide Angle Lens to my shopping cart.

 

I think a large piece of black cardstock on the top inside of the container would have cut down on sunlight reflecting of the inside of the container.

 

I hope you enjoyed reading along as much as I enjoyed making and documenting this project.

 

Thanks again Element14!

 

 

References

https://ontarionature.org/wp-content/uploads/2017/10/crayfish_apr08.pdf

https://www.dfo-mpo.gc.ca/species-especes/publications/baitfish-poissons-appats/page01-eng.html

  • Sign in to reply

Top Comments

  • javagoza
    javagoza over 5 years ago +3
    Brilliant. I love the solar backpack.
  • dougw
    dougw over 5 years ago +2
    Cool project. Getting it all working in the wild is very impressive. I liked the crayfish footage at the end of the video. You found Nemo and Mr. Krabs.
  • scottiebabe
    scottiebabe over 5 years ago in reply to 14rhb +2
    Surprising, the only mishap was capturing a bug in between camera lens and lens cap the day prior. I discovered this the next day when by seeing mess of bug excretions on the lens glass. Fortunately with…
Parents
  • 14rhb
    14rhb over 5 years ago

    There's something great and care-free about seeing electronics being floated in the river; well done for doing what I'm not brave enough to try image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 5 years ago in reply to 14rhb

    Surprising, the only mishap was capturing a bug in between camera lens and lens cap the day prior. I discovered this the next day when by seeing mess of bug excretions on the lens glass. Fortunately with lens being glass it was easy to clean:).

     

    Though, I wasn't brave enough to homebrew a viewing port. I still have a lot to research to do about underwater photography. With the water having a different index of refraction than air the problem gets even more complicated yet. Which was likely turning the telephoto lens into a super-telephoto lens.

    image

    Thank you for the words of encouragement.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • scottiebabe
    scottiebabe over 5 years ago in reply to 14rhb

    Surprising, the only mishap was capturing a bug in between camera lens and lens cap the day prior. I discovered this the next day when by seeing mess of bug excretions on the lens glass. Fortunately with lens being glass it was easy to clean:).

     

    Though, I wasn't brave enough to homebrew a viewing port. I still have a lot to research to do about underwater photography. With the water having a different index of refraction than air the problem gets even more complicated yet. Which was likely turning the telephoto lens into a super-telephoto lens.

    image

    Thank you for the words of encouragement.