A Question of Scale
  • Challenges & Projects
  • Project14
  • A Question of Scale
  • More
  • Cancel
A Question of Scale
Blog Tiny24hourMoBot #3 : 13 hours have passed
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join A Question of Scale to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 7 Feb 2019 11:26 PM Date Created
  • Views 3154 views
  • Likes 12 likes
  • Comments 9 comments
  • mobile robots
  • tiny24hourmobot
  • hc-sr04
  • robotics projects
  • questionofscalech
  • arduino
Related
Recommended

Tiny24hourMoBot #3 : 13 hours have passed

dubbie
dubbie
7 Feb 2019
image

A Question of Scale

Enter Your Electronics & Design Project for a Chance to Win a Cartridge-Sized NES Portable or a $100 Shopping Cart!

Back to The Project14 homepage image

Project14 Home
Monthly Themes
Monthly Theme Poll

 

It is now over half way through the 24 hours for my Tiny Mobile Robot and I have a sort of working prototype.

 

image

 

I 3D printed a cylinder slightly wider than the widest part of the two motors which also had a mounting bar at the bottom. I very carefully used self-tapping screws to fix the motor unit to the mounting bar. It is stable but could easily break if knocked - so hopefully I will not knock it. I have programmed the Arduino Nano to simply move both wheels together so that the whole mobile robot moves backwards and forwards in a straight line as I need repeatability while I stuff everything inside the cylinder. As it is a mobile robot it needed to have some sort of sensor and as I had a HC-SR04 ultrasonic distance sensor I decided to use that. The HC-SR04 is a simple to use sensor as all you need to do is to add power, a trigger signal of at least 10 microseconds length and then measure the length in time of the echo pulse detected. Dividing the length of the detected echo by 58 converts time into distance in centimetres. At the moment it is not making use of the data from the sensor but it is all working, see below:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

There is a great deal of wheel slip as the batteries are quite heavy and it really needs elastic bands for tyres, but unfortunately I do not have any. I will see about using AAA instead of AA batteries later and see about fitting everything into the cylinder. I have also 3D printed a top for the cylinder so that I should be able to mount the ultrasonic rangefinder to that. I don't think it is going to look as good as I had hoped, nor is it going to be as tiny as I originally planned. Maybe I should call it the not quite so tiny mobile robot.

 

Well, it is late now so I'm going to bed soon. There is still time for a couple of hours work tomorrow morning before my 24 hours is up.

 

Dubbie

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 7 years ago +6
    Pretty sure you won't be able to stop working on this after 24 hours :-)
  • jw0752
    jw0752 over 7 years ago +6
    Often when working on a project for an extended period of time I will stop and find a point at which I can put it aside. I usually can't put it aside mentally even if I physically walk away from it. While…
  • dubbie
    dubbie over 7 years ago in reply to fmilburn +4
    Frank, You are probably right. I have already been thinking that maybe it could be a 25 hour (or 26 hours, or maybe ……). Having already (almost) made one I have already been thinking about making it smaller…
Parents
  • genebren
    genebren over 7 years ago

    Nice, simple design.  Have you thought about using O-rings as the tires?  I have used them quite successfully in the past.  I have accumulated a wide variety of O-rings which are part of my robotics tool box.

     

    Good luck with your project!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago in reply to genebren

    Gene,

     

    I did think about O rings, a lot, but mainly in frustration as I don't have any. I think they might be something I might need to buy. I would then have to work out how to design the wheels in TinkerCAD to make the grove for them to fit into. I'm not sure how difficult that might be.

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 7 years ago in reply to genebren

    Gene,

     

    I did think about O rings, a lot, but mainly in frustration as I don't have any. I think they might be something I might need to buy. I would then have to work out how to design the wheels in TinkerCAD to make the grove for them to fit into. I'm not sure how difficult that might be.

     

    Dubbie