Recycle & Retrofit
  • Challenges & Projects
  • Project14
  • Recycle & Retrofit
  • More
  • Cancel
Recycle & Retrofit
Blog Convert a PC PS to a Bench Power Supply
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Recycle & Retrofit to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 18 Oct 2020 9:16 AM Date Created
  • Views 10249 views
  • Likes 20 likes
  • Comments 35 comments
  • doug wong
  • bench supply
  • recycleretrofitch
  • pcps
  • pc power supply
Related
Recommended

Convert a PC PS to a Bench Power Supply

dougw
dougw
18 Oct 2020
image

Recycle & Retrofit

Enter Your Electronics & Design Project for a chance to win a $200 shopping cart!

Submit an EntrySubmit an Entry  Back to homepage image
Project14 Home
Monthly Themes
Monthly Theme Poll

 

I have a collection of old PCs from various scavenging activities. Somehow I just couldn't seem to pass up opportunities to acquire "free" PCs. They are probably all working, but I don't actually have a use for them as computers. I have "intended" for a long time to scavenge whatever might be repurposed off some of these computers - disk drives, power supplies, heat sinks, etc. But even for those items, I don't have a pressing need. I did make several attempts to design a conversion to create a bench power supply from the PC power supplies, because in the past I always seemed to need more power supplies, and they can be pretty expensive to buy.

I bought connectors and binding posts and even designed a couple of versions of PCB to get started. However I always stalled when trying to come up with a reasonable (cheap) way to package the bench supply. This Projec14 Upcycling theme is a good excuse to finally put a complete supply together.

image

These old PC power supplies have a bunch of output power connectors and the main connector comes in a couple of variants.

image

Note that the V2 connectors have all the same pins in the same places as the V1 connector so they are backward compatible, except the V2 power supplies are less likely to have a -5 V output.

Additionally, some of these power supplies need a load before they will regulate properly. The supply in the picture below is like this so I have provision for a load resistor on my PCBs.

I bought both types of connector, just in case, but the bigger one will always work, if plugged in at the right end.

I also bought a cheap commercial version (also shown in the picture below - the green card), but its tiny binding posts are at a non-standard spacing and cannot accommodate banana plugs.

image

Note that this particular power supply uses a V1 connector and it has a -5V output. (The LEDs from left to right indicate +12, +5, + 3.3, -12, -5)

The larger card (that is powered up in the above picture) was the first one I designed - when I had a different idea about how to package it.

The smaller card takes no more room than the power supply front face, so this is what I used in the build.

The supply I used in the build (different from the one pictured above) has a V2 connector and it does not need load resistors to regulate properly, but it has no -5 output.

Here is a video showing how these parts fit in the case I designed:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

I still have enough parts to build at least 2 more complete bench supplies plus more supplies and partial kits of parts, if I can find the time or if a need arises.

These supplies do take up space, but not as much as the full PC box they came out of.

I am happy that I didn't need to order parts (because I bought them years ago) and I am happy that I can at least mostly cross this project off my backlog/bucket list of projects.

It turned out to be quite a bit more work than I had envisioned way back, but I am happy with the final look of the supply, given all the awkward constraints it needed to accommodate.

I could have picked a more photogenic color, but black was what was in the printer.

In the end it does look like a bench supply with a nice handle and it has high quality binding posts.

Update:

I traced the power switch issue to a faulty switch and fixed it:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

A question arose in the comments below about how much power the 5VSB (5V stand by) pin could supply. I extracted another PC supply from yet another old PC to test it.

I connected my little load box which can switch in a load of up to four 10 ohm resistors in parallel and measure the voltage and current...

The 5VSB could supply 0.5 amps more or less okay, but 2 resistors (= 5 ohms) brought the voltage down below 3V...at which point the meter didn't have enough voltage to work.

imageimage

No load = 5.01V                                                      10 ohm load -> 4.39V, 0.46A

My power supply doesn't do anything with this pin.

 

Relevant links:

Project14 | Recycle & Retrofit: Reduce Waste in Style By Upcycling Vintage Electronics!

A later project to convert a PC Power Supply

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 5 years ago +7
    Something to be wary of is that if you don't have any over-current protection, the ATX spec allows up to ~20A to be drawn before tripping a short circuit protection which is enough current to make thinner…
  • DAB
    DAB over 5 years ago +6
    Great build Douglas. DAB
  • dougw
    dougw over 5 years ago in reply to genebren +6
    I was thinking about doing this before I had a 3D printer - just somehow hack saw and bash the sheet metal PC case into a power supply shape. I am sure it would have been pretty ugly.
Parents
  • Gough Lui
    Gough Lui over 5 years ago

    Something to be wary of is that if you don't have any over-current protection, the ATX spec allows up to ~20A to be drawn before tripping a short circuit protection which is enough current to make thinner wires get toasty real quick. More than that is the fact that more modern power supplies are even more lax about this - originally dividing up the beefy 12V rail into multiple rails that fit under the limit, but depending on how you wire the supply, it can be possible to short both rails together and thus exceed that 20A "limit". Later "gamer" style supplies eschewed the multi-rail design as that would occasionally cause heavy-load devices to trip their OCP limits, instead going for a single beefy 12V rail which might have 60A available (sometimes even more).

     

    While the power of the quality PSUs should be top notch, the lack of a current limit is a big concern for this reason. The lower-quality power supplies (e.g. no-brands from China) and older supplies which have served their time may not have such nice ripple and noise specs as well due to poor/aged capacitors. I also wouldn't count on the output to be isolated from ground (often, it is not), so it's not a wise idea to series units together for other voltages. It's a good fall-back for common voltages assuming you have nothing else, but I wouldn't be too enthusiastic about it having done a similar thing with AT supplies and fighting with minimum load, audible noise (at times) and cross-load behaviour (e.g. some supplies will have out-of-spec voltages if the loading on the rails doesn't approximate a PC in some way).

     

    - Gough

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to Gough Lui

    Thanks for sharing the insight. Sometimes what looks like a great solution can bite you in the buttocks. I have had the experience of a low gauge wire becoming fuses as you describe.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • colporteur
    colporteur over 5 years ago in reply to Gough Lui

    Thanks for sharing the insight. Sometimes what looks like a great solution can bite you in the buttocks. I have had the experience of a low gauge wire becoming fuses as you describe.

    • Cancel
    • Vote Up +6 Vote Down